EAGLE User Support (English) Through hole parts connected to the top layer
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
  • Replies 7 replies
  • Subscribers 182 subscribers
  • Views 2362 views
  • Users 0 members are here
Related

Through hole parts connected to the top layer

Plecto
Plecto over 13 years ago

Hi. I'm trying to make a board and then send it off to a board house for etching. I made the autorouter make the traces for me, both top and bottom traces with vias and all. The thing is that I have both SMT parts and through-hole parts on my board, but the autorouter doesn't seem to care. It sends top layer traces to my through-hole parts, how do I fix this?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    On 18/09/12 21:56, Tor-Arne Forsmo wrote:

    Hi. I'm trying to make a board and then send it off to a board house

    for etching. I made the autorouter make the traces for me, both top

    and bottom traces with vias and all. The thing is that I have both

    SMT parts and through-hole parts on my board, but the autorouter

    doesn't seem to care. It sends top layer traces to my through-hole

    parts, how do I fix this?

     

    Route it by hand?

     

    Why do you consider it needs fixing? If you're having a double sided

    board made professionally, surely it's going to be through-plated.

    Tracks connecting to through-hole components on the top side is not

    wrong - it's perfectly normal.

     

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Plecto
    Plecto over 13 years ago in reply to Former Member

    Yeah I thought about that, but there are alot of through hole components that simply cannot be soldered to on both sides (not by me atleast). Resistors, ceramic disc caps are probably easy to solder on both sides, but how do one go about doing that for a 4700uF 50V electrolytic cap? On my board I have two minijack connectors and a dual sided pot with a switch. The top contact points for these will be completely covered, so this can't be soldered to the top layer. Couldn't this be an issue for professional people aswell? Why do eagle assume that all through-hole components can be soldered to both layers?

     

    I also wonder about those vias. Will a PCB manufacturer care about how many they are? Or can I litter the board with vias and still get the same price? I'm just picturing that they take longer to make image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Plecto
    Plecto over 13 years ago in reply to Former Member

    Yeah I thought about that, but there are alot of through hole components that simply cannot be soldered to on both sides (not by me atleast). Resistors, ceramic disc caps are probably easy to solder on both sides, but how do one go about doing that for a 4700uF 50V electrolytic cap? On my board I have two minijack connectors and a dual sided pot with a switch. The top contact points for these will be completely covered, so this can't be soldered to the top layer. Couldn't this be an issue for professional people aswell? Why do eagle assume that all through-hole components can be soldered to both layers?

     

    I also wonder about those vias. Will a PCB manufacturer care about how many they are? Or can I litter the board with vias and still get the same price? I'm just picturing that they take longer to make image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 13 years ago in reply to Plecto

    Am 19.09.2012 08:17, schrieb Tor-Arne Forsmo:

    Yeah I thought about that, but there are alot of through hole components that simply cannot be soldered to on both sides (not by me atleast). Resistors, ceramic disc caps are probably easy to solder on both sides, but how do one go about doing that for a 4700uF 50V electrolytic cap? On my board I have two minijack connectors and a dual sided pot with a switch. The top contact points for these will be completely covered, so this can't be soldered to the top layer. Couldn't this be an issue for professional people aswell? Why do eagle assume that all through-hole components can be soldered to both layers?

     

    Eagle assumes nothing. You assume something wrong. A via is a little

    metal pipe connecting bottom and top tracks without any solder. The wire

    of a through hole component is going thorough the "pipe" and is soldered

    at the bottom only. It does not matter if the top is covered by the

    component since the connection to the top is made by the via itself

    already. Check the internet for pcb and via.

    I also wonder about those vias. Will a PCB manufacturer care about how many they are? Or can I litter the board with vias and still get the same price? I'm just picturing that they take longer to make image

     

    You get the answer from the manufacturer of your choice...

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Plecto

    Tor-Arne Forsmo wrote on Wed, 19 September 2012 02:17

    Yeah I thought about that, but there are alot of through hole

    components that simply cannot be soldered to on both sides (not by me

    atleast).

     

    They don't need to be.  As Rob mentioned, you will get plated thru holes.

    Each hole already connects the top and bottom layers even without a wire

    thru it and soldered.

     

    Quote:

    Why do eagle assume that all through-hole components can be soldered to

    both layers?

     

    Eagle doesn't assume anything.  This is dependent on how you set up the

    auto router.  However, the defaults are set up assuming plated thru holes

    because that's how multi-layer boards are made.

     

    Quote:

    I also wonder about those vias. Will a PCB manufacturer care about how

    many they are?

     

    Some do, some don't.  This comes down to the pricing strategy of the

    particular board house you choose.  Some board houses charge extra for more

    than some number of vias per square inch average.  Usually low volume

    prototype services don't charge extra for such things because there is

    significant margin built into the price already.  The same board house may

    apply a complicated formula to give you a quote for high volumes.  They

    often don't even tell you what their formula is, They simply give you a

    quote for some number of that particular board.

     

    For a two layer board with lots of thru hole parts, there is some advantage

    to routing most of the interconnects on the bottom layer.  This allows for

    easier editing to make cuts and jumpers and add parts as you find problems.

    This can be done with the auto router by setting the layer costs and other

    parameters appropriately.  If your interconnect scheme is not too

    complicated, you can try to reserve the top layer to be mostly a ground

    plane with only the minimum necessary "jumpers" in that layer that can't be

    routed in the single plane of the bottom layer.

     

    However, the bigger issue is why are you designing a real board for thru

    hole components?  Thru hole makes no sense other than when a part has to

    take some mechanical abuse, like a connector.  Otherwise, surface mount

    parts are smaller, cheaper, more available, have a much wider selection,

    and are easier to solder.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Plecto
    Plecto over 13 years ago in reply to Former Member

    Eagle doesn't assume anything.  This is dependent on how you set up the

    auto router.  However, the defaults are set up assuming plated thru holes

    because that's how multi-layer boards are made.

     

    So a board house makes holes for through-hole components like vias, with a conductive connection between the top and bottom layer? I guess I could talk to a pcb house to get the verified.

     

    However, the bigger issue is why are you designing a real board for thru

    hole components?  Thru hole makes no sense other than when a part has to

    take some mechanical abuse, like a connector.  Otherwise, surface mount

    parts are smaller, cheaper, more available, have a much wider selection,

    and are easier to solder.

     

    The through hole componets are two minijacks, a pot, two electrolytic caps, a led and a wafer connector. I guess the minijack and the wafer connector could be SMD, but I had little luck finding SMD minijacks and I have loads of through hole wafer connectors laying around. The pot is mounted to the side of the case and it's going to support the weight of the PCB so this has to be a through hole part. The led is mounted behind the minijack and it's pins are going to be bent over it and through the side of the case so I believe it's safer to have the LED as a through hole part aswell. I haven't been looking for a 100uF SMD cap, if they exist then I could replace the through-hole caps for SMD ones.