EAGLE User Support (English) Through hole parts connected to the top layer
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
  • Replies 7 replies
  • Subscribers 182 subscribers
  • Views 2366 views
  • Users 0 members are here
Related

Through hole parts connected to the top layer

Plecto
Plecto over 13 years ago

Hi. I'm trying to make a board and then send it off to a board house for etching. I made the autorouter make the traces for me, both top and bottom traces with vias and all. The thing is that I have both SMT parts and through-hole parts on my board, but the autorouter doesn't seem to care. It sends top layer traces to my through-hole parts, how do I fix this?

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 13 years ago

    On 18/09/12 21:56, Tor-Arne Forsmo wrote:

    Hi. I'm trying to make a board and then send it off to a board house

    for etching. I made the autorouter make the traces for me, both top

    and bottom traces with vias and all. The thing is that I have both

    SMT parts and through-hole parts on my board, but the autorouter

    doesn't seem to care. It sends top layer traces to my through-hole

    parts, how do I fix this?

     

    Route it by hand?

     

    Why do you consider it needs fixing? If you're having a double sided

    board made professionally, surely it's going to be through-plated.

    Tracks connecting to through-hole components on the top side is not

    wrong - it's perfectly normal.

     

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Plecto
    Plecto over 13 years ago in reply to Former Member

    Yeah I thought about that, but there are alot of through hole components that simply cannot be soldered to on both sides (not by me atleast). Resistors, ceramic disc caps are probably easy to solder on both sides, but how do one go about doing that for a 4700uF 50V electrolytic cap? On my board I have two minijack connectors and a dual sided pot with a switch. The top contact points for these will be completely covered, so this can't be soldered to the top layer. Couldn't this be an issue for professional people aswell? Why do eagle assume that all through-hole components can be soldered to both layers?

     

    I also wonder about those vias. Will a PCB manufacturer care about how many they are? Or can I litter the board with vias and still get the same price? I'm just picturing that they take longer to make image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 13 years ago in reply to Plecto

    Am 19.09.2012 08:17, schrieb Tor-Arne Forsmo:

    Yeah I thought about that, but there are alot of through hole components that simply cannot be soldered to on both sides (not by me atleast). Resistors, ceramic disc caps are probably easy to solder on both sides, but how do one go about doing that for a 4700uF 50V electrolytic cap? On my board I have two minijack connectors and a dual sided pot with a switch. The top contact points for these will be completely covered, so this can't be soldered to the top layer. Couldn't this be an issue for professional people aswell? Why do eagle assume that all through-hole components can be soldered to both layers?

     

    Eagle assumes nothing. You assume something wrong. A via is a little

    metal pipe connecting bottom and top tracks without any solder. The wire

    of a through hole component is going thorough the "pipe" and is soldered

    at the bottom only. It does not matter if the top is covered by the

    component since the connection to the top is made by the via itself

    already. Check the internet for pcb and via.

    I also wonder about those vias. Will a PCB manufacturer care about how many they are? Or can I litter the board with vias and still get the same price? I'm just picturing that they take longer to make image

     

    You get the answer from the manufacturer of your choice...

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 13 years ago in reply to Plecto

    Am 19.09.2012 08:17, schrieb Tor-Arne Forsmo:

    Yeah I thought about that, but there are alot of through hole components that simply cannot be soldered to on both sides (not by me atleast). Resistors, ceramic disc caps are probably easy to solder on both sides, but how do one go about doing that for a 4700uF 50V electrolytic cap? On my board I have two minijack connectors and a dual sided pot with a switch. The top contact points for these will be completely covered, so this can't be soldered to the top layer. Couldn't this be an issue for professional people aswell? Why do eagle assume that all through-hole components can be soldered to both layers?

     

    Eagle assumes nothing. You assume something wrong. A via is a little

    metal pipe connecting bottom and top tracks without any solder. The wire

    of a through hole component is going thorough the "pipe" and is soldered

    at the bottom only. It does not matter if the top is covered by the

    component since the connection to the top is made by the via itself

    already. Check the internet for pcb and via.

    I also wonder about those vias. Will a PCB manufacturer care about how many they are? Or can I litter the board with vias and still get the same price? I'm just picturing that they take longer to make image

     

    You get the answer from the manufacturer of your choice...

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag