Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) A collection of questions from a beginer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 514 views
  • Users 0 members are here
Related

A collection of questions from a beginer

StefanTh
StefanTh over 13 years ago

Hi

 

Why does not Eagle come with a most of the standard packages included, for exmaple,

if I do a seach for "*SOT-223*" this one do not show up, neither do SOT-25, SOT-89 etc.

If eagle have these standard packages, they should be searchable.

 

When I a create a new device in the library I add the ">NAME" and ">VALUE" to the schematics,

but whne I include this created device the "NAME" become "U$1" why ? Should it not become IC1 ?

 

When I create a new device I want to reserve an area where no copper may be used, filled or be drawned,

in any of the pcb layers. I assume I just create an area in the package editor of the device

but should it be of the type "41 tRestriced" or what ?

Do I have to add an area for each copper layer ?

 

Unplesant behaviour of the "Net" in schematic,

unless the pins for a device in the library is made in Imperial (100 mil distance) the Net does not

connect to the pins when making a schematic with the device.

Expected and normal behaviour should be that the "Net" automatically connects to the nearst

pin within +- 2 grid steps.

 

 

/Stefan

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am 01.10.2012 16:55, schrieb Stefan Olsson:

    Why does not Eagle come with a most of the standard packages included, for exmaple,

    if I do a seach for "SOT-223" this one do not show up, neither do SOT-25, SOT-89 etc.

    If eagle have these standard packages, they should be searchable.

     

    They ARE available, and you CAN search them. Unfortunately, different

    manufacturers call them differently. In this case, EAGLE calls them

    SOT223-5EV-VREGSOT223-5EV-VREG etc. (WITHOUT the hyphen).

     

    When I a create a new device in the library I add the ">NAME" and ">VALUE" to the schematics,

    but whne I include this created device the "NAME" become "U$1" why ? Should it not become IC1 ?

     

    No. It should NOT automatically become IC1. Of course YOU know that you

    have just created an IC component in the library, but EAGLE doesn't. You

    might have just created a resistor, which should become R1, or a

    capacitor, which should be named C1. Therefore, you must tell EAGLE in

    the library HOW the component should be labelled:

     

    In the device editor, use the PREFIX button at the bottom right and then

    type in the prefix you want the component to have: R for resistors, C

    for capacitors, IC for ICs, etc. The NUMBERS are set be EAGLE automatically.

     

    When I create a new device I want to reserve an area where no copper may be used, filled or be drawned,

    in any of the pcb layers. I assume I just create an area in the package editor of the device

    but should it be of the type "41 tRestriced" or what ?

     

    Yes. The 'Restrict' layers do that.

     

    Do I have to add an area for each copper layer ?

     

    Yes. Objects in the 'tRestrict' layer prevent copper from automatically

    appearing in the TOP layer, 'bRestrict' for the BOTTOM layer.

     

    Unplesant behaviour of the "Net" in schematic,

    unless the pins for a device in the library is made in Imperial (100 mil distance) the Net does not

    connect to the pins when making a schematic with the device.

     

    This IS a restriction, yes, but ALL the library parts use that grid. And

    it is a VERY good idea to build your library parts using that grid, too,

    even if you perhaps don't like it too much.

     

    Expected and normal behaviour should be that the "Net" automatically connects to the nearst

    pin within +- 2 grid steps.

     

    For simple schematics, that might be OK. For large or dense schematics,

    this is NOT such a good idea, since it might easily create connections

    to the WRONG pins.

     

    Andreas Weidner

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am 01.10.2012 16:55, schrieb Stefan Olsson:

    Why does not Eagle come with a most of the standard packages included, for exmaple,

    if I do a seach for "SOT-223" this one do not show up, neither do SOT-25, SOT-89 etc.

    If eagle have these standard packages, they should be searchable.

     

    They ARE available, and you CAN search them. Unfortunately, different

    manufacturers call them differently. In this case, EAGLE calls them

    SOT223-5EV-VREGSOT223-5EV-VREG etc. (WITHOUT the hyphen).

     

    When I a create a new device in the library I add the ">NAME" and ">VALUE" to the schematics,

    but whne I include this created device the "NAME" become "U$1" why ? Should it not become IC1 ?

     

    No. It should NOT automatically become IC1. Of course YOU know that you

    have just created an IC component in the library, but EAGLE doesn't. You

    might have just created a resistor, which should become R1, or a

    capacitor, which should be named C1. Therefore, you must tell EAGLE in

    the library HOW the component should be labelled:

     

    In the device editor, use the PREFIX button at the bottom right and then

    type in the prefix you want the component to have: R for resistors, C

    for capacitors, IC for ICs, etc. The NUMBERS are set be EAGLE automatically.

     

    When I create a new device I want to reserve an area where no copper may be used, filled or be drawned,

    in any of the pcb layers. I assume I just create an area in the package editor of the device

    but should it be of the type "41 tRestriced" or what ?

     

    Yes. The 'Restrict' layers do that.

     

    Do I have to add an area for each copper layer ?

     

    Yes. Objects in the 'tRestrict' layer prevent copper from automatically

    appearing in the TOP layer, 'bRestrict' for the BOTTOM layer.

     

    Unplesant behaviour of the "Net" in schematic,

    unless the pins for a device in the library is made in Imperial (100 mil distance) the Net does not

    connect to the pins when making a schematic with the device.

     

    This IS a restriction, yes, but ALL the library parts use that grid. And

    it is a VERY good idea to build your library parts using that grid, too,

    even if you perhaps don't like it too much.

     

    Expected and normal behaviour should be that the "Net" automatically connects to the nearst

    pin within +- 2 grid steps.

     

    For simple schematics, that might be OK. For large or dense schematics,

    this is NOT such a good idea, since it might easily create connections

    to the WRONG pins.

     

    Andreas Weidner

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • StefanTh
    StefanTh over 13 years ago in reply to e14 Contributor

    Hi

     

    Thanks a lot for your quick answear,

     

    I found some SOt's by removing the hyphen, thanks.

     

     

     

    Additonal stuff.

     

    When the board is routed the first times, you usally place the components out and then give some test shoots

    with the auto router to see how complicated the routign become and then start to move the components around

    to get a simpler solution.

    Is there a quck way of removing all the copper lines in the "Board view" with one click ?

    As it is now I do "ripup" on every single line.

     

    Also, is it possible to route a specific net ?

    For example, I want to route all the lines connected to ground (or supply) first with a little thicker line than the signal lines.

    As now, I first have to route the board, rip up those lines that is directly connected to ground, reset the line thickness,

    and do auto route.

     

    /Stefan