Hi
Why does not Eagle come with a most of the standard packages included, for exmaple,
if I do a seach for "*SOT-223*" this one do not show up, neither do SOT-25, SOT-89 etc.
If eagle have these standard packages, they should be searchable.
When I a create a new device in the library I add the ">NAME" and ">VALUE" to the schematics,
but whne I include this created device the "NAME" become "U$1" why ? Should it not become IC1 ?
When I create a new device I want to reserve an area where no copper may be used, filled or be drawned,
in any of the pcb layers. I assume I just create an area in the package editor of the device
but should it be of the type "41 tRestriced" or what ?
Do I have to add an area for each copper layer ?
Unplesant behaviour of the "Net" in schematic,
unless the pins for a device in the library is made in Imperial (100 mil distance) the Net does not
connect to the pins when making a schematic with the device.
Expected and normal behaviour should be that the "Net" automatically connects to the nearst
pin within +- 2 grid steps.
/Stefan