1) I cannot delete/remove the dimesions (6.2).
How to do this?
2) The dimensions do not change if the element that was use to create them change its size.
Can this be done, like in CAD program?
1) I cannot delete/remove the dimesions (6.2).
How to do this?
2) The dimensions do not change if the element that was use to create them change its size.
Can this be done, like in CAD program?
Soeren Boegh wrote:
1) I cannot delete/remove the dimesions (6.2).
How to do this?
Use the DELETE tool and click on the arrow points. There is another point.
You should read the HELP to understand where this will be located, as it
varies.
2) The dimensions do not change if the element that was use to create
them change its size.
Can this be done, like in CAD program?
The dimensions do not snap to other objects and thus are independant of
other objects.
Do some tests and you will see that dimensions snap to the grid so the grid
needs to be fine enough when dimensioning so errors are not introduced.
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
Soeren Boegh wrote:
1) I cannot delete/remove the dimesions (6.2).
How to do this?
Use the DELETE tool and click on the arrow points. There is another point.
You should read the HELP to understand where this will be located, as it
varies.
2) The dimensions do not change if the element that was use to create
them change its size.
Can this be done, like in CAD program?
The dimensions do not snap to other objects and thus are independant of
other objects.
Do some tests and you will see that dimensions snap to the grid so the grid
needs to be fine enough when dimensioning so errors are not introduced.
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
No, that does not work (both).
But, if the measured object is moved or deletet - then the dimension can be deleted on the outermost pixel (common with the object).
Seems to me as a bug - because what you and the manual describe does not work.