Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Dimensions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 458 views
  • Users 0 members are here
Related

Dimensions

e14 Contributor
e14 Contributor over 13 years ago

1) I cannot delete/remove the dimesions (6.2).

 

How to do this?

 

2) The dimensions do not change if the element that was use to create them change its size.

 

Can this be done, like in CAD program?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Soeren Boegh wrote:

    1) I cannot delete/remove the dimesions (6.2).

     

    How to do this?

     

     

    Use the DELETE tool and click on the arrow points. There is another point.

    You should read the HELP to understand where this will be located, as it

    varies.

     

    2) The dimensions do not change if the element that was use to create

    them change its size.

     

    Can this be done, like in CAD program?

     

    The dimensions do not snap to other objects and thus are independant of

    other objects.

    Do some tests and you will see that dimensions snap to the grid so the grid

    needs to be fine enough when dimensioning so errors are not introduced.

     

    HTH

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    No, that does not work (both).

     

    But, if the measured object is moved or deletet - then the dimension can be deleted on the outermost pixel (common with the object).

     

    Seems to me as a bug - because what you and the manual describe does not work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    No, that does not work (both).

     

    But, if the measured object is moved or deletet - then the dimension can be deleted on the outermost pixel (common with the object).

     

    Seems to me as a bug - because what you and the manual describe does not work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Il 03/10/2012 23:03, Warren Brayshaw ha scritto:

     

    beta 6.2.3 adds more functionality

       - Some extensions to the DIMENSION command:

         - Selection of rectangles and origins of elements or parts.

         - Snap to objects on defining the second dimension point.

     

     

    That will be very nice!

    EAGLE is a CAD (well, should be) but it doesn't have a lot of common

    features of standard CAD softwares.

     

    Marco

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Soeren Boegh wrote:

    No, that does not work (both).

     

    But, if the measured object is moved or deletet - then the dimension

    can be deleted on the outermost pixel (common with the object).

     

     

    Seems to me as a bug - because what you and the manual describe does

    not work.

     

    It does work for me with Windows and using Eagle beta 6.2.2

    Which Windows/Mac/Linux  are you using. That my be relevant.

    Consider downloading the latest beta and see if all is well then.

     

    There are only three places you can click to delete the dimension object.

    Ensure you understand how to select the object you require. See HELP

    Selecting Objects in a Dense Area

     

    I said previously

    ...".The dimensions do not snap to other objects and thus are independent of

    other objects.".....

    This is not true. The first point does snap to some objects as the HELP

    (beta 6.2.2 ) suggests

     

    beta 6.2.3 adds more functionality

      - Some extensions to the DIMENSION command:

        - Selection of rectangles and origins of elements or parts.

        - Snap to objects on defining the second dimension point.

     

    To have the dimensions move with the object, you can group the object and

    the dimension points and move them as a set. If you group the object and one

    end of the dimension then the text value will adjust to the new distance.

     

    HTH

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de