May I suggest coming up with a less cryptic method of setting up layers
in the DRC? Perhaps a front-end or a wizard that would set the setup line.
Just right off the top of my head, have several text boxes that ask
/pertinent/ questions:
Active layers: 1,2,3,14,15,16
Via connections: All
Blind Vias: 1-2-3,14-15-16
Buried Vias: 2-3,14-15
A dash represents a connection between layers. In the above example,
blind vias are defined to connect layer 1, 2, and 3, and to connect
layers 14,15, and 16. Buried vias connect layers 2 and 3, and connect
layers 14 and 15.
There really is no need to even ask whether or not an insulating layer
is core or prepreg, nor is there a need to define the thicknesses of
each layer. This is something that goes in a README file when the
gerbers are sent to the board house.
I wonder if this could be done in a ULP.
Best regards,
- Chuck