Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Library editor integration
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 506 views
  • Users 0 members are here
  • library_editor
Related

Library editor integration

e14 Contributor
e14 Contributor over 13 years ago

Hi, I had to change the shape of one pad (in the IC Package the pin 1 is a square so as to help correct orientation when assembling the board). I had to right-click, find the library file name and the name of the part; then open the library, search for the package, open it, change the shape of the pin, save. Then back to the board and update the library.

 

Maybe there is a shortcut I am not aware of, but I would suggest adding an "edit library" or similar in the right-click menu that would open the component for edit and do the update on exiting.

 

Regards!

  • Sign in to reply
  • Cancel
  • CSWalt
    CSWalt over 13 years ago

    Hi,

     

    On 11/03/12 14:57, luis marka wrote:

    Hi, I had to change the shape of one pad (in the IC Package the pin 1 is a square so as to help correct orientation when assembling the board). I had to right-click, find the library file name and the name of the part; then open the library, search for the package, open it, change the shape of the pin, save. Then back to the board and update the library.

     

    Maybe there is a shortcut I am not aware of, but I would suggest adding an "edit library" or similar in the right-click menu that would open the component for edit and do the update on exiting.

     

    Regards!

     

    That's already on our todo list and we hope to have this very soon.

     

    Regards,

    Walter Spermann

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi Warren!

    Thanks a lot, got the file in my email and it works great! Nice shortuct for an otherwise cumbersome operation...

     

    Best regards!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi there Warren!

    That should make things easier... but I can't seem to find the attached Get_Name.ulp file on your reply, maybe that's because this is the very first time I am using this forum and still haven't got the hang of it...!

    If you feel like it, email the file to luis.marka@terra.com.br, ok?

     

    Best regards, and thanks a lot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Quote:

    Hi, I had to change the shape of one pad (in the IC Package the pin 1

    is a square so as to help correct orientation when assembling the board).

    I had to right-click, find the library file name and the name of the

    part; then open the library, search for the package, open it, change the

    shape of the pin, save. Then back to the board and update the library.

     

    Maybe there is a shortcut I am not aware of, but I would suggest adding

    an "edit library" or similar in the right-click menu that would open the

    component for edit and do the update on exiting

     

     

    I agree, there should be a quick(native) way to get from a symbol or

    element to the source library  item.

     

    Until that feature is added you can do it the following way, for a board

    element(package):

    1) Save the attached ULP (Get_Name.ulp) into your ULP folder.

    2) In the board editor, create a custom context menu item by entering into

    the command line:

     

      set context element 'Edit Package' 'run Get_Name'

     

    In use you right click the package(element) of interest. Actually any

    element will do. The context menu opens and you should see, towards the

    bottom, the item 'Edit Package' which you click.

    This runs the attached ULP  'Get_Name.ulp' into which you enter the name of

    the part of interest. e.g. R1

    Get_element.ulp then calls the ULP 'edit-used-dev-pac-sym.ulp' which opens

    the library package you want.(The package of R1 in this example).

     

    The above also works in the schematic and you get taken to the Device

    editor.

    You need to set up the context item in the schematic using the command

     

    set context instance 'Edit Package' 'run Get_Name'

     

    HTH

    Warren

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.