Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Allow creating a schematic without creating a board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 407 views
  • Users 0 members are here
  • eagle
  • layout
  • eagle_cad
  • library
  • library_editor
  • drafting
  • cad
  • Design
  • libraries
  • features
Related

Allow creating a schematic without creating a board

reidkersey
reidkersey over 13 years ago

I sometimes just want to create a schematic, to demonstrate signal flow, a system overview, or as a refrence for a freewired system. I find myself troubled by the workaround that I have to do to make this work.

 

I would like to be able to create library parts that do not have a physical package, and put them into the schematic. Currently as a workaround, I create the parts that I want, and just randomly connect them to a package that has 200+ pads.

 

It is possible to make boards without schematics. Why is it not possible to do it the otherway around?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 11/5/2012 12:27 PM, Reid Kersey wrote:

     

    Hi Reid,

     

    This is possible just draw the symbols without using any pins, if you do

    that EAGLE will allow you to create devices which don't need packages.

     

    Additionally in V6 we introduced the EXTERNAL attribute which allows

    you to define a device which doesn't require a package.

     

    See the manual for more info or HELP PACKAGE.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    On 11/5/2012 12:27 PM, Reid Kersey wrote:

     

    Hi Reid,

     

    This is possible just draw the symbols without using any pins, if you do

    that EAGLE will allow you to create devices which don't need packages.

     

    Additionally in V6 we introduced the EXTERNAL attribute which allows

    you to define a device which doesn't require a package.

     

    See the manual for more info or HELP PACKAGE.

     

    Best Regards,

    Jorge Garcia