Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Using Eagle libraries on a shared network drive
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 190 subscribers
  • Views 896 views
  • Users 0 members are here
Related

Using Eagle libraries on a shared network drive

e14 Contributor
e14 Contributor over 13 years ago

Hi

 

I have started working in a company where Eagle is used, but there is currently no library management going on. I would like to organise the way we work so that there is a central repository for libraries such that we can ensure any new designs are created with the latest version of any component library.

 

This may be a simple question, but are there any pitfalls to using Eagle with its libraries located on a shared network drive? This would be ideal as it means there will be no duplicate copies anywhere. However I may be overlooking something vital so would appreciate some feedback on whether simply pointing Eagle to find its libraries on a shared network drive is a good solution?

 

 

Many thanks!

 

Angus

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Angus Thomson wrote:

     

    >This may be a simple question, but are there any pitfalls to using

    Eagle with its libraries located on a shared network drive?

     

    no problem, just make sure there are no concurrent edits.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • igalloway
    igalloway over 13 years ago in reply to e14 Contributor

    I'd like to suggest an alternative is to run a SVN (Subversion) or other repository, and have each user checkout the library and project files on their own machine locally.

    - We use TortoiseSVN and actually have it linked to Bugzilla for automatic updating of bugs when commiting the change!

    Version control is very helpful when working on a schematic and board!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to igalloway

    Iain Galloway wrote:

     

    >I'd like to suggest an alternative is to run a SVN (Subversion) or other repository, and have each user checkout the library and project files on their own machine locally.

    >- We use TortoiseSVN and actually have it linked to Bugzilla for automatic updating of bugs when commiting the change!

    >Version control is very helpful when working on a schematic and board!

     

    of course, that's one reason why I voted for a plain text format in

    the past.

     

    Nevertheless you have to provide mesures against concurrent edits.

     

    Well, with the V6 XML format, you might be able to merge changes,

    but I think that's not what a user wants to do.

     

    Oliver

     

    P.S. could somebody at element14 limit the line length to 70

    characters or so?

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to igalloway

    Iain Galloway wrote:

     

    >I'd like to suggest an alternative is to run a SVN (Subversion) or other repository, and have each user checkout the library and project files on their own machine locally.

    >- We use TortoiseSVN and actually have it linked to Bugzilla for automatic updating of bugs when commiting the change!

    >Version control is very helpful when working on a schematic and board!

     

    of course, that's one reason why I voted for a plain text format in

    the past.

     

    Nevertheless you have to provide mesures against concurrent edits.

     

    Well, with the V6 XML format, you might be able to merge changes,

    but I think that's not what a user wants to do.

     

    Oliver

     

    P.S. could somebody at element14 limit the line length to 70

    characters or so?

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    On 23/11/12 07:38, Oliver Betz wrote:

    Nevertheless you have to provide mesures against concurrent edits.

     

    Using SVN (or any other VCS, probably) it is possible to mark files as

    non-mergeable. The result of this is that the local copy is read-only

    until the user tries to lock it for editing. If somebody else has it

    locked then this attempt fails with a helpful message. That's normally

    enough "measures against concurrent edits"

     

    HTH

    Rob