how I will find the centre of hole
In order to I connect the pin with polygon
toths wrote:
hi friend Image:test.png
how I will find the centre of hole
In order to I connect the pin with polygon
I dont see any un-routed signal wires (airwires). Is that layer turned off
or have you created a board without using a schematic?
If so you will need to run a SIGNAL from that pad to another pad or SMD that
should be connected. That signal shouold be given the same name as your
polygon.
If the board was generated from a schematic, run an ERC check as you may
have nets that are not connected to the pin in the schematic
For the polygon to connect to the pin they both have to have the NAME. The
pin name in this context is the signal name (net name) attached to the pin
Hope this helps
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
No solution in my problem
I bought this program that does not offer nothing other apart from the basic operations cad and these with the use ulp
And non-existent team of support
I was not careful as long as it would be supposed
I thank for the solution that you gave in my problem the team of support
But I am compelled to search for some professional PCB CAD
CadSoft you correct this error
Technical Support – element14 tech support forum
Get technical support from the CadSoft staff and other EAGLE users. You will be connected to our forum within the element14 engineering community site.