EAGLE User Support (English) CAM output bug, all versions.
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 549 views
  • Users 0 members are here
  • bugs
  • bug
  • job
  • cam
  • cam_job
Related

CAM output bug, all versions.

xxxajk
xxxajk over 10 years ago

Eagle 7.3.0 on Linux (and quite possible ALL older versions) has a very annoying bug.

When outputting CAM file, the coordinates seem to always be off +0.01 inches in both the X and Y directions..

Here is an example with X/Y offset at 0.5inches

 

image

If I subtract an additional 0.01 inches it will line up, but this is clearly a bug. I should not have to do this.

 

Looking at the output, the offset is not set correctly. It is using an offset of -0.49!

 

G75*

%MOIN*%

%OFA0B0*%

%FSLAX25Y25*%

%IPPOS*%

%LPD*%

%AMOC8*

5,1,8,0,0,1.08239X$1,22.5*

%

%ADD10C,0.00000*%

D10*

X-0049000Y0001000D02*

X0555000Y0001000D01*

X0505000Y-0049000D02*

X0505000Y0401000D01*

X0555000Y0351000D02*

X-0049000Y0351000D01*

X0001000Y0401000D02*

X0001000Y-0049000D01*

M02*

 

and here is the output with the extra .01 subtracted (offsets @ 0.51inch):

 

G75*

%MOIN*%

%OFA0B0*%

%FSLAX25Y25*%

%IPPOS*%

%LPD*%

%AMOC8*

5,1,8,0,0,1.08239X$1,22.5*

%

%ADD10C,0.00000*%

D10*

X-0050000Y0000000D02*

X0554000Y0000000D01*

X0504000Y-0050000D02*

X0504000Y0400000D01*

X0554000Y0350000D02*

X-0050000Y0350000D01*

X0000000Y0400000D02*

X0000000Y-0050000D01*

M02*

 

This also happens in the positive direction, or if there is to be no offset at all.

This is the output with a "0" offset. Clearly it is not at zero.

 

G75*

%MOIN*%

%OFA0B0*%

%FSLAX25Y25*%

%IPPOS*%

%LPD*%

%AMOC8*

5,1,8,0,0,1.08239X$1,22.5*

%

%ADD10C,0.00000*%

D10*

X0051000Y0001000D02*

X0051000Y0451000D01*

X0001000Y0401000D02*

X0605000Y0401000D01*

X0555000Y0451000D02*

X0555000Y0001000D01*

X0605000Y0051000D02*

X0001000Y0051000D01*

M02*

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago in reply to xxxajk +1
    Hi Andrew, I hope you're doing well. I don't think this is a bug, you probably have the pos. coords setting on in the CAM processor. For this setting to work properly all of the tabs within your CAM job…
Parents
  • xxxajk
    xxxajk over 10 years ago

    Update: it is also off by 50% of the line width at zero too.

    a 12 mil line will make the offset wrong by 0.016 inches.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to xxxajk

    Hi Andrew,

     

    I hope you're doing well. I don't think this is a bug, you probably have

    the pos. coords setting on in the CAM processor. For this setting to

    work properly all of the tabs within your CAM job need to have it set

    the same way. (All checked or none checked).

     

    It basically adds a small offset so that all of your board data is on

    the positive X and Y axis. If you disable the checkbox in your CAM jobs

    you'll see that everything is as you expect.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago in reply to xxxajk

    Hi Andrew,

     

    I hope you're doing well. I don't think this is a bug, you probably have

    the pos. coords setting on in the CAM processor. For this setting to

    work properly all of the tabs within your CAM job need to have it set

    the same way. (All checked or none checked).

     

    It basically adds a small offset so that all of your board data is on

    the positive X and Y axis. If you disable the checkbox in your CAM jobs

    you'll see that everything is as you expect.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • xxxajk
    xxxajk over 10 years ago in reply to autodeskguest

    Thanks! image

     

    Why is there a default like this?! Argh :-)