Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) APPCRASH EAGLE 6.4 on WIN 7 64
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 195 subscribers
  • Views 5062 views
  • Users 0 members are here
  • eagle
Related

APPCRASH EAGLE 6.4 on WIN 7 64

terje
terje over 13 years ago

Dear the support team at Cadsoft!

I have just purchased and installed Eagle pro shematic and layout package on to my brand new win 7 64 computer.

 

I'm now trying to design some new components with the library editor but every 3 to 10 minutes the application crashes and the work is lost.

To me it appears that the crash happens randomly. It can happen when I'm resizing the window, moving a element, copy a element, changing the grid. pushing the undo button  etc. etc.

For now the Eagle is useless as this happens too frequently.

 

The eagle program is installed under C:\eagle

The version is 6.4.0.

 

What did I do wrong?

 

Is this a known issue?

 

 

 

Windows crash report:

 

Problem event name: APPCRASH

Programname: eagle.exe

Programversion: 0.0.0.0

Timestamp for program: 50eaf0df

Error module name: ntdll.dll

Error module version: 6.1.7601.17725

Timestamp on error module: 4ec49b8f

Exeption code: c0000005

Exeption scew: 0002e3be

OS-versjon: 6.1.7601.2.1.0.256.48

ID for national setting: 1044

Additional information 1: 0a9e

Additional information2: 0a9e372d3b4ad19135b953a78882e789

Additional information3: 0a9e

Additional information4: 0a9e372d3b4ad19135b953a78882e789

 

 

 

Best Regards

Terje

  • Sign in to reply
  • Cancel
Parents
  • Krycek
    Krycek over 13 years ago

    I am having the same problems using 6.4.0 under Windows 7 64 bit.

     

    First I could get the app to crash while editing text properties in the schematic editor but now I have just lost a lot of work in the library editor when editing the properties of a plated through hole drill size when modifying an existing part.

     

    When I booted Eagle 6.4.0 back up it had lost the working directory I use as well as where my libraries are stored and reverted back to defaults.

     

    My projects and library files are saved on a network drive and have been since I first started using Eagle at version 6.0 so its not that - I have reverted back to 6.3 so I can continue working on an urgent project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Krycek

    TO ALL:

         The problem is with all 32bit programs running within the 64bit Windows. Change from 64 to 32 and probelm solved. From the day Windows XP was avalilable in 32bit and 64bit mode, it has been a problem. And it has not been solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Considering the number of applications out there (Photoshop, Sony Vegas Pro

    etc.) that are going to 64 bit only, having to switch back to 32 bit is

    hardly a "handy" solution these days (although I do dual boot into XP Pro

    32 if I want).  My wife won't let me have a separate computer for each

    application though ...

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Considering the number of applications out there (Photoshop, Sony Vegas Pro

    etc.) that are going to 64 bit only, having to switch back to 32 bit is

    hardly a "handy" solution these days (although I do dual boot into XP Pro

    32 if I want).  My wife won't let me have a separate computer for each

    application though ...

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.