Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) APPCRASH EAGLE 6.4 on WIN 7 64
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 195 subscribers
  • Views 5059 views
  • Users 0 members are here
  • eagle
Related

APPCRASH EAGLE 6.4 on WIN 7 64

terje
terje over 13 years ago

Dear the support team at Cadsoft!

I have just purchased and installed Eagle pro shematic and layout package on to my brand new win 7 64 computer.

 

I'm now trying to design some new components with the library editor but every 3 to 10 minutes the application crashes and the work is lost.

To me it appears that the crash happens randomly. It can happen when I'm resizing the window, moving a element, copy a element, changing the grid. pushing the undo button  etc. etc.

For now the Eagle is useless as this happens too frequently.

 

The eagle program is installed under C:\eagle

The version is 6.4.0.

 

What did I do wrong?

 

Is this a known issue?

 

 

 

Windows crash report:

 

Problem event name: APPCRASH

Programname: eagle.exe

Programversion: 0.0.0.0

Timestamp for program: 50eaf0df

Error module name: ntdll.dll

Error module version: 6.1.7601.17725

Timestamp on error module: 4ec49b8f

Exeption code: c0000005

Exeption scew: 0002e3be

OS-versjon: 6.1.7601.2.1.0.256.48

ID for national setting: 1044

Additional information 1: 0a9e

Additional information2: 0a9e372d3b4ad19135b953a78882e789

Additional information3: 0a9e

Additional information4: 0a9e372d3b4ad19135b953a78882e789

 

 

 

Best Regards

Terje

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to matriedel

    Why are you trying to run Eagle under Windows 64 ?

    On Microsoft site in Dev Center is this info: "WOW64 is the x86 emulator that allows 32-bit Windows-based applications to run seamlessly on 64-bit Windows."

    It is clear that this emulator is not running seamlessly all of the time.

    So until Microsoft fixes this, it makes more sense to run 32 bit versions until then.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • matriedel
    matriedel over 13 years ago

    I tried EAGLE 6.4.2 beta. Still crashing after 1h. Very bad for me ....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wardelder
    wardelder over 13 years ago

    Beta 6.4.2 fixed the issue for me too.  Good work but poor communication.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Krycek
    Krycek over 13 years ago in reply to Krycek

    I have just tried the BETA 6.4.2 and I can confirm that changing properties on text as well as opening and closing the help screen haven't caused this version to crash on my system. Fingers crossed for a full release soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to COMPACT

    I uninstalled EAGLE 6.4 to trial EAGLE 6.4.2 beta. The crashing has stopped. This is great news.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to COMPACT

    Note to all: Even running EAGLE as administrator has the identical behaviour.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to wardelder

    I reported this issue with EAGLE support when I got my new PC (with Windows 8 64-bit) in February but it was promptly dismissed as a user installation error.

     

    This blog trail has confirmed that it was not me and there is actually a fault.

     

    I can confirm that the Press F1 for help and closing the subsequent help dialog box is the fastest way of getting the error.

     

    As a guess it'll be a single cause creating this angst.

     

    Hopefully it will be fixed soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Mr.Pi
    Mr.Pi over 13 years ago

    Hi everybody.

     

    I am not using Windows 7 but I still have the same problems with Eagle crashing.

    I am using Windows XP SP3 and Eagle 6.4.0 free Version.

     

    Here is what I noticed:

    I switch on my notebook, start Eagle and work for hours without any problem.

    Then I start Acrobat Reader to open a data sheet or whatever and that is when the problem begins.

    Sometimes I can see Eagle disappear from  the task bar while Acrobat opens. Usually Eagle is closed without warning when I click on any of the icons or in the menu bar.

    After this it is not possible to continue working with Eagle even after the reader is closed. I have to restart the notebook and then I can continue.

     

    The same thing happens when I switch on the notebook, start Acrobat Reader, close it (or leave it open) and then start Eagle.

    Acrobat Reader version 10.1.6

     

    I hope this helps solving the problem.

     

    Regards

    Hermann

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wardelder
    wardelder over 13 years ago in reply to Krycek

    I just installed Eagle 6.4.0 on my second Win7 x64 machine and it works fine.  Both machines are laptops with Win7 x64.  One works, one fails (solid/repeatable failures).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Krycek
    Krycek over 13 years ago in reply to Krycek

    I have this exact same problem with the BETA 6.4.1 so it looks like it hasn't been addressed yet.

     

    Still using 6.3.0 here at work to over come this but I am being asked to start to roll out Eagle to new development engineers and the environment will be the same : Windows 7 64 bit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>