Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) APPCRASH EAGLE 6.4 on WIN 7 64
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 195 subscribers
  • Views 4952 views
  • Users 0 members are here
  • eagle
Related

APPCRASH EAGLE 6.4 on WIN 7 64

terje
terje over 13 years ago

Dear the support team at Cadsoft!

I have just purchased and installed Eagle pro shematic and layout package on to my brand new win 7 64 computer.

 

I'm now trying to design some new components with the library editor but every 3 to 10 minutes the application crashes and the work is lost.

To me it appears that the crash happens randomly. It can happen when I'm resizing the window, moving a element, copy a element, changing the grid. pushing the undo button  etc. etc.

For now the Eagle is useless as this happens too frequently.

 

The eagle program is installed under C:\eagle

The version is 6.4.0.

 

What did I do wrong?

 

Is this a known issue?

 

 

 

Windows crash report:

 

Problem event name: APPCRASH

Programname: eagle.exe

Programversion: 0.0.0.0

Timestamp for program: 50eaf0df

Error module name: ntdll.dll

Error module version: 6.1.7601.17725

Timestamp on error module: 4ec49b8f

Exeption code: c0000005

Exeption scew: 0002e3be

OS-versjon: 6.1.7601.2.1.0.256.48

ID for national setting: 1044

Additional information 1: 0a9e

Additional information2: 0a9e372d3b4ad19135b953a78882e789

Additional information3: 0a9e

Additional information4: 0a9e372d3b4ad19135b953a78882e789

 

 

 

Best Regards

Terje

  • Sign in to reply
  • Cancel
Parents
  • Mr.Pi
    Mr.Pi over 13 years ago

    Hi everybody.

     

    I am not using Windows 7 but I still have the same problems with Eagle crashing.

    I am using Windows XP SP3 and Eagle 6.4.0 free Version.

     

    Here is what I noticed:

    I switch on my notebook, start Eagle and work for hours without any problem.

    Then I start Acrobat Reader to open a data sheet or whatever and that is when the problem begins.

    Sometimes I can see Eagle disappear from  the task bar while Acrobat opens. Usually Eagle is closed without warning when I click on any of the icons or in the menu bar.

    After this it is not possible to continue working with Eagle even after the reader is closed. I have to restart the notebook and then I can continue.

     

    The same thing happens when I switch on the notebook, start Acrobat Reader, close it (or leave it open) and then start Eagle.

    Acrobat Reader version 10.1.6

     

    I hope this helps solving the problem.

     

    Regards

    Hermann

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Mr.Pi
    Mr.Pi over 13 years ago

    Hi everybody.

     

    I am not using Windows 7 but I still have the same problems with Eagle crashing.

    I am using Windows XP SP3 and Eagle 6.4.0 free Version.

     

    Here is what I noticed:

    I switch on my notebook, start Eagle and work for hours without any problem.

    Then I start Acrobat Reader to open a data sheet or whatever and that is when the problem begins.

    Sometimes I can see Eagle disappear from  the task bar while Acrobat opens. Usually Eagle is closed without warning when I click on any of the icons or in the menu bar.

    After this it is not possible to continue working with Eagle even after the reader is closed. I have to restart the notebook and then I can continue.

     

    The same thing happens when I switch on the notebook, start Acrobat Reader, close it (or leave it open) and then start Eagle.

    Acrobat Reader version 10.1.6

     

    I hope this helps solving the problem.

     

    Regards

    Hermann