Hi,
Top and bottom layers can be referred to by the built in constants
LAYER_TOP and LAYER_BOTTOM but how do you refer to inner layers?
Thanks.
Keith
Hi,
Top and bottom layers can be referred to by the built in constants
LAYER_TOP and LAYER_BOTTOM but how do you refer to inner layers?
Thanks.
Keith
Keith Raper wrote:
Hi,
Top and bottom layers can be referred to by the built in constants
LAYER_TOP and LAYER_BOTTOM but how do you refer to inner layers?
Thanks.
Keith
Route2
....
Route15
See HELP LAYER or the manual
--
Viewed / responded via the newsgroup at
news.cadsoft.de
On 24/01/2013 18:18, Warren Brayshaw wrote:
Keith Raper wrote:
Hi,
Top and bottom layers can be referred to by the built in constants
LAYER_TOP and LAYER_BOTTOM but how do you refer to inner layers?
Thanks.
Keith
Route2
....
Route15
See HELP LAYER or the manual
>
Warren,
Thanks for the reply but that doesn't work. The error is "unknown
identifier 'Route2'". If you use "LAYER_ROUTE2" you get "unknown
identifier 'LAYER_ROUTE2'" (and for pretty much any combination I have
been able to think of).
I haven't been able to find anything in the help or the manual about how
to refer to the inner layers in a ULP. For some reason it doesn't seem
to be the same as "name" or "Layer_name" normally used to refer to the
layer, even though "layer_top" and "layer_bottom" works.
Keith
Keith Raper wrote:
On 24/01/2013 18:18, Warren Brayshaw wrote:
Keith Raper wrote:
Hi,
Top and bottom layers can be referred to by the built in constants
LAYER_TOP and LAYER_BOTTOM but how do you refer to inner layers?
Thanks.
Keith
Route2
....
Route15
See HELP LAYER or the manual
Warren,
Thanks for the reply but that doesn't work. The error is "unknown
identifier 'Route2'". If you use "LAYER_ROUTE2" you get "unknown
identifier 'LAYER_ROUTE2'" (and for pretty much any combination I have
been able to think of).
I haven't been able to find anything in the help or the manual about
how to refer to the inner layers in a ULP. For some reason it
doesn't seem to be the same as "name" or "Layer_name" normally used
to refer to the layer, even though "layer_top" and "layer_bottom"
works.
Keith
Now I see what you are asking.
There are no constants for the inner layers. LAYER_TOP and LAYER_BOTTOM are
integer constants that return 1 and 16 respectively. That equates to their
layer numbers so just test for layer numbers or make up you own. Personally
in a ULP I simply test LAYER.NAME = = 2 or what ever I'm interested in .
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
On 22/02/2013 06:21, Warren Brayshaw wrote:
Keith
Now I see what you are asking.
There are no constants for the inner layers. LAYER_TOP and LAYER_BOTTOM are
integer constants that return 1 and 16 respectively. That equates to their
layer numbers so just test for layer numbers or make up you own. Personally
in a ULP I simply test LAYER.NAME = = 2 or what ever I'm interested in .
HTH
Warren
Warren,
Thanks. I was coming to the conclusion that there weren't built in
constants for the other layers. I need to read a bit more about the ULP
language to try to achieve what I want.
Keith
On 22/02/2013 06:21, Warren Brayshaw wrote:
Keith
Now I see what you are asking.
There are no constants for the inner layers. LAYER_TOP and LAYER_BOTTOM are
integer constants that return 1 and 16 respectively. That equates to their
layer numbers so just test for layer numbers or make up you own. Personally
in a ULP I simply test LAYER.NAME = = 2 or what ever I'm interested in .
HTH
Warren
Warren,
Thanks. I was coming to the conclusion that there weren't built in
constants for the other layers. I need to read a bit more about the ULP
language to try to achieve what I want.
Keith