Hi
I often work on boards with big difference in size of components.
This involves changing the grid size all the time.
The only thing i need is to be able on a hotkey to duble and half grid.
No need for gui parts just the command eg. GRID MUL2 and GRID DIV2
NOT to be confused with the multiplier in the grid menu that only changes the displaying in multiplums
I tryed to make a hot key for the grids i use the most but it becomes alot of keys to remember
insted of just two and i ended up back to changing in in the menu...
I belive that there was the posibility in some old version in the form of two buttons under grid settings but i am no sure.
I remember being anoid about a change in that menu...
As a programmer I cant see this taking more than an hour to implement and perhaps another to test posible problems.
Keep up the good work
I have been using Eagle more or less daily both in the free and pro version for some 10 years now.
And like it very much especially the going to XML format since this has opend op for using software dev. versioning tools like GIT, SVN or CVS.
We allready moved all our eagle projects in to GIT repositorys, meaning perfect version history throughout the project. Also takes care of merging
Librarys when two persons have added a component be fore sync'ing.
Best regards
Asbjørn Holland Christensen
Musalk