Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to manage composite parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1350 views
  • Users 0 members are here
Related

How to manage composite parts

autodeskguest
autodeskguest over 13 years ago

Hello,

 

sometime I have a part composed of multiple components.

Some examples:

 

- battery holder: two clips

- MCU module: two or more connectors

 

 

In the schematic is correct to have one symbol for the whole part. It

makes no sense to place two different clips (which must be placed at an

exact distance with the correct silkscreen info) o two different

connectors for the MCU module.

 

The downside is it's hard to manage and maintain the BOM because I will

get only one item rather than 2 or more. And the manufacturer code isn't

really applied to the whole part but to the single sub-items.

 

I wonder how you would handle this.

Thank you

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 13 years ago

    On 03/16/2013 10:31 AM, Marco Trapanese wrote:

    Hello,

     

    sometime I have a part composed of multiple components.

    Some examples:

     

    - battery holder: two clips

    - MCU module: two or more connectors

     

     

    In the schematic is correct to have one symbol for the whole part. It

    makes no sense to place two different clips (which must be placed at

    an exact distance with the correct silkscreen info) o two different

    connectors for the MCU module.

     

    The downside is it's hard to manage and maintain the BOM because I

    will get only one item rather than 2 or more. And the manufacturer

    code isn't really applied to the whole part but to the single sub-items.

     

    I wonder how you would handle this.

     

    It's called a sub-assembly.  But there's no direct way of handling this

    through Eagle.  In a full BOM, each assembly consists of one or more

    components, and one or more other assemblies, each of which would be

    referred to as a sub-assembly, forming a hierarchy.  The battery holder

    with two clips would be modeled as a single part in eagle, and in your

    BOM software it would be referenced as a sub-assembly.  The sub-assembly

    for this would be the two connectors.

     

    Going the other direction, your finished PCB is not the final product,

    but merely one sub-assembly.  The next higher level assembly may include

    the machined case in which the board is mounted, standoffs, hold down

    screws, buttons, switches, displays, labels, etc., forming your finished

    product assembly.  Going up one level higher, one can include the

    finished product (as a sub-assembly), packing materials (bubble wrap,

    peanuts), a unit container, and perhaps even a shipping container in a

    top-level assembly that one might call "as-shipped".

     

    A hierarchy such as this makes it easy to do a cost roll-up.

     

    As you can see, Eagle plays a small role in the overall BOM, but it does

    a pretty decent job detailing the PCB.  A model to consider is to create

    the battery holder with its two connectors as a single device in your

    library.  Then use attributes to specify the manufacturer's part numbers

    for the holder.

        MFGRPN1=12222

        MFGRPN2=2345

        ...

     

    You can modify the standard bom.ulp to also emit attributes of each

    part, even filtering out attributes that do not begin with "MFGRPN".

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to dukepro

    Il 16/03/2013 16:34, Chuck Huber ha scritto:

     

     

     

     

    Thank you for your clear answer.

     

     

    A hierarchy such as this makes it easy to do a cost roll-up.

     

    As you can see, Eagle plays a small role in the overall BOM, but it does

    a pretty decent job detailing the PCB.  A model to consider is to create

    the battery holder with its two connectors as a single device in your

    library.  Then use attributes to specify the manufacturer's part numbers

    for the holder.

         MFGRPN1=12222

         MFGRPN2=2345

         ...

     

    You can modify the standard bom.ulp to also emit attributes of each

    part, even filtering out attributes that do not begin with "MFGRPN".

     

     

    This could be fine but I'm afraid it would need a "three-dimensional" table.

     

    My own libraries have an attribute for each supplier's order code. I

    mean the part name (base name + technology + package) is actually the

    manufacturer code.

    Then I have several attributes, to store the order codes, i.e.:

     

    FARNELL=XXX

    MOUSER=YYY

    DIGIKEY=ZZZ

     

    in this way when I open my BOM in Excel it's easier to place orders.

     

    According to your hint I should add an attribute for each sub-part, but

    each sub-part itself should have the order codes for each supplier - no

    way image

     

     

    I think a smart ulp could do the trick:

     

    1. add an attribute for each sub-part with the exact EAGLE refs

    (sub-assembly prefix, gate, library, part, tech, package)

     

    2. export the BOM with attributes

     

    3. run a post-processing ULP that finds the sub-assembly prefix and

    explode the attributes adding rows to the BOM itself with the

    information read from the other libraries.

     

     

    Not very handy, indeed, but in this way there is no multiple data (e.g.

    the sub-parts information are stored only in the initial library) and

    the higher level of the sub-assembly is always up to date.

     

     

    Another big issue is the coherence of the designators.

    In the schematic it's correct to view the battery holder as, say, B1. In

    the BOM you will have the two sub-parts but the designator is still B1

    and the guys who will make the board will complain about this.

     

     

    Marco

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 13 years ago in reply to autodeskguest

    On 03/16/2013 12:07 PM, Marco Trapanese wrote:

    ...

     

    I think a smart ulp could do the trick:

     

    1. add an attribute for each sub-part with the exact EAGLE refs

    (sub-assembly prefix, gate, library, part, tech, package)

     

    2. export the BOM with attributes

     

    3. run a post-processing ULP that finds the sub-assembly prefix and

    explode the attributes adding rows to the BOM itself with the

    information read from the other libraries.

     

    True.  In the instances where I have sub-assemblies mounted on the

    board, I provide the assembly house with not only the PCB BOM, but also

    the BOM of the sub-assembly.  K1-DB on the main board, for example,

    would refer to a daughter board whose primary function is that of a

    relay (hence the 'K').  It has been assigned an internal part number.

     

    Then I provide a complete BOM for the daughter board, which contains K1,

    and a diode.

     

    In the example you provided, the battery holder B1 would be assigned

    your own internal part number (BXXX-DB), then the BOM would include the

    two connectors cited earlier.

     

    Thinking out loud for a moment, this would provide one side of the

    connector - that which is installed on the battery holder, but it still

    does not address the two mating connectors that you need on your main board.

     

    Suffice to say that the Eagle BOM is not the utopia of BOM's.  In fact,

    I have written a C program that imports the CSV produced by Eagle and

    load it into a MySQL database.  This same program also reads a

    supplementary file to add parts to or remove parts from the assembly.

    Components that are removed from what Eagle exports are test points

    (usually just SMD pads or holes), and spark gaps.  Other things to

    remove would be a bit more esoteric components such as controlled

    impedance resistors built on to the board.  After that, I use PHP

    scripts on an internal web server to access the assembly database from a

    browser.

     

    I'm not sure if ULP is the best way to go here.  Consider a language

    outside of Eagle - something that will readily import what Eagle

    produces then massage it from there.

     

    Enjoy,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to dukepro

    Il 16/03/2013 22:44, Chuck Huber ha scritto:

     

    True.  In the instances where I have sub-assemblies mounted on the

    board, I provide the assembly house with not only the PCB BOM, but also

    the BOM of the sub-assembly.  K1-DB on the main board, for example,

    would refer to a daughter board whose primary function is that of a

    relay (hence the 'K').  It has been assigned an internal part number.

     

    Then I provide a complete BOM for the daughter board, which contains K1,

    and a diode.

     

     

    This is exactly what I do usually. Manually.

    It would be nice to manage this in EAGLE directly, because if after two

    years you have to change something you will likely forget something...

     

     

    In the example you provided, the battery holder B1 would be assigned

    your own internal part number (BXXX-DB), then the BOM would include the

    two connectors cited earlier.

     

    Thinking out loud for a moment, this would provide one side of the

    connector - that which is installed on the battery holder, but it still

    does not address the two mating connectors that you need on your main board.

     

     

    Yes, this is the point. I instruct the the assembly house how to handle

    B1 but of course it's not very straightforward.

     

     

    Suffice to say that the Eagle BOM is not the utopia of BOM's.  In fact,

    I have written a C program that imports the CSV produced by Eagle and

    load it into a MySQL database.  This same program also reads a

    supplementary file to add parts to or remove parts from the assembly.

    Components that are removed from what Eagle exports are test points

    (usually just SMD pads or holes), and spark gaps.  Other things to

    remove would be a bit more esoteric components such as controlled

    impedance resistors built on to the board.  After that, I use PHP

    scripts on an internal web server to access the assembly database from a

    browser.

     

     

    I wrote a simple Excel macro do to this - it's the same thing.

     

     

    I'm not sure if ULP is the best way to go here.  Consider a language

    outside of Eagle - something that will readily import what Eagle

    produces then massage it from there.

     

     

    I was thinking about ULP because (I guessed) it would be easier to

    access the other libraries to extract the information of the other parts.

    But I was wrong... the lbr files are just plain xml files!

     

    When I will have some spare time I'll try to develop a simple C++

    application to improve the BOM.

     

    Anyway, if the CADSOFT's guys would like to help us adding some features

    we all will be very happy!

     

    Best regards

    Marco

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 13 years ago in reply to dukepro

    Il 16/03/2013 22:44, Chuck Huber ha scritto:

     

    True.  In the instances where I have sub-assemblies mounted on the

    board, I provide the assembly house with not only the PCB BOM, but also

    the BOM of the sub-assembly.  K1-DB on the main board, for example,

    would refer to a daughter board whose primary function is that of a

    relay (hence the 'K').  It has been assigned an internal part number.

     

    Then I provide a complete BOM for the daughter board, which contains K1,

    and a diode.

     

     

    This is exactly what I do usually. Manually.

    It would be nice to manage this in EAGLE directly, because if after two

    years you have to change something you will likely forget something...

     

     

    In the example you provided, the battery holder B1 would be assigned

    your own internal part number (BXXX-DB), then the BOM would include the

    two connectors cited earlier.

     

    Thinking out loud for a moment, this would provide one side of the

    connector - that which is installed on the battery holder, but it still

    does not address the two mating connectors that you need on your main board.

     

     

    Yes, this is the point. I instruct the the assembly house how to handle

    B1 but of course it's not very straightforward.

     

     

    Suffice to say that the Eagle BOM is not the utopia of BOM's.  In fact,

    I have written a C program that imports the CSV produced by Eagle and

    load it into a MySQL database.  This same program also reads a

    supplementary file to add parts to or remove parts from the assembly.

    Components that are removed from what Eagle exports are test points

    (usually just SMD pads or holes), and spark gaps.  Other things to

    remove would be a bit more esoteric components such as controlled

    impedance resistors built on to the board.  After that, I use PHP

    scripts on an internal web server to access the assembly database from a

    browser.

     

     

    I wrote a simple Excel macro do to this - it's the same thing.

     

     

    I'm not sure if ULP is the best way to go here.  Consider a language

    outside of Eagle - something that will readily import what Eagle

    produces then massage it from there.

     

     

    I was thinking about ULP because (I guessed) it would be easier to

    access the other libraries to extract the information of the other parts.

    But I was wrong... the lbr files are just plain xml files!

     

    When I will have some spare time I'll try to develop a simple C++

    application to improve the BOM.

     

    Anyway, if the CADSOFT's guys would like to help us adding some features

    we all will be very happy!

     

    Best regards

    Marco