I'm making a symbol for the QFN20 and SSOP24 variants of the Silicon Laboratories Si473x family devices.
Apart from the SSOP having more NC and earth pins (which I can connect as duplicates), there's an extra pin (DYBP) on the SSOP which isn't brought out on the QFN. If I add this pin to the device, I get errors using the QFN package because it isn't connected. Likewise the PAD on the QFN doesn't exist on the SSOP, so same problem in reverse.
Is it possible to have a pin in a device which is not available in all package variants? How?
Or do I have to make separate devices for these?
Clifford Heath.