Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Create device with a package that doesn't connect all pins?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 187 subscribers
  • Views 422 views
  • Users 0 members are here
Related

Create device with a package that doesn't connect all pins?

autodeskguest
autodeskguest over 13 years ago

I'm making a symbol for the QFN20 and SSOP24 variants of the Silicon Laboratories Si473x family devices.

 

Apart from the SSOP having more NC and earth pins (which I can connect as duplicates), there's an extra pin (DYBP) on the SSOP which isn't brought out on the QFN. If I add this pin to the device, I get errors using the QFN package because it isn't connected. Likewise the PAD on the QFN doesn't exist on the SSOP, so same problem in reverse.

 

Is it possible to have a pin in a device which is not available in all package variants? How?

Or do I have to make separate devices for these?

 

 

Clifford Heath.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 13 years ago

    On 4/7/2013 7:08 AM, Clifford Heath wrote:

    I'm making a symbol for the QFN20 and SSOP24 variants of the Silicon

    Laboratories Si473x family devices.

     

    Apart from the SSOP having more NC and earth pins (which I can connect

    as duplicates), there's an extra pin (DYBP) on the SSOP which isn't

    brought out on the QFN. If I add this pin to the device, I get errors

    using the QFN package because it isn't connected. Likewise the PAD on

    the QFN doesn't exist on the SSOP, so same problem in reverse.

     

    Is it possible to have a pin in a device which is not available in all

    package variants? How?

    Or do I have to make separate devices for these?

     

     

    Clifford Heath.

     

    Hi Cliff,

     

    I hope you're doing well, you would have to make seperate devices for

    this. Currently EAGLE only allows one symbol per device and there are no

    provisions for altering the symbol based on package.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    On 04/09/13 04:31, Jorge Garcia wrote:

    On 4/7/2013 7:08 AM, Clifford Heath wrote:

    I'm making a symbol for the QFN20 and SSOP24 variants of the Silicon

    Laboratories Si473x family devices.

     

    Apart from the SSOP having more NC and earth pins (which I can connect

    as duplicates), there's an extra pin (DYBP) on the SSOP which isn't

    brought out on the QFN. If I add this pin to the device, I get errors

    using the QFN package because it isn't connected. Likewise the PAD on

    the QFN doesn't exist on the SSOP, so same problem in reverse.

     

    Is it possible to have a pin in a device which is not available in all

    package variants? How?

    Or do I have to make separate devices for these?

     

     

    Clifford Heath.

     

    Hi Cliff,

     

    I hope you're doing well, you would have to make seperate devices for this. Currently EAGLE only allows one symbol per device and there are no provisions for altering the symbol based on package.

     

     

    Ok, that's a shame. It would be good to have a pin connection status of "unavailable",

    then the same symbol could be used for the different packages - as long as unavailable

    pins weren't connected in the schematic.

     

    Thanks for your help anyhow!

     

    Clifford Heath.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    On 04/09/13 04:31, Jorge Garcia wrote:

    On 4/7/2013 7:08 AM, Clifford Heath wrote:

    I'm making a symbol for the QFN20 and SSOP24 variants of the Silicon

    Laboratories Si473x family devices.

     

    Apart from the SSOP having more NC and earth pins (which I can connect

    as duplicates), there's an extra pin (DYBP) on the SSOP which isn't

    brought out on the QFN. If I add this pin to the device, I get errors

    using the QFN package because it isn't connected. Likewise the PAD on

    the QFN doesn't exist on the SSOP, so same problem in reverse.

     

    Is it possible to have a pin in a device which is not available in all

    package variants? How?

    Or do I have to make separate devices for these?

     

     

    Clifford Heath.

     

    Hi Cliff,

     

    I hope you're doing well, you would have to make seperate devices for this. Currently EAGLE only allows one symbol per device and there are no provisions for altering the symbol based on package.

     

     

    Ok, that's a shame. It would be good to have a pin connection status of "unavailable",

    then the same symbol could be used for the different packages - as long as unavailable

    pins weren't connected in the schematic.

     

    Thanks for your help anyhow!

     

    Clifford Heath.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    Il 10/04/2013 03:48, Clifford Heath ha scritto:

     

    Ok, that's a shame. It would be good to have a pin connection status of

    "unavailable",

    then the same symbol could be used for the different packages - as long

    as unavailable

    pins weren't connected in the schematic.

     

     

    I agree.

    I hope CADSOFT would add at least this small feature, even if it hasn't

    any plan to support multiple symbols.

     

     

    Marco