Hello,
EAGLE assumes that any part name is composed in the following way:
BASE_NAME|TECHNOLOGY|PACKAGE
some parts come with another order:
BASE_NAME|PACKAGE|TECHNOLOGY
How to handle this?
Thanks
Marco
Hello,
EAGLE assumes that any part name is composed in the following way:
BASE_NAME|TECHNOLOGY|PACKAGE
some parts come with another order:
BASE_NAME|PACKAGE|TECHNOLOGY
How to handle this?
Thanks
Marco
Marco Trapanese schrieb:
EAGLE assumes that any part name is composed in the following way:
BASE_NAME|TECHNOLOGY|PACKAGE
some parts come with another order:
BASE_NAME|PACKAGE|TECHNOLOGY
How to handle this?
IMHO, the "technology" is absolutely senseless/useless anyway. You get
the same effect just by setting a proper VALUE.
So all my libraries contain devices that are as generic as possible, and
none of them uses "technology". When putting them into the schematic, I
assign a meaningful value, and all is done.
Tilmann
Il 08/04/2013 13:44, Tilmann Reh ha scritto:
IMHO, the "technology" is absolutely senseless/useless anyway. You get
the same effect just by setting a proper VALUE.
So all my libraries contain devices that are as generic as possible, and
none of them uses "technology". When putting them into the schematic, I
assign a meaningful value, and all is done.
My experience is different than yours. The technology field (since EAGLE
supports the "append" features for pin/pad) is very useful for me to
take care of the small differences among parts.
For example the C/I designator for temperature ranges is properly
handled with the technology fields, allowing you to have ONE part in the
library. Or think about an LDO or TVS family: they could have dozen of
different voltages. Each one with its own order code.
If you don't use the technology fields you must create a different part
for every variant!
The best would be to define the "part name" according to the
manufacturer specifications. But I admit this could be quite complex to
implement.
Marco
Marco Trapanese schrieb:
IMHO, the "technology" is absolutely senseless/useless anyway. You get
the same effect just by setting a proper VALUE.
So all my libraries contain devices that are as generic as possible, and
none of them uses "technology". When putting them into the schematic, I
assign a meaningful value, and all is done.
My experience is different than yours. The technology field (since EAGLE
supports the "append" features for pin/pad) is very useful for me to
take care of the small differences among parts.
For example the C/I designator for temperature ranges is properly
handled with the technology fields, allowing you to have ONE part in the
library. Or think about an LDO or TVS family: they could have dozen of
different voltages. Each one with its own order code.
If you don't use the technology fields you must create a different part
for every variant!
That's exactly what is not necessary.
Different temperature ranges, different regulator voltages etc. can
perfectly be handled just with different VALUES.
For example, a generic voltage regulator is "78xx", for any 7800 series
(or similar) three-pin positive regulator - with package variants for
TO220 (vertical and horizontal), TO92, DPAK, D2PAK etc..
In the schematic, simply pick it (with the right package variant), then
assign the proper value (like 7805, 78L12 - or even LP2950-3.3).
Or, for TVS diodes: we use one single device, with a few package
variants (some common THT sizes, SMA, SMB, SMC) - and then set a proper
value (like P6SMB15CAT3GP6SMB15CAT3G, for example).
Of course you need to take care - don't assign an LP2950 to a TO220
package. But as developer, you need to take care anyway, and for much
more subtle details...
The best would be to define the "part name" according to the
manufacturer specifications. But I admit this could be quite complex to
implement.
No, it's quite easy: use the part name provided by the manufacturer AS
VALUE.
Tilmann
Marco Trapanese schrieb:
In the past I did exactly that.
It was fine until I had to go in production. Who mounts the boards ask
me not only the part value but also the order codes from suppliers
(Farnell, Mouser, Digikey).
I store them in the attributes and the BOM is ready in a while.
Following your method I must write the order codes every time by hand.
Yes. However, very many standard components don't require special order
codes for particular suppliers - you buy them where you get them (or
where you place an order anyway). So creating a BOM isn't that hard (we
also use an ULP that does most of the work). There always are only a few
parts that really need to be specified in more detail.
Otherwise, you need trillions of different devices for basically the
same part. Just one more example: a simple 470/35 capacitor, for me it's
just a 10 mm diameter part. Depending on the circuit, it needs to be a
standard capacitor (brand doesn't matter), or some special low-ESR type,
or eventually a special high-temperature type. Sometimes, height also is
an issue. Using attributes and order codes, you'd need about a dozen
different devices just for this single capacitor (and the same amount
for every other C/U combination) - while opposed to this, our generic 10
mm device suits about a dozen different C/U combinations including all
particular types and brands (which are remarked in the value, if necessary).
Finally, it's your decision if you want to put more effort on creating a
BOM - or on maintaining bloated libraries and keeping the design files
in sync with them.
Tilmann
Il 08/04/2013 15:10, Tilmann Reh ha scritto:
That's exactly what is not necessary.
Different temperature ranges, different regulator voltages etc. can
perfectly be handled just with different VALUES.
For example, a generic voltage regulator is "78xx", for any 7800 series
(or similar) three-pin positive regulator - with package variants for
TO220 (vertical and horizontal), TO92, DPAK, D2PAK etc..
In the schematic, simply pick it (with the right package variant), then
assign the proper value (like 7805, 78L12 - or even LP2950-3.3).
Or, for TVS diodes: we use one single device, with a few package
variants (some common THT sizes, SMA, SMB, SMC) - and then set a proper
value (like P6SMB15CAT3GP6SMB15CAT3G, for example).
In the past I did exactly that.
It was fine until I had to go in production. Who mounts the boards ask
me not only the part value but also the order codes from suppliers
(Farnell, Mouser, Digikey).
I store them in the attributes and the BOM is ready in a while.
Following your method I must write the order codes every time by hand.
Am I wrong?
Marco
René König schrieb:
Different temperature ranges, different regulator voltages etc. can
perfectly be handled just with different VALUES.
And the ATTRIBUTEs are probably different as well, or do you even have a
generic ATTRIBUTE-set? Or don't you use ATTRIBUTEs at all? I simply
cannot imagine me entering all the necessary ATTRIBUTEs over and over
again...
Exactly: I also don't use attributes at all.
KISS principle.
Tilmann
René König schrieb:
Different temperature ranges, different regulator voltages etc. can
perfectly be handled just with different VALUES.
And the ATTRIBUTEs are probably different as well, or do you even have a
generic ATTRIBUTE-set? Or don't you use ATTRIBUTEs at all? I simply
cannot imagine me entering all the necessary ATTRIBUTEs over and over
again...
Exactly: I also don't use attributes at all.
KISS principle.
Tilmann