Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 6.4.0: extremely slow conversion of big libraries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 858 views
  • Users 0 members are here
Related

Eagle 6.4.0: extremely slow conversion of big libraries

CalebCZ
CalebCZ over 13 years ago

Not sure if it is bug or just extreme code inefficiency, but conversion of big libraries to new XML format takes very long time in Eagle 6.4.0 (on Windows 7 64-bit). For example, this 10 MB library takes about 14 minutes image to open on Core i7 processor at 3.2 GHz:

 

http://www.cadsoftusa.com/downloads/file/xilinx_devices_105.zip

 

In fact, I thought Eagle simply freezed (locked up) at first. But then I left it going over my lunch break and when I returned, the library was converted. After I saved it in XML format, the library bloated to 40 MB, but seems to work OK. Still, I don't think such a long conversion time is normal, especially when a bit smaller (around 1 MB) libraries convert in some 4 seconds on the same PC.

 

I tried this on two different PC (the other running Windows XP 32-bit), but it is the same on both.

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to CalebCZ

    On 4/11/2013 5:09 AM, Caleb Dead wrote:

    I see. Well, if you fail to speed it up considerably, please at least

    let the user know that the conversion is in progress (possibly with

    typical "percentage left" bar?). Like I said, I thought Eagle locked up

    at first and it was sheer luck I left the conversion run so long.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/73850#73850

     

     

    Hi Caleb,

     

    That is an excellent idea. So far this is the only library I've run into

    that takes so long. Granted it's probably one of the largest libraries

    up on our website.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CalebCZ
    CalebCZ over 13 years ago in reply to autodeskguest

    I see. Well, if you fail to speed it up considerably, please at least let the user know that the conversion is in progress (possibly with typical "percentage left" bar?). Like I said, I thought Eagle locked up at first and it was sheer luck I left the conversion run so long.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago

    On 4/10/2013 7:17 AM, Caleb Dead wrote:

    Not sure if it is bug or just extreme code inefficiency, but conversion

    of big libraries to new XML format takes very long time in Eagle 6.4.0

    (on Windows 7 64-bit). For example, this 10 MB library takes about 14

    minutes image to open on Core i7 processor at 3.2 GHz:

     

    http://www.cadsoftusa.com/downloads/file/xilinx_devices_105.zip

     

    In fact, I thought Eagle simply freezed (locked up) at first. But then I

    left it going over my lunch break and when I returned, the library was

    converted. After I saved it in XML format, the library bloated to 40 MB,

    but seems to work OK. Still, I don't think such a long conversion time

    is normal, especially when a bit smaller (around 1 MB) libraries convert

    in some 2 seconds on the same PC.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/73798#73798

     

    Hi Caleb,

     

    I hope you're doing well. That's a very comprehensive library of Xilinx

    devices and it takes a while to perform the initial conversion from the

    closed binary format to XML. Once it's in XML format it opens much faster.

     

    File sizes did increase by going to XML about 4x which is what you

    experienced. In this age of terabyte hard drives we figured it was a

    good trade off for the convenience of the XML. When dealing with large

    libraries this for now is the norm, it's not a bug. We're looking into

    ways of speeding up these operations for a future release.

     

    hth,

    Jorge Garcia