Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) EAGLE GUI (12): Making things easier for new users
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 191 subscribers
  • Views 2996 views
  • Users 0 members are here
Related

EAGLE GUI (12): Making things easier for new users

autodeskguest
autodeskguest over 13 years ago

Though the user interface of EAGLE is trimmed for doing things QUICKLY

and EFFECTIVELY, the difference between its own GUI and (de-facto

standard) Office-like programs makes it increasingly difficult for

'newbies' to accept the program as something really useful (as seen in

previous posts). With a little bit of time, people see that EAGLE's GUI

is not complete rubbish, but just DIFFERENT, and learn to accept it as

useful. But often, the FIRST IMPRESSION counts.

 

In order to loose neither professional long-term users nor potential new

customers, CadSoft would be well-advised to try to connect both worlds

(EAGLE and Office).

 

The main points critisised in the forums seem to be

  - the lacking possibility to SELECT objects,

  - the lacking possibility to DO things with those objects and

  - the lacking possibility to GROUP objects.

(Though EAGLE does NOT lack some of the above points and does not NEED

the others, this is often the first impression of new users, so I just

leave that uncommented for now)

 

The following paragraphs suggest a way how CadSoft might implement ONE

additional command to make the first-time user much more happy than at

the moment:

 

  1. Prelude A: Make all current commands work properly with either

     single objects or groups. This mainly concerns

      - MOVE/COPY/INVOKE etc., which do not work with only ONE

        (ungrouped) object across sheets,

      - VALUE, which does not work with groups and

      - INFO, which does not work for groups, either.

     This obviously is quite a bit of work, but it would make the

     interface MUCH more logical.

  2. Prelude B: Make the INFO dialog NON-modal and add the possibility

     to anchor it somewhere in a window border. For the current EAGLE

     behaviour, that doesn't make too much sense, but the whole thing

     becomes useful when reading the next points.

  3. Prelude C: Make the GROUP command also accept dragging rectangles

     together with CTRL: This would add the selected objects to the

     group (or remove them from it).

  4. Add ONE command that is started with a button with a POINTER ARROW

     on it. This is what newbies use for 'selecting things'. This

     command will be QUITE difficult to implement, because it does

     QUITE a lot of things:

      a) If the user clicks a point where there is NO object available,

         the current group is emptied, and the (non-modal) INFO dialog

         shows nothing useful.

      b) If the user clicks on an object, this object gets the SOLE

         member of a (highlighted) group, and the INFO dialog shows the

         usual things (editable, with an 'accept' button or similar).

      c) If the user ctrl-clicks an object, this object is added to

         or subtracted from the current group. The INFO dialog shows

         only those fields that are available for ALL grouped

         objects. If a field is the same for ALL grouped objects,

         this field contains the common value, if NOT all objects

         agree, the field is left empty or a word like 'several' (or

         similar) is shown (checkboxes etc. would need TRISTATE

         support). The INFO fields are all editable (therefore,

         point 2 is crucial).

      d) If the user drags a rectangle beginning at a place where

         there is NO object, the command behaves the same as GROUP:

         Either a new group is created, or objects are added to or

         removed from it. The INFO dialog always stays working.

     Up to now, the new command does more or less the same as

     GROUP - it just cannot select objects with a polygon. But now

     some additional functionality:

      e) If the mouse button is pressed on an object from the current

         group and the mouse is then dragged, the group is MOVED (as

         is the case with nearly all graphics programs). I would

         suggest that this movement is triggered by the LEFT mouse

         button, even though 'normally', the RIGHT mouse button

         would move the group. BUT we want to have Office-like

         functionality here, and it should STILL be possible to

         rotate and/or mirror the group.

      f) Double-clicking on an object from a group shows the INFO

         dialog (non-modal), even if it wasn't visible previously.

      g) When double-clicking on an object NOT in the group, this

         object gets the SOLE member of a new group, and the INFO

         dialog is made visible.

      h) (Ctrl)-right-clicking on an object from the group shows

         a local menu based on the GROUP (and not only the clicked

         OBJECT as done now).

     With this approach, NEW users would have their often-sought

     'selecting' method, and even long-time users could do moving

     easier than before, because no change between group/move etc.

     would be necessary. For SPECIAL wishes like grouping with a

     polygon, the 'usual' commands would of course still work

     (and even without ANY change).

  5. Other thoughts:

      a) Since the word GROUP is normally used for PERSISTENT

         groups in every graphics program on earth, it MIGHT be

         useful to rename GROUP to SELECTION (the old command

         name would of course STILL work for compatibility).

      b) Currently, the INFO dialog does NOT focus any edit

         field after opening (which I always find a nuisance).

         In the future, it would be nice if the MOST OBVIOUS

         field would be automatically focused:

          - In case of all objects of the group containing

            the field that was LAST focused, use this.

          - In case of NO previous focus, use the field that

            the user will most likely want to EDIT. For

            components: value, for nets/busses: name, for

            wires: width, ...

      c) Since the new 'pointer' command does not do ANYTHING

         that cannot already be done with other EAGLE commands,

         but just allows to use them more quickly (and perhaps

         even more intuitively), there would be NO necessity

         to include this in the command line syntax. Well,

         STARTING the command via the command line would be very

         useful, but please NO additional parameters (they would

         be too complicated and useless, anyway).

      d) Prelude A needs QUITE some thinking about how existing

         commands should behave when confronted with groups.

         This is NOT difficult programming, though. SOME ideas

         for this should already have been mentioned in previous

         EAGLE GUI posts of mine (as far as I remember).

 

The above approach would do several things:

  - NOT break the current EAGLE workflow (which is much BETTER

    than Office-style stuff)

  - But ALLOW for Office-like usage for the most-often used

    functions like 'selecting', moving and changing parameters,

    meaning those functions that new users will most likely

    try out first

  - WITHOUT having to reprogram the whole of EAGLE, but just

    adding ONE (quite complex) command.

  - In my opinion, a win-win situation for both newbies and

    professionals. The only ones weeping will probably be the

    CadSoft programmers - but they are quite definitely the

    minority...

 

Andreas Weidner

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 13 years ago

    Andreas Weidner wrote on Wed, 10 April 2013 16:34

    <snip>

      2. Prelude B: Make the INFO dialog NON-modal and add the possibility

         to anchor it somewhere in a window border. For the current EAGLE

         behaviour, that doesn't make too much sense, but the whole thing

         becomes useful when reading the next points.

    <snip>

     

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.  Don't tell me that you can't name something when I change the name

    there, simply run the name command in the background and do it.  I also

    want to be able to dock that dialog or have it float so I can manage my

    screen real estate dynamically.

     

    It would also be nice if that info dialog could include some real-time info

    on the design, like number of unrouted airwires in the PCB and have it

    update as you route (you know when you collapse an airwire).

     

    To be orthogonal, the errors dialog should be able to made non-modal and

    dockable as well.  Sometimes I want that to be permanently visible.

     

    Cheers,

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.

     

    Also ACK here. Especially the attributes.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.

     

    Also ACK here. Especially the attributes.