Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) EAGLE GUI (12): Making things easier for new users
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 191 subscribers
  • Views 2994 views
  • Users 0 members are here
Related

EAGLE GUI (12): Making things easier for new users

autodeskguest
autodeskguest over 13 years ago

Though the user interface of EAGLE is trimmed for doing things QUICKLY

and EFFECTIVELY, the difference between its own GUI and (de-facto

standard) Office-like programs makes it increasingly difficult for

'newbies' to accept the program as something really useful (as seen in

previous posts). With a little bit of time, people see that EAGLE's GUI

is not complete rubbish, but just DIFFERENT, and learn to accept it as

useful. But often, the FIRST IMPRESSION counts.

 

In order to loose neither professional long-term users nor potential new

customers, CadSoft would be well-advised to try to connect both worlds

(EAGLE and Office).

 

The main points critisised in the forums seem to be

  - the lacking possibility to SELECT objects,

  - the lacking possibility to DO things with those objects and

  - the lacking possibility to GROUP objects.

(Though EAGLE does NOT lack some of the above points and does not NEED

the others, this is often the first impression of new users, so I just

leave that uncommented for now)

 

The following paragraphs suggest a way how CadSoft might implement ONE

additional command to make the first-time user much more happy than at

the moment:

 

  1. Prelude A: Make all current commands work properly with either

     single objects or groups. This mainly concerns

      - MOVE/COPY/INVOKE etc., which do not work with only ONE

        (ungrouped) object across sheets,

      - VALUE, which does not work with groups and

      - INFO, which does not work for groups, either.

     This obviously is quite a bit of work, but it would make the

     interface MUCH more logical.

  2. Prelude B: Make the INFO dialog NON-modal and add the possibility

     to anchor it somewhere in a window border. For the current EAGLE

     behaviour, that doesn't make too much sense, but the whole thing

     becomes useful when reading the next points.

  3. Prelude C: Make the GROUP command also accept dragging rectangles

     together with CTRL: This would add the selected objects to the

     group (or remove them from it).

  4. Add ONE command that is started with a button with a POINTER ARROW

     on it. This is what newbies use for 'selecting things'. This

     command will be QUITE difficult to implement, because it does

     QUITE a lot of things:

      a) If the user clicks a point where there is NO object available,

         the current group is emptied, and the (non-modal) INFO dialog

         shows nothing useful.

      b) If the user clicks on an object, this object gets the SOLE

         member of a (highlighted) group, and the INFO dialog shows the

         usual things (editable, with an 'accept' button or similar).

      c) If the user ctrl-clicks an object, this object is added to

         or subtracted from the current group. The INFO dialog shows

         only those fields that are available for ALL grouped

         objects. If a field is the same for ALL grouped objects,

         this field contains the common value, if NOT all objects

         agree, the field is left empty or a word like 'several' (or

         similar) is shown (checkboxes etc. would need TRISTATE

         support). The INFO fields are all editable (therefore,

         point 2 is crucial).

      d) If the user drags a rectangle beginning at a place where

         there is NO object, the command behaves the same as GROUP:

         Either a new group is created, or objects are added to or

         removed from it. The INFO dialog always stays working.

     Up to now, the new command does more or less the same as

     GROUP - it just cannot select objects with a polygon. But now

     some additional functionality:

      e) If the mouse button is pressed on an object from the current

         group and the mouse is then dragged, the group is MOVED (as

         is the case with nearly all graphics programs). I would

         suggest that this movement is triggered by the LEFT mouse

         button, even though 'normally', the RIGHT mouse button

         would move the group. BUT we want to have Office-like

         functionality here, and it should STILL be possible to

         rotate and/or mirror the group.

      f) Double-clicking on an object from a group shows the INFO

         dialog (non-modal), even if it wasn't visible previously.

      g) When double-clicking on an object NOT in the group, this

         object gets the SOLE member of a new group, and the INFO

         dialog is made visible.

      h) (Ctrl)-right-clicking on an object from the group shows

         a local menu based on the GROUP (and not only the clicked

         OBJECT as done now).

     With this approach, NEW users would have their often-sought

     'selecting' method, and even long-time users could do moving

     easier than before, because no change between group/move etc.

     would be necessary. For SPECIAL wishes like grouping with a

     polygon, the 'usual' commands would of course still work

     (and even without ANY change).

  5. Other thoughts:

      a) Since the word GROUP is normally used for PERSISTENT

         groups in every graphics program on earth, it MIGHT be

         useful to rename GROUP to SELECTION (the old command

         name would of course STILL work for compatibility).

      b) Currently, the INFO dialog does NOT focus any edit

         field after opening (which I always find a nuisance).

         In the future, it would be nice if the MOST OBVIOUS

         field would be automatically focused:

          - In case of all objects of the group containing

            the field that was LAST focused, use this.

          - In case of NO previous focus, use the field that

            the user will most likely want to EDIT. For

            components: value, for nets/busses: name, for

            wires: width, ...

      c) Since the new 'pointer' command does not do ANYTHING

         that cannot already be done with other EAGLE commands,

         but just allows to use them more quickly (and perhaps

         even more intuitively), there would be NO necessity

         to include this in the command line syntax. Well,

         STARTING the command via the command line would be very

         useful, but please NO additional parameters (they would

         be too complicated and useless, anyway).

      d) Prelude A needs QUITE some thinking about how existing

         commands should behave when confronted with groups.

         This is NOT difficult programming, though. SOME ideas

         for this should already have been mentioned in previous

         EAGLE GUI posts of mine (as far as I remember).

 

The above approach would do several things:

  - NOT break the current EAGLE workflow (which is much BETTER

    than Office-style stuff)

  - But ALLOW for Office-like usage for the most-often used

    functions like 'selecting', moving and changing parameters,

    meaning those functions that new users will most likely

    try out first

  - WITHOUT having to reprogram the whole of EAGLE, but just

    adding ONE (quite complex) command.

  - In my opinion, a win-win situation for both newbies and

    professionals. The only ones weeping will probably be the

    CadSoft programmers - but they are quite definitely the

    minority...

 

Andreas Weidner

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to CSWalt

     

    "Walter Spermann" <Walter.Spermann@cadsoft.de> a écrit dans le message de news:

    kklml6$7bg$1@cheetah.cadsoft.de...

    Hi James,

     

    On 04/16/13 21:05, James Morrison wrote:

    Andreas Weidner wrote on Wed, 10 April 2013 16:34

    <snip>

      2. Prelude B: Make the INFO dialog NON-modal and add the possibility

         to anchor it somewhere in a window border. For the current EAGLE

         behaviour, that doesn't make too much sense, but the whole thing

         becomes useful when reading the next points.

    <snip>

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.  Don't tell me that you can't name something when I change the name

    there, simply run the name command in the background and do it.  I also

    want to be able to dock that dialog or have it float so I can manage my

    screen real estate dynamically.

     

    It would also be nice if that info dialog could include some real-time info

    on the design, like number of unrouted airwires in the PCB and have it

    update as you route (you know when you collapse an airwire).

     

    To be orthogonal, the errors dialog should be able to made non-modal and

    dockable as well.  Sometimes I want that to be permanently visible.

     

    actually both our ERC and DRC error dialogs are non-modal, but not dockable !

     

    Please! non-modal dialog-box also for ULP's

     

    Regards,

    Walter Spermann

     

    Cheers,

     

    James.

     

     

    --

    ---------------------------------------------------------------

    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    ---------------------------------------------------------------

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    ---------------------------------------------------------------

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 13 years ago in reply to autodeskguest

    Hi James,

     

    On 04/16/13 21:05, James Morrison wrote:

    Andreas Weidner wrote on Wed, 10 April 2013 16:34

    <snip>

      2. Prelude B: Make the INFO dialog NON-modal and add the possibility

         to anchor it somewhere in a window border. For the current EAGLE

         behaviour, that doesn't make too much sense, but the whole thing

         becomes useful when reading the next points.

    <snip>

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.  Don't tell me that you can't name something when I change the name

    there, simply run the name command in the background and do it.  I also

    want to be able to dock that dialog or have it float so I can manage my

    screen real estate dynamically.

     

    It would also be nice if that info dialog could include some real-time info

    on the design, like number of unrouted airwires in the PCB and have it

    update as you route (you know when you collapse an airwire).

     

    To be orthogonal, the errors dialog should be able to made non-modal and

    dockable as well.  Sometimes I want that to be permanently visible.

     

    actually both our ERC and DRC error dialogs are non-modal, but not dockable !

     

    Regards,

    Walter Spermann

     

    Cheers,

     

    James.

     

     

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.

     

    Also ACK here. Especially the attributes.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skyflyrr
    skyflyrr over 13 years ago in reply to autodeskguest

    Unfortunately running so many ULP's for what in many caes should be menu items is making Eagle more of a hobby program rather than a professional program. I totally can see your point that ULP's allow many to have custom functions, be able to write functions they need, etc. In our case we just cannot do that. I always recall when DOS was first out and the fun we all had writing programs. These days many of us need programs that are productive right out of the box. That is what I need now for our company. I like Eagle very much and certainly cost was a large factor in our purchase decision, which is why I keep asking for menu functions rather than ULP's.

     

    The comments that started this conversation regarding groups etc are things I sorely need to be part of the main Eagle program. I hope they are available in a future version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to CSWalt

    Am 16.04.2013 10:45, schrieb Walter Spermann:

    Yes. Though it IS possible to use the command line for the infamous

    "value 100n", you still need to click on EVERY capacitor. For typical

    boards, we have about >50 of those, and ALL on the same sheet. Same

    thing with diode matrices and "1N4148" etc.

    OK, convinced !

     

    If more or less ALL commands could work with groups, there would even be

    an additional plus later on: This would finally make SEARCH or FIND

    tools much more useful - these could just GROUP all found objects, and

    then the user could even DO things with them...

     

    I don't think there are many editors who can actually ADD rectangular regions,

    at least I don't know anyone.

     

    Hmmm, strange: EVERY vector graphics program I encountered during the

    last 20 years (GEM Artline, CorelDraw, Professional Draw, MicrografX

    Designer, Adobe Illustrator, Deneba Canvas, Aldus Freehand, AutoSketch,

    InkScape, DrawPlus, OpenDraw, Tenado CAD - to just name a few of them)

    supports that with its pointer (selection) tool. Most of them with

    SHIFT, some with CTRL, but definitely ALL of them...

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago

    Andreas Weidner wrote on Wed, 10 April 2013 16:34

    <snip>

      2. Prelude B: Make the INFO dialog NON-modal and add the possibility

         to anchor it somewhere in a window border. For the current EAGLE

         behaviour, that doesn't make too much sense, but the whole thing

         becomes useful when reading the next points.

    <snip>

     

     

    Full ack Andreas.  And make ALL of the fields editable from that non-modal

    dialog.  Don't tell me that you can't name something when I change the name

    there, simply run the name command in the background and do it.  I also

    want to be able to dock that dialog or have it float so I can manage my

    screen real estate dynamically.

     

    It would also be nice if that info dialog could include some real-time info

    on the design, like number of unrouted airwires in the PCB and have it

    update as you route (you know when you collapse an airwire).

     

    To be orthogonal, the errors dialog should be able to made non-modal and

    dockable as well.  Sometimes I want that to be permanently visible.

     

    Cheers,

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    Markus Rudolf wrote on Tue, 16 April 2013 14:32

    On 16.04.2013 18:23, Jorge Garcia wrote:

     

    We already have some ULPs running as menu items. The issue is that

    not

    everything can and should be a menu item. A lot of what EAGLE can

    do

    simply wouldn't be possible without ULPs. We don't have a lot of

    developers to implement many of the features users request,

    allowing

    users to develop custom functionality that suits there individual

    tastes

    is a win for the individual user and for others who have had

    similar ideas.

     

    Additionally it's not very difficult to make a ULP a shortcut or

    custom

    button in the text menu look at the designlink and LTSpice ULPs and

    how

    they're exposed in the tool bar.

     

    I agree that some stuff is more elegant in an ULP.

     

    But I was talking about making a command applicable to a group. For my

     

    understanding every command should be applicable to groups, even if you

     

    might not see the need for it in the very first moment.

     

     

    I agree and go even further--all commands should be orthogonal i.e. they

    all operate the same way in general.  The fact that some work on groups and

    others don't is confusing, and in many cases, frustrating.  Other examples

    of non-orthogonal behaviour:

     

    rename doesn't work on technologies in a device

    lock doesn't work on raw objects

    editing name doesn't work from the info box but editing (x,y) end location

    does

     

    Cheers,

     

    James.

     

     

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    On 16.04.2013 18:23, Jorge Garcia wrote:

     

    We already have some ULPs running as menu items. The issue is that not

    everything can and should be a menu item. A lot of what EAGLE can do

    simply wouldn't be possible without ULPs. We don't have a lot of

    developers to implement many of the features users request, allowing

    users to develop custom functionality that suits there individual tastes

    is a win for the individual user and for others who have had similar ideas.

     

    Additionally it's not very difficult to make a ULP a shortcut or custom

    button in the text menu look at the designlink and LTSpice ULPs and how

    they're exposed in the tool bar.

     

    I agree that some stuff is more elegant in an ULP.

     

    But I was talking about making a command applicable to a group. For my

    understanding every command should be applicable to groups, even if you

    might not see the need for it in the very first moment.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    On 4/16/2013 12:31 AM, Markus Rudolf wrote:

    On 15.04.2013 22:59, Bob Moreno wrote:

    However why do we need to run so many external programs? These functions

    should be available within Eagle as menu items.

     

    Thats what I always say....

     

    We already have some ULPs running as menu items. The issue is that not

    everything can and should be a menu item. A lot of what EAGLE can do

    simply wouldn't be possible without ULPs. We don't have a lot of

    developers to implement many of the features users request, allowing

    users to develop custom functionality that suits there individual tastes

    is a win for the individual user and for others who have had similar ideas.

     

    Additionally it's not very difficult to make a ULP a shortcut or custom

    button in the text menu look at the designlink and LTSpice ULPs and how

    they're exposed in the tool bar.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 13 years ago in reply to autodeskguest

    On 04/15/13 11:43, Andreas Weidner wrote:

    Am 13.04.2013 22:25, schrieb Walter.Spermann@cadsoft.de:

    We have some architectural restrictions here: Generally commands don't

    work across sheets

    unless you operate with groups. I hope we can once overcome this

    restriction.

     

    Yes, please.

     

    Does it make sense to set/change the VALUE for a whole group ?

     

    Yes. Though it IS possible to use the command line for the infamous

    "value 100n", you still need to click on EVERY capacitor. For typical

    boards, we have about >50 of those, and ALL on the same sheet. Same

    thing with diode matrices and "1N4148" etc.

    OK, convinced !

     

     

    Changing a group needs some additional user questions in the following

    case (I think I already mentioned that sometime, but anyway):

    1. In case ALL grouped objects have been defined with 'VALUE=ON',

        all grouped objects get the new value.

    2. In case at least one grouped object was defined with 'VALUE=OFF',

        the user should be asked something like 'At least one object has

        no user-defineable value. Do you want to change these values, too?'

         - In case of YES, all grouped objects get the new value.

         - In case of NO, only the objects with 'VALUE=ON' get the new

           value, the others NOT.

         - In case of CANCEL, NO objects gets the new value.

    3. All grouped objects that don't HAVE a value are completely ignored.

    OK.

     

    Anyway it's only applicable for part instances and elements. And you

    want to give them all the same value ?

     

    Of course this does not happen THAT often. Making those commands behave

    properly with groups is just a function that should be implemented in

    order to make the non-modal info dialog work with ALL sorts of selections.

     

    Info for GROUP could be either the 'least common denominator' of all

    group entities or something like

    "group consisting of x Elements, y signals, z vias" and maybe listing

    those.

     

    Implementing ONLY the latter is rather useless - this would NOT make it

    possible to change parameters at all. I would like to have BOTH things

    shown:

    4. As a heading, show 'No selection' if nothing is 'selected', or

        the object type in case only ONE object type is selected (e.g.

        '1 element' or '3 elements'), or the group information as stated

        by you ('3 elements, 5 signals'). Since this MIGHT get too long,

        it would also be OK to just display ('8 objects'), and NOT list

        them (when selecting MANY objects, a list would be too cumbersome).

    5. Below the heading display (and enable editing) of all parameters

        common to ALL grouped objects.

    OK, that's what I meant with 'least common denominator'.

     

    6. This obviously would NOT enable the user to drag a 'selection'

        across a sheet and change the value of all capacitors to '100n',

        because not only the capacitors, but also connected NETS would be

        grouped. This is why the VALUE command itself (and other commands

        as well) should properly support groups.

     

    Are you aware that GROUP actually accepts Ctrl ?

     

    Yes. That's why I wrote 'accept dragging rectangles together with CTRL':

    At the moment, it's possible EITHER to drag a rectangle OR select SINGLE

    objects with CTRL. You cannot ADD rectangular regions to an already

    existing group or remove such a region from one. It would be nice if

    EAGLE could do it in the way every other graphical vector editor does it...

    I don't think there are many editors who can actually ADD rectangular regions,

    at least I don't know anyone. This should not prevent us from implementing

    something like that image

     

    I have the impression it's a better idea to change the existing GROUP a

    bit:

     

    I am NOT talking about a change in the current behaviour of the GROUP

    command here. All I wanted is to make it possible to add/subtract

    NUMEROUS rectangular regions to/from a group, which is not possible

    currently. The 'pointer' command I was talking about would NOT have the

    full functionality of GROUP (e.g., no polygon selections), but just a

    limited set for a more 'Office-like' feeling.

     

    You need the Ctrl-click now in order to support MOVE with the normal

    click

    if I understand correct.

     

    Again, I am NOT talking about changing the behaviour of EXISTING

    commands. All mentioned functionality lies SOLELY in the 'pointer'

    command, and does NOT have any impact on others. This means that all the

    grouping, moving, deleting, rotating etc. mentioned is NOT done by

    activating different commands, but by JUST activating the ONE 'pointer'

    command that does all these things automatically, depending on the click

    points.

     

    OK, if this should work we'd have to rename GROUP to something like

    GROUPMOVE or GROUPACTION image

     

    No, no, no! NO existing command needs to be renamed, and the behaviour

    of all existing commands stays as always. Keep in mind that ALL

    functionality lies in the ONE new 'pointer' command. This adds Office

    functionality for the new users, but most experienced users will stay

    with the more powerful existing EAGLE commands.

     

    The new 'pointer' command is NOT a way to automatically switch between

    the existing commands, but it has the FUNCTIONALITY (well, SOME of it)

    of SEVERAL existing commands WITHOUT having to switch between them at all.

     

    Andreas Weidner

    OK, thanks for sharing your ideas !

     

    Regards,

    Walter Spermann

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>