I keep getting an "out of memory" error even though my PC shows as having over a gig of free memory. Also started crashing, I assume due to the same memory problem. Any ideas please?
Thanks,
Bob Moreno
I keep getting an "out of memory" error even though my PC shows as having over a gig of free memory. Also started crashing, I assume due to the same memory problem. Any ideas please?
Thanks,
Bob Moreno
On 5/6/2013 4:25 PM, Bob Moreno wrote:
I keep getting an "out of memory" error even though my PC shows as
having over a gig of free memory. Also started crashing, I assume due to
the same memory problem. Any ideas please?
Thanks,
Bob Moreno
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/75827#75827
Hi Bob,
Could you provide more details about your OS setup? Is this a 64-bit
machine? Do you have any special type of setup or IT limitations?
Any and all details are welcome.
Let me know if there's anything else I can do for you.
Best Regards,
Jorge Garcia
Jorge,
The OS is Win 7, 64 bit, no special setup, no IT limitations. My PC shows lots of available memory, over one gig free. I've had Eagle 6.4 Pro since release, however this is the first new board I've done and the crashes occur during routing. Using same routing control file as prior used on Eagle 6.3.Same board specs anyway. The main problem is "out of memory" error during hand routing or I say at the start of attempting to hand route. I cannot hand route at all. It will auto route.
Thanks,
Bob Moreno
On 5/8/2013 9:33 AM, Bob Moreno wrote:
Jorge,
The OS is Win 7, 64 bit, no special setup, no IT limitations. My PC
shows lots of available memory, over one gig free. I've had Eagle 6.4
Pro since release, however this is the first new board I've done and the
crashes occur during routing. Using same routing control file as prior
used on Eagle 6.3.Same board specs anyway. The main problem is "out of
memory" error during hand routing or I say at the start of attempting to
hand route. I cannot hand route at all. It will auto route.
Thanks,
Bob Moreno
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/76049#76049
Hi Bob,
Please try uninstalling EAGLE and then reinstalling it to the Documents
directory. I want to try to isolate EAGLE from any Windows 7 craziness.
Let me know what happens when you do that.
Best Regards,
Jorge Garcia
Jorge,
Ok done, I'll let you know how that goes.
Thanks, Bob Moreno
On 5/9/2013 10:42 AM, Bob Moreno wrote:
Jorge,
Are you referring to the working files when you say install in the docs
directory? If so, that is where Eagle is installed.
Thanks,
Bob Moreno
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/76145#76145
Hi Bob,
I'm referring to having EAGLE's installation directory in Documents
instead of Program Files (x86) which is where Windows normally wants
program to be installed.
Let me know if there's anything else I can do for you.
Best Regards,
Jorge Garcia
Jorge,
Are you referring to the working files when you say install in the docs directory? If so, that is where Eagle is installed.
Thanks,
Bob Moreno
Jorge,
Are you referring to the working files when you say install in the docs directory? If so, that is where Eagle is installed.
Thanks,
Bob Moreno
Jorge,
Ok done, I'll let you know how that goes.
Thanks, Bob Moreno
On 5/9/2013 10:42 AM, Bob Moreno wrote:
Jorge,
Are you referring to the working files when you say install in the docs
directory? If so, that is where Eagle is installed.
Thanks,
Bob Moreno
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/76145#76145
Hi Bob,
I'm referring to having EAGLE's installation directory in Documents
instead of Program Files (x86) which is where Windows normally wants
program to be installed.
Let me know if there's anything else I can do for you.
Best Regards,
Jorge Garcia