EAGLE User Support (English) Eagle graphical glitch with fglrx drivers on Linux
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
  • Replies 26 replies
  • Subscribers 181 subscribers
  • Views 3153 views
  • Users 0 members are here
  • board
  • fglrx
  • eagle
  • Ubuntu
  • schematic
  • linux
Related

Eagle graphical glitch with fglrx drivers on Linux

Former Member
Former Member over 12 years ago

Hello i am having an issue with eagle on Ubuntu 12.10 using a AMD HD 7770 graphics card using the fglrx drivers, currently im using the latest drivers (13.3) from their website but i have also tried older versions which come with ubuntu no difference.

 

I have also tried multiple versions of eagle, all have the same problem.

 

anything within the work area on either schematic or boardlayout will glitch up, i found another post in german with the same problem so its not just me having the issue. http://www.element14.com/community/message/73170

 

previously i had been using a nvidia card which worked fine on this system.

 

image

 

any help would be welcome, thank you.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 12 years ago

    Hey all,

     

    I've noticed that this problem isn't just restricted to Eagle. Most graphics programs (including unity) have issues with the ATI card. It appears that configured settings are not applied correctly upon reboot.

     

    To get Eagle functioning properly, I've found that playing around with a combination of Tear-Free and other refresh settings, applying each time, and then zooming/scrolling a schematic after re-launching Eagle can eventually result in it being useable. If I come accross a successful set of repeatable operations I'll provide more information.

     

    As this effects several work computers I think the easiest and cheapest solution is going to be to put a Nvidia card in them.

     

    -nada

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to Former Member

    Nathan Dyer wrote:

     

    Hey all,

     

    I've noticed that this problem isn't just restricted to Eagle. Most

    graphics programs (including unity) have issues with the ATI card. It

    appears that configured settings are not applied correctly upon reboot.

     

    To get Eagle functioning properly, I've found that playing around with a

    combination of Tear-Free and other refresh settings, applying each time,

    and then zooming/scrolling a schematic after re-launching Eagle can

    eventually result in it being useable. If I come accross a successful

    set of repeatable operations I'll provide more information.

     

    As this effects several work computers I think the easiest and cheapest

    solution is going to be to put a Nvidia card in them.

     

    -nada

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/91595#91595

     

    FYI, Eagle runs fine on the Radeon HD6450 (ATI 'Caicos' card) in my Gentoo

    system using the open-source radeon driver. If you have a card supported by

    the open drivers and don't do high-framerate gaming that's another option.

    IMO the binary fglrx drivers are hopeless. I've also had good luck with

    Nvidia and their binary blob in the past. In my experience any combination

    other than ATI/OpenSource or NVidia/BinaryBlob is iffy at best.

     

    Bob

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    On 16/10/13 07:26, Robert Johnson wrote:

    In my experience any combination

    other than ATI/OpenSource or NVidia/BinaryBlob is iffy at best.

     

    I've used NVidia/nouveau with reasonable success.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    On 16/10/13 07:26, Robert Johnson wrote:

    In my experience any combination

    other than ATI/OpenSource or NVidia/BinaryBlob is iffy at best.

     

    I've used NVidia/nouveau with reasonable success.