EAGLE User Support (English) LTspice
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
  • Replies 2 replies
  • Subscribers 177 subscribers
  • Views 1486 views
  • Users 0 members are here
Related

LTspice

autodeskguest
autodeskguest over 12 years ago

When I try to export my eagle schematic to LTSpice IV a windows box pops up

and displays "LTspiceIV (scad3.exe) not found."

Where do I configure Eagle-6.4.0 to my LTspice IV directory.

Is LTspice IV interface is block because I'm using the free version of

Eagle?

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 12 years ago

    Am 18.06.2013 16:08, schrieb Dale Farmer:

    When I try to export my eagle schematic to LTSpice IV a windows box pops up

    and displays "LTspiceIV (scad3.exe) not found."

     

    Ditto with our PCs here, apparently because LTSpice is NOT installed in

    its default directory.

     

    Where do I configure Eagle-6.4.0 to my LTspice IV directory.

     

    Apparently you cannot configure this:

      - The help file tells me to go into the setup with 'run ltspice /S',

        but this also only complains about the missing EXE file.

      - The only other thing the help for the ULP tells me is that it would

        find LTSpice automatically, but does NOT tell me about any plan B

        (in case it doesn't).

     

    Is LTspice IV interface is block because I'm using the free version of

    Eagle?

     

    No, we're using the professional version here, and it behaves the same.

     

    CadSoft: HOW do I get the ULP running without having to go through all

    the source code, try to understand it and make manual changes? Thanks.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago

    Dale Farmer wrote on Tue, 18 June 2013 15:56

    When I try to export my eagle schematic to LTSpice IV a windows box

    pops up

    and displays "LTspiceIV (scad3.exe) not found."

    Where do I configure Eagle-6.4.0 to my LTspice IV directory.

     

     

    Hi. If you still haven't fixed that, here is how I did it this morning.

     

    In the EAGLE control panel find the "ltspice.ulp" (under User Language

    Programs), right click and open it.

     

    In the editor, find the string "rootpath" (it should be at line 4082) and

    add inside the {} (just after the { is fine), the path of your LTspiceIV

    folder, between "" and followed by a comma.

     

    Example:

     

    Original line 4082

    string rootpath[] = { "C:/Programme/", "C:/Program files (x86)/",

    "C:/Program files/", "D:/Program files (x86)/", "D:/Program files/" };

     

    Your LTspiceIV folder

    C:\Progs\LTC\LTspiceIV\

     

    New line 4082

    string rootpath[] = { "C:/Progs/LTC/", "C:/Programme/", "C:/Program files

    (x86)/", "C:/Program files/", "D:/Program files (x86)/", "D:/Program

    files/" };

     

    This is a "brute force" solution and has not been fully tested, I hope thai

    it works and that the Techical Support will fix it in a better way.

     

    Hope it helps. image

     

    Luigi Giovannelli

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.