Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 126 replies
  • Subscribers 200 subscribers
  • Views 10929 views
  • Users 0 members are here
  • our
  • have
  • expert
  • eagle?
  • jorge!
  • ask
  • a
  • cadsoft
  • about
  • question
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!

Jorge_Garcia
Jorge_Garcia over 13 years ago

If you have questions about CadSoft EAGLE, please click here to post your question!


If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

richardhammerl.png

 

Jorge Garcia

I'm a young engineer with extensive experience working on EAGLE. My interests include Power Supply design and LED solid state lighting, and I'm always impressed by a well designed PCB.

 

 

If not already, you'll need to

image or image

 


to ask your question.

Otherwise, click reply below.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello Jorge,

     

    I am a pcb engineer who is returning to Eagle from Orcad.

    Here is my issue...

     

    I have created the following aspects for the generic part:

     

    1.) Symbol

    2.) Package

    3.) Device

     

    I have connected all the package's pin functions when I created the device.

     

    When I created the package's aspects(symbol,package,device) I set the grid size to 1 mil @ 1 multiple/ Alt:1 mil due to the package size being 4mm X 5mm X .75mm, and the pins being smaller @ 27.55906 mils X 9.84252 mils. 

     

    Now I am having the most frustrating/hair pulling time connecting not only the device's pins but all the other components as well.

    What am I doing wrong here that nothing connects and that connections are very difficult to snap? 

     

    This project's ttm debut is in 3 weeks.

     

    Thank you in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 3/23/2014 11:38 PM, Emjay Ahday wrote:

     

     

    When I created the package's aspects(symbol,package,device) I set the

    grid size to 1 mil @ 1 multiple/ Alt:1 mil due to the package size being

    4mm X 5mm X .75mm, and the pins being smaller @ 27.55906 mils X 9.84252

    mils.

     

    Here's your problem. For the schematic symbol you should always stick to

    a 0.1"(2.54mm) grid. For the package you may use whatever is convenient

    but for the symbol we very strongly encourage users to stick to a 0.1"

    grid. The reason being that all of the components are made to that grid,

    and in order for connections to be properly formed you must connect end

    points exactly. If you're off by even a fraction of a mil, things won't

    connect.

     

    The solution is to fix the symbol so that the pins land on a 0.1" grid,

    after that you'll notice that everything connects very easily.

     

    hth,

    Jorge Garcia

     

    Now I am having the most frustrating/hair pulling time connecting not

    only the device's pins but all the other components as well.

    What am I doing wrong here that nothing connects and that connections

    are very difficult to snap?

     

    This project's ttm debut is in 3 weeks.

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to autodeskguest

    Thank you Jorge for the reply. I truly appreciate it.

     

    So let me make sure I have this straight...

     

    Whenever creating an OCM component of any size I want to be sure to leave the SYMBOL ONLY grid setting @ 0.1 Inch(2.54mm) to make sure the pins snap/connect correctly?

     

    Now to correct my current conundrum...

     

    What is the process to "fix" the symbol?

     

    Are you saying all I have to do is recreate the entire symbol aspect ONLY of the OCM component?

    or,

    Just change the OCM's symbol's grid to 0.1 Inch(2.54mm)?

     

    I don't understand.

     

    I await your wise counsel Sir.

     

    Thanks again Jorge for I am almost home! image

     

    Emjay Ahday

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Chuck,

    Thank you again for the reply for I appreciate your help immensely.I am working on it now.


    From your instructions it appears I will have to enlarge the component's symbol aspect considerably in order for each of the pins to line up to the 0.1" in 1 intersects for proper wire connection. Is this correct?


    Remember, I originally created this component's symbol(as well as the package & device) aspect all in 1 mil grid increments as the component is only 4mm X 5mm X 0.75 mm. Being the component is so small I chose to build its symbol aspect in mils. This is before your correction of course.


    So by me enlarging the component's symbol size to match with each 0.1" spacing to allow wire connections this will have no bearing on the schematic?

     

    Just to let you know the component has eight pads on each side along with a bottom(gnd) pad to make 17 pads in total.

    Spacing each pad to conform to the 0.1" grid will enlarge the component exponentially from what I originally created(in mils).

     

    Thanks again'Chuck for the correction instructions! I love learning(relearning in this case) it is a never ending journey! image

     

    Emjay

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Chuck,

    Thank you again for the reply for I appreciate your help immensely.I am working on it now.


    From your instructions it appears I will have to enlarge the component's symbol aspect considerably in order for each of the pins to line up to the 0.1" in 1 intersects for proper wire connection. Is this correct?


    Remember, I originally created this component's symbol(as well as the package & device) aspect all in 1 mil grid increments as the component is only 4mm X 5mm X 0.75 mm. Being the component is so small I chose to build its symbol aspect in mils. This is before your correction of course.


    So by me enlarging the component's symbol size to match with each 0.1" spacing to allow wire connections this will have no bearing on the schematic?

     

    Just to let you know the component has eight pads on each side along with a bottom(gnd) pad to make 17 pads in total.

    Spacing each pad to conform to the 0.1" grid will enlarge the component exponentially from what I originally created(in mils).

     

    Thanks again'Chuck for the correction instructions! I love learning(relearning in this case) it is a never ending journey! image

     

    Emjay