Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Hi I am new to Eagle!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 239 views
  • Users 0 members are here
Related

Hi I am new to Eagle!

e14 Contributor
e14 Contributor over 12 years ago

Hi I am new to Eagle. I want to start using it. I am doing a project that uses the PIC18F66K80 to write/read to the FM25V05 FRAM by Cypress. The PIC will also communicate via UART with the C329 camera

module. It will also communicate with a PC via UART and will also utilize the CAN interface.

I have seen that Eagle don't have PIC18F66K80. How do I create it in the library? I want also to create the FM25V05. From where do I start? Please give me some support.

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 12 years ago

    On 12/31/2013 03:07 AM, Alexandros Stefanidis wrote:

    Hi I am new to Eagle. I want to start using it. I am doing a project

    that uses the PIC18F66K80 to write/read to the FM25V05 FRAM by Cypress.

    The PIC will also communicate via UART with the C329 camera

    module. It will also communicate with a PC via UART and will also

    utilize the CAN interface.

    I have seen that Eagle don't have PIC18F66K80. How do I create it in the

    library? I want also to create the FM25V05. From where do I start?

    Please give me some support.

     

    Start by looking in the doc directory below Eagle's installation

    directory.  On Linux, this is typically /opt/eagle-6.5.0/doc.

     

    In that directory you will find tutorial_en.pdf and

    manual_en.pdf .  The tutorial has a section describing exactly what

    you're trying to do.

     

    In summary, you need to create your own private library.  Next, create a

    symbol for the PIC.  Then, you need to create at least one package for

    the PIC.  A suitable SMD package /may/ be found// in smd-ipc.lbr, from

    which you can copy into your library (see "HELP COPY").  And finally you

    need to create a device for the PIC.  The device is what associates the

    symbol with the package.  Most microcontrollers can be purchased in

    different packages (DIP, QFP, PLCC, etc.).  To accommodate this, you can

    optionally create and add additional packages to a device, giving each

    package its own suffix.

     

    Once that is done, go back to your schematic, and USE the library you

    just created, and ADD the device to the schematic, choosing an

    appropriate package.  If the library changes after it's in the

    schematic's USE list, use the UPDATE tool to reflect the changes into

    your schematic and board.

     

    HTH,

        - Chuck

     

     

    Attachments:
    8407.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 12 years ago

    On 12/31/2013 03:07 AM, Alexandros Stefanidis wrote:

    Hi I am new to Eagle. I want to start using it. I am doing a project

    that uses the PIC18F66K80 to write/read to the FM25V05 FRAM by Cypress.

    The PIC will also communicate via UART with the C329 camera

    module. It will also communicate with a PC via UART and will also

    utilize the CAN interface.

    I have seen that Eagle don't have PIC18F66K80. How do I create it in the

    library? I want also to create the FM25V05. From where do I start?

    Please give me some support.

     

    Start by looking in the doc directory below Eagle's installation

    directory.  On Linux, this is typically /opt/eagle-6.5.0/doc.

     

    In that directory you will find tutorial_en.pdf and

    manual_en.pdf .  The tutorial has a section describing exactly what

    you're trying to do.

     

    In summary, you need to create your own private library.  Next, create a

    symbol for the PIC.  Then, you need to create at least one package for

    the PIC.  A suitable SMD package /may/ be found// in smd-ipc.lbr, from

    which you can copy into your library (see "HELP COPY").  And finally you

    need to create a device for the PIC.  The device is what associates the

    symbol with the package.  Most microcontrollers can be purchased in

    different packages (DIP, QFP, PLCC, etc.).  To accommodate this, you can

    optionally create and add additional packages to a device, giving each

    package its own suffix.

     

    Once that is done, go back to your schematic, and USE the library you

    just created, and ADD the device to the schematic, choosing an

    appropriate package.  If the library changes after it's in the

    schematic's USE list, use the UPDATE tool to reflect the changes into

    your schematic and board.

     

    HTH,

        - Chuck

     

     

    Attachments:
    8407.att1.html.zip