EAGLE User Support (English) Forward and back annotation broken. Help!
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 2147 views
  • Users 0 members are here
  • back
  • forward
  • annotations
Related

Forward and back annotation broken. Help!

Former Member
Former Member over 11 years ago

Late last week I downloaded the free version of Eagle 6.5 following Jeremy Blum's tutorial on Eagle.  All went well, I was able to create a schematic and then transfer it to a board and do routing.  Sometime in the last couple days I screwed something up and I have no idea what I did.

If I create any type of schematic and then go to open a new board Eagle gives me the error massage  that the forward and back annotations are not available.  As a test I placed a battery, LED and one resistor in the work area for Eagle and then made the correct connections.  I ran the electric circuit check and all connections were fine. But even with that simple design, clicking on new board gave me that same error and then none of the components were transferred to the board.  I have uninstalled Eagle and reinstalled it with the same results.  I have even gone into the registry and deleted all references to Cadsoft and Eagle.  I also deleted all directories and subfolders use by Eagle, and then did another fresh install.  Same problem. When I create any type of circuit in the schematic and open a new board it gives me a forward and back annotation error and no components on the board.

 

i'm afraid I have things so screwed up I'll never get Eagle to work again. 

 

Any help would be greatly appreciated!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    Glad that fixed the problem.  For us over 60 crowd, it can be tough laying

    out those boards for the octal sockets with our vacuum tubes  image

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago

    Glad that fixed the problem.  For us over 60 crowd, it can be tough laying

    out those boards for the octal sockets with our vacuum tubes  image

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    What I hate is chiseling out the rock base.  :-)