Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Cannot remove wrong placed routes on pcb
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 1952 views
  • Users 0 members are here
  • eagle
  • lines
  • delete
  • error
Related

Cannot remove wrong placed routes on pcb

e14 Contributor
e14 Contributor over 12 years ago

When drawing some lines on the PCB, and when i want remove some lines, i use the Delete tool.

But when i click on the line, most time it's not working because i have warning:

"Can't backannotate this operation. Please do this in the schematic".

 

Huh? When is deleting wrong placed lines not allowed? I can only move them but that is more work. I want delete it faster and re-draw it again.

 

Why is this annoying error message almost ALWAYS popped when i want delete some lines. It feels the program is pretty bugged because there is nothing wrong with deleting lines.

Fix the problem immediately. *sigh*

image

  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    AnalogNotes over 12 years ago

    (Sorry, I didn't mean to send that last message so quickly without an explanation.  Here it is...)

     

    There's a difference between actually deleting a net (which has to be done in the schematic) and converting that net's airwire to a trace and then ripping up that trace to convert it back to the airwire so that you can route it again.

     

    From the EAGLE help file:

    With active Forward&Back Annotation, no wires or vias can be deleted from a signal that is connected to components in a board. Also, no components can be deleted that have signals connected to them. Modifications like these have to be done in the schematic.

     

    Does that help?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • AnalogNotes
    AnalogNotes over 12 years ago

    (Sorry, I didn't mean to send that last message so quickly without an explanation.  Here it is...)

     

    There's a difference between actually deleting a net (which has to be done in the schematic) and converting that net's airwire to a trace and then ripping up that trace to convert it back to the airwire so that you can route it again.

     

    From the EAGLE help file:

    With active Forward&Back Annotation, no wires or vias can be deleted from a signal that is connected to components in a board. Also, no components can be deleted that have signals connected to them. Modifications like these have to be done in the schematic.

     

    Does that help?