Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Shaping a Ground plane
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 606 views
  • Users 0 members are here
Related

Shaping a Ground plane

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I want to shape the ground plane and remove the unnecessary parts of the ground plane and make everything tidy. Its manually routed on bottom layer so that I can easily make it using toner transfer method at home. So far I used bRestrict and drew polygons to remove parts of the ground plane that are unncessary. But it is not even. For example. See the bottom left corner of the board below. I want the ground plane to be perfect.
image

 

 

 

It's my second PCB Im routing myself. So I am open to suggestions. It is a USBASP circuit to program Atmel Atmega MCUs

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    On 04/13/2014 10:29 AM, Ayush Chand wrote:

    So far I used bRestrict and drew polygons to remove parts of the ground

    plane that are unncessary.

    Use more then one ground polygon.They will be smaller then the board.

    Use the split and miter to move the edge of the polygon to clear the

    areas as needed. Instead of restrict polygons just use a thin wire. Be

    sure to have orphans off on the polygon.

    This is an example with the +5 buss highlighted and down mostly with

    polygons

    http://arcelectronicsinc.com/testinfo/plus5.png

     

    Paul

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 12 years ago

    On 04/13/2014 10:29 AM, Ayush Chand wrote:

    So far I used bRestrict and drew polygons to remove parts of the ground

    plane that are unncessary.

    Use more then one ground polygon.They will be smaller then the board.

    Use the split and miter to move the edge of the polygon to clear the

    areas as needed. Instead of restrict polygons just use a thin wire. Be

    sure to have orphans off on the polygon.

    This is an example with the +5 buss highlighted and down mostly with

    polygons

    http://arcelectronicsinc.com/testinfo/plus5.png

     

    Paul