Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Need trace stretch feature
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 190 subscribers
  • Views 1041 views
  • Users 0 members are here
  • eagle
  • cad
  • stretch
Related

Need trace stretch feature

e14 Contributor
e14 Contributor over 12 years ago

Would it be possible to add a trace stretch feature that preserves adjacent segment angles?  This feature would really be helpful when routing more complex designs.  Being able to do this for multiple selected traces would be nice, but just preserving adjacent angles for a single trace when moving would be a huge improvement.  Our usual layout engineer refuses to use Eagle on complex boards (high-density BGA) only because of this lacking feature.  Now that I'm forced to route this board,  I see why.  It would be very helpful.

 

Description from another software of the feature needed:

Track Dragging with Angle Preservation

Re-routing is not always the best approach to modifying routing, for example, situations where you want to move a track segment slightly, keeping the neat 45° and 90° corners at either end. (xxxxxx)  supports this, through multi-track dragging with angle preservation. Dragging behavior is controlled by the Preserve Angle When Dragging option in the PCB Editor - Interactive Routing page of the Preferences dialog.

To drag, click once on the segment to select it - the cursor will change to a quad-arrow - then click and drag to slide it to a new location. You will notice that the angles to adjacent track segments are preserved, maintaining the routing style.

 


 









  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    Todd Elliott wrote on Wed, 28 May 2014 13:09

    Would it be possible to add a trace stretch feature that preserves

    adjacent segment angles?  This feature would really be helpful when

    routing more complex designs.  Being able to do this for multiple

    selected traces would be nice, but just preserving adjacent angles for

    a

    single trace when moving would be a huge improvement.  Our usual

    layout

    engineer refuses to use Eagle on complex boards (high-density BGA)

    only

    because of this lacking feature.  Now that I'm forced to route this

    board,  I see why.  It would be very helpful.

     

    Description from another software of the feature needed:

    h2. Track Dragging with Angle Preservation

    Re-routing is not always the best approach to modifying routing, for

    example, situations where you want to move a track segment slightly,

    keeping the neat 45° and 90° corners at either end. (xxxxxx) 

    supports

    this, through multi-track dragging with angle preservation. Dragging

    behavior is controlled by the Preserve Angle When Dragging option in

    the PCB Editor - Interactive Routing page of the Preferences

    dialog.

    To drag, click once on the segment to select it - the cursor will

    change

    to a quad-arrow - then click and drag to slide it to a new location.

    You

    will notice that the angles to adjacent track segments are preserved,

    maintaining the routing style.

     

     

    Hello Todd,

     

    Right now with EAGLE v6, to get what you are looking for, it can be done

    but you have to first group the segments you want.  I have group assigned

    to CTRL+G so it is pretty quick but it does take more mouse clicks.  And on

    dense designs (of which we've done many) it would be much more efficient if

    these angles were maintained during moving so that grouping was not

    required for most basic moves.

     

    I know you didn't mention it, but taking the first sentence and googling

    it, I can see that you've taken that text from Altium's docs.  But let's

    not give the excuse of an expensive tool having this feature.  KiCAD (the

    gEDA open-source CAD tool) now has something very similar thanks to the

    good folks at CERN.  See this tutorial:

     

     

     

    ( reference https://www.youtube.com/watch?v=CCG4daPvuVI )

     

    So it appears that the low bar of the industry has just been raised.  This

    is a good time for such a feature to be added to EAGLE.  I'm not asking for

    all this interactive routing to be added right away, but being able to move

    a trace and keep the angles of adjacent segments would be useful.  I also

    like their snapping feature when one segment lines up with another and it

    can be optimised into one line--that is a nice touch.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

     

    Take advantage of v7 License Promotion right now at

    http://www.eaglecentral.ca

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 12 years ago in reply to autodeskguest

    Hi,

     

    Right now with EAGLE v6, to get what you are looking for, it can be done

    but you have to first group the segments you want.  I have group assigned

    to CTRL+G so it is pretty quick but it does take more mouse clicks.  And on

    dense designs (of which we've done many) it would be much more efficient if

    these angles were maintained during moving so that grouping was not

    required for most basic moves.

     

     

     

    I use that technique too (except that I assign ALT+G instead of Ctrl+G ! ). But this is efficient when we move several wires. When moving a single wire it's quite annoying.

     

    I would point out that if this feature could be add to eagle, it would be nice to implement it for every 'wire style' element such as polygons borders.

    And of course, it can also be useful in schematic and library editor...


    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kikoun
    kikoun over 12 years ago in reply to autodeskguest

    Hi,

     

    Right now with EAGLE v6, to get what you are looking for, it can be done

    but you have to first group the segments you want.  I have group assigned

    to CTRL+G so it is pretty quick but it does take more mouse clicks.  And on

    dense designs (of which we've done many) it would be much more efficient if

    these angles were maintained during moving so that grouping was not

    required for most basic moves.

     

     

     

    I use that technique too (except that I assign ALT+G instead of Ctrl+G ! ). But this is efficient when we move several wires. When moving a single wire it's quite annoying.

     

    I would point out that if this feature could be add to eagle, it would be nice to implement it for every 'wire style' element such as polygons borders.

    And of course, it can also be useful in schematic and library editor...


    Guillaume.