EAGLE User Support (English) Eagle 6.5 on Debian 7.4, freezes on 'Esc' and on tool switch.
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 585 views
  • Users 0 members are here
  • bug
Related

Eagle 6.5 on Debian 7.4, freezes on 'Esc' and on tool switch.

Former Member
Former Member over 11 years ago

Hi, new-user,

1. Options->Directories->Projects is empty and that causes screw-ups when you try to create a 'New Project' - it silently refuses to add a new project.

2. After I 'Add' a part from the library, when I hit 'Esc'  (once, twice, many times) to go back to the Parts-Library window, the whole thing freezes (cursor moves but clicking on a tool does nothing). I have to Ctrl-C to exit.

3. I add a bunch of parts and click the 'Select' tool to try to 'group select' then I click-drag to select and it freezes and no amount of 'Esc' allows me to click on another tool. The cursor moves but nothing else - no menus, and Ctrl-Panel doesn't recognise clicks

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 6/1/2014 9:30 PM, Veek M wrote:

    Hi, new-user,

    1. Options->Directories->Projects is empty and that causes screw-ups

    when you try to create a 'New Project' - it silently refuses to add a

    new project.

    Hi Veek,

     

    EAGLE can't create a new project if it doesn't know where to create it.

    Under Options -> Directories -> Projects make sure that some location is

    specified. I would recommend an EAGLE folder in documents, but any

    directory as long as it's not in the Program Files x86 folder(Windows)

    or in the Applications(Mac) folder will do.

    2. After I 'Add' a part from the library, when I hit 'Esc'  (once,

    twice, many times) to go back to the Parts-Library window, the whole

    thing freezes (cursor moves but clicking on a tool does nothing). I have

    to Ctrl-C to exit.

    3. I add a bunch of parts and click the 'Select' tool to try to 'group

    select' then I click-drag to select and it freezes and no amount of

    'Esc' allows me to click on another tool. The cursor moves but nothing

    else - no menus, and Ctrl-Panel doesn't recognise clicks

    When you went through the installation process did the installer

    complain about any missing libraries or things like that?

     

    Let's start there.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    nope - it didn't complain, and i checked using 'ldd'. I just can't use 'Esc' everything else works.

     

    'EAGLE can't create a new project if it doesn't know where to create it.'

    err.. that's what i said.. what I meant was that in the next release if someone in Eagle could point it to /opt/eagle-x.x.x/projects/ that would fix the issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 6/2/2014 9:41 PM, Veek M wrote:

    'EAGLE can't create a new project if it doesn't know where to create

    it.'

    err.. that's what i said.. what I meant was that in the next release if

    someone in Eagle could point it to /opt/eagle-x.x.x/projects/ that would

    fix the issue.

    Hi Veek,

     

    I hope you're doing well. What I meant to say was that you should set

    that path to whatever path is convenient on your machine and to your

    preferences. Different people work different ways and normally EAGLE

    defaults to a home location for the user projects under linux but for

    some reason it didn't on your machine.

     

    As to the Esc key issue. What keyboard driver are you using? If Esc is

    the only key that isn't working maybe an unusual keyboard driver might

    be to blame.

     

    hth,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    Hi Jorge, yup - I'm okay image as in I haven't bust an artery over this image everything else seems to be working. The thing is, I'm new to Eagle and was trying to follow one of the tutorials and i kept clicking 'Project' in the Eagle Control Panel and nothing was happening.

     

    I'm on Linux-Xorg so 'xev' tells me, when I press 'Esc', that i'm generating keycode 9 (keysym 0xff1b, Escape). Also, vim, GIMP etc work just fine with my Esc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 6/4/2014 6:25 AM, Veek M wrote:

    Hi Jorge, yup - I'm okay image as in I haven't bust an artery over this image

    everything else seems to be working. The thing is, I'm new to Eagle and

    was trying to follow one of the tutorials and i kept clicking 'Project'

    in the Eagle Control Panel and nothing was happening.

     

    I'm on Linux-Xorg so 'xev' tells me, when I press 'Esc', that i'm

    generating keycode 9 (keysym 0xff1b, Escape). Also, vim, GIMP etc work

    just fine with my Esc.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/115155

     

     

    Hi Veek,

     

    This is very unusual, I have an Ubuntu machine on my end here and the

    Esc key works just fine. EAGLE takes whatever the OS gives it so it's

    weird that something wouldn't work like that. Is there any possiblity

    the window manager is intercepting the Esc key, this happens with Alt

    often I've never seen it happen with Esc.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 6/4/2014 6:25 AM, Veek M wrote:

    Hi Jorge, yup - I'm okay image as in I haven't bust an artery over this image

    everything else seems to be working. The thing is, I'm new to Eagle and

    was trying to follow one of the tutorials and i kept clicking 'Project'

    in the Eagle Control Panel and nothing was happening.

     

    I'm on Linux-Xorg so 'xev' tells me, when I press 'Esc', that i'm

    generating keycode 9 (keysym 0xff1b, Escape). Also, vim, GIMP etc work

    just fine with my Esc.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/115155

     

     

    Hi Veek,

     

    This is very unusual, I have an Ubuntu machine on my end here and the

    Esc key works just fine. EAGLE takes whatever the OS gives it so it's

    weird that something wouldn't work like that. Is there any possiblity

    the window manager is intercepting the Esc key, this happens with Alt

    often I've never seen it happen with Esc.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    I use olvwm - which is quite dated. I don't think it's intercepting a key, but it's quite possible that after the 'Esc' is read, something odd is taking place.. i'll fool around and if I find out i'll post.