Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) New eagle licensing -> goodbye Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 86 replies
  • Subscribers 203 subscribers
  • Views 16676 views
  • Users 0 members are here
  • licensing
Related

New eagle licensing -> goodbye Eagle

SpacedCowboy
SpacedCowboy over 12 years ago

So, I've used Eagle now for over 10 years. In all that time I've always upgraded to the latest version, but that's just stopped.

 

I have multiple computers, and I use multiple locations. I've always only ever used one instance of Eagle at a time, and I've never given the license details to anyone else. Unfortunately, the latest way in which Eagle is licensed is way too restrictive for me to work with the product as I have done for over a decade now.

 

The problem is two-fold:

  • You are only allowed to install on 2 (which is pitiful!) computers if you have a single user license.
  • You cannot use a flexlm-based license for a single-user license.

 

The combination of those two things means I can't duplicate the setup I currently have, so this is the classic example of how proprietary software owners can screw you over without you having any recompense or workaround, despite you being a paying and loyal customer for an extended period of time. I don't consider cracking the software to be an adequate workaround.

 

So, if I'm going to have to spend $$$ in the thousands, I'll take a good look at the competition first, and even at the freebies like kikad. Eagle has major shortcomings anyway - no "bus routing" and the differential pair support is poor at best. I think, with this decision, cadsoft couldn't have done more to help along the freebies, and lose the people who might some day splash the cash and go for the pro option.

 

A primary rule for any software "upgrade" is "don't break the existing workflows". Eagle v7 is completely useless to me, not because of its feature-set, not because of any price issues, but because the management is being pants-on-head moronic about how it goes about licensing. Licensing, of all things.

 

Very disappointed.

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14 Contributor

    Hi Pascal,

     

    Just try contacting me directly support@cadsoftusa.com or

    jorge@cadsoftusa.com. Make sure to include your serial number so that I

    can forward the information to you.

     

    Let me know if there's anything else I can do for you.

     

    hth,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    Hello!

    I have a problem right now. I was in version 7.3 (Mac). I have installed 7.4 which fortunately

    installed without erasing 7.3. I have used the same license file (I always copy the license key

    in the application folder, therefore it was in EAGLE-7.3.0) to the new 7.4 folder. As I keep my

    license numbers and passwords in a text file also in the Eagle folder, I'm pretty sure it's the

    same password as last time.

    Result: it simply doesn't work.

    I have tried to contact sales@cadsoftusa.com and it came back with an error.

    Any hint about how to get a new password (if possible a working one)?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to kedwa30

    On 9/15/2015 12:20 PM, Kenneth Edwards wrote:

    I've read the first and last pages and so I understand the issue to be

    resolved with this particular product, but I had an idea that I just

    wanted to put out there.

     

    "You are only allowed to install on 2 (which is pitiful!) computers if

    you have a single user license."

     

    Hi Kenneth,

     

    I hope you're doing well. Again, this is obsolete information. We

    removed that licensing mechanism one month after the release of V7 and

    reverted back to our old system which allows users to install on as many

    machines as they have.

     

    These types of concerns are precisely why(thankfully) management made

    the decision to back off on this licensing mechanism(I'm sure the

    horrendous blow to sales helped a bit too image ).

     

    This entire thread is obsolete because we removed that very offensive

    licensing scheme.

     

    This is how things stand now 09/15/2015:

    1. You may install EAGLE on as many machines as you own. As long as no

    more than the number of licensed users are using EAGLE at any point in

    time you are complying with the license.

     

    Ex. If you have a 3 user license, you can install EAGLE on an infinite

    number of machines as long as no more than 3 people are using EAGLE at

    the same time everything is cool.

     

    2. Licenses are assigned to a location. So for example if you have 3

    offices around the world. Each one needs to have it's own license, this

    enables the person responsible for the license at each location to

    monitor the use of the licenses locally.

     

    3. All of the updates within a major version are free.

     

    Ex. We are now in V7. You will receive 7.1, 7.2, 7.3, 7.4, etc. for no

    additional cost. You use the same key file and installation code to

    license each update.

     

    4. Upgrades are not compulsory, users determine if they wish to upgrade

    or not.

     

    Ex. Once V8 is released, you have the option to continue using V7

    without paying another cent. Keep in mind that development of a major

    series stops once a new major version comes out so you will not receive

    any new bugfixes or corrections(Unless it's something exceptional). The

    other choice is to upgrade to V8 for an upgrade fee. The upgrade fee is

    roughly 1/3 of your original purchase price.

     

    hth,

    Jorge Garcia

    Cadsoft Support

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kedwa30
    kedwa30 over 11 years ago

    I've read the first and last pages and so I understand the issue to be resolved with this particular product, but I had an idea that I just wanted to put out there.

     

    "You are only allowed to install on 2 (which is pitiful!) computers if you have a single user license."

     

    What about the possibility of installing to a virtual machine? If that is allowed at all, then that could solve the problem since you'd be able to put the virtual machine file on a external drive or keep it in the cloud and boot it to any host machine you happen to have available.

    Of course it's not an ideal solution since the virtual machine is always a fraction of the power of the bare metal machine. Technically it would only be installed to the one virtual machine which would only exist when it is booted. Another workaround is to use one of many programs that allows you to control a computer remotely. Of course that requires a network connection.

     

    Someday the notion of having a single machine will be erased as home computers become made up of arrays of single board computers setup like a supercomputer. Rather than upgrade to a faster desktop, increasing compute power will be accomplished by adding boards to the array. Boards that go bad will simply be removed from the array.

     

    When a person buys a product they expect to pay one time. When they buy a service or a subscription, that's different. If two people share three cars, they end up paying for six insurance policies, one per person per car. They don't expect to do the same with software.

    It's not the same and should not be billed the same. Software is not insurance. If it was, then it should be regulated like insurance is regulated. Think about that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    V7 introduced some extra license types, now called "Make Pro" and "Make

    Personal", that require Internet connections and such. Just ignore them.

    The "standard" and "professional" licenses are the same as they always were.

     

    Make Personal, is the Hobbyist renamed it doesn't require an internet

    connection. The only real new thing is Make Pro, which has an area

    limitation instead of the fixed dimensions we used to have. That's the

    only real new thing.

     

    Basically with Make Pro as long as your board is less than approx 24 sq

    inches you'll be OK, you have flexible limits.

     

    Everything else is just a rose by a different name.

     

    hth,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to rbtx99

    On 14/09/15 09:22, rbtx99 wrote:

    CadSoft Guest wrote:

     

    This is an entirely obsolete issue. The current (main) V7 license

    works

     

    the same way as the V5 one did. Yes, there are new options that you

     

    probably don't want, but you don't have to have them.

     

    Well that is good news and tempting to do an update. But what do you

    mean about the options?

     

    V7 introduced some extra license types, now called "Make Pro" and "Make

    Personal", that require Internet connections and such. Just ignore them.

    The "standard" and "professional" licenses are the same as they always were.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rbtx99
    rbtx99 over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

    This is an entirely obsolete issue. The current (main) V7 license works

    the same way as the V5 one did. Yes, there are new options that you

    probably don't want, but you don't have to have them.

     

    Well that is good news and tempting to do an update. But what do you mean about the options?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to rbtx99

    On 13/09/15 19:35, Angelos Gonias wrote:

    The licencing is the main reason I didn't upgrade past V5.

     

    Catch up at the back there!

     

    This is an entirely obsolete issue. The current (main) V7 license works

    the same way as the V5 one did. Yes, there are new options that you

    probably don't want, but you don't have to have them.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rbtx99
    rbtx99 over 11 years ago

    The licencing is the main reason I didn't upgrade past V5. I do fancy some of the new features and I was considering upgrading but not if I have to loose the flexibility of running EAGLE at work, home and laptop. Whilst Cadsoft may have prevented some licencing fraud in my case they lost both the V6 and V7 upgrades.

     

    I like EAGLE and I will continue to use my v5 version as long as I can; then move to something else. KiCad perhaps. The good news is that the v5 runs on Windows 10 so I am not pressed to change and I can continue to maintain the old projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 12 years ago in reply to dcomer

    Hi,

    Dave Comer a écrit:

     

    I'd like to thank Jorge and his excellent attitude in helping me get my license updated.

    I would like to thank Jorge too, he also help me to convert my license 7.0 in to 7.1 He is really helpful, and not only for license problem. So

     

    Thank you Jorge, and thank you Cadsoft for their attention to customer complains or suggestions.

     

    Guillaume Barrey.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>