Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) CONSTANT crashing Eagle 7.1.0 under MacOS 10.9.4 - is Eagle a real piece of software?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 189 subscribers
  • Views 1336 views
  • Users 0 members are here
Related

CONSTANT crashing Eagle 7.1.0 under MacOS 10.9.4 - is Eagle a real piece of software?

e14 Contributor
e14 Contributor over 12 years ago

I have an urgent project that *constantly* crashed the autorouter approximately 95% of the time.  The result is an application that is utterly unusable, and while tweaking the auto router and doing things like routing the ground plane first eventually produced a 100% route, the polygons subsequently "fall apart" on my ground plane, completing only 80% of the only fairly complex board.

 

System has 24 cores at 3.46Ghz and 64GB of ram...

 

Is this software just junk?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    On 9/15/2014 10:02 PM, Ben Cannon wrote:

    I have an urgent project that constantly crashed the autorouter

    approximately 90% of the time.  The system is unusable, and while

    tweaking the auto router and doing things like routing the ground plane

    first eventually produced a 100% route, the polygons subsequently "fall

    apart" on my ground plane, completing only 80% of the only fairly

    complex board.

     

    System has 24 cores at 3.46Ghz and 64GB of ram...

     

    Is this software just junk?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/126511

     

    Hello Ben,

     

    I hope you're doing well. Define "crash", do you mean EAGLE actually

    closes or does it just seem to stop working. The pre-router variant can

    take a while to process. To test this run the autorouter but uncheck the

    prerouter option that shows up in the first dialog after you click on

    the autorouter.

     

    Keep in mind that an autorouter is a tool, and being a designer involves

    knowing when to use one tool over the other. Polygons fall apart when

    too many traces run through them and isolated islands of copper form. If

    you have any high-speed or high-power signals don't use the autorouter.

    If you have any low level signals to process don't use the autorouter.

     

    Your hardware can't be fully leveraged by EAGLE so past a certain point

    having more ram or cores doesn't produce any improvement in processing time.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to autodeskguest

    Hi Jorge, thank you for chiming in. 

     

    I mean crashing.  As in, "The application EAGLE unexpectedly quit, click here to reopen". 

     

    I see that the top router does take a lot longer, but it does seem to produce some exciting results.

     

    It looks like none of the auto routers are able to route a board of any complexity that incorporates a ground plane. (Why it doesn't simply add Vias to reconnect a "fallen apart" ground plane is beyond me.)   Just auto routing the GND class/net with via cost way down produces a beautiful result, but as soon as the rest of the board is routed with ground/VCC planes, everything goes to heck.  But that's another story.

     

    I've got to get around these crashes first, it's all but completely un-useable now, the crashes are 100% now, somewhere between 5 and 15min into an autoroute (that looks like it should be a multi-hour process with my settings.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 9/17/2014 1:10 AM, Ben Cannon wrote:

    Hi Jorge, thank you for chiming in.

     

    I mean crashing.  As in, "The application EAGLE unexpectedly quit, click

    here to reopen".

     

    I see that the top router does take a lot longer, but it does seem to

    produce some exciting results.

     

    It looks like none of the auto routers are able to route a board of any

    complexity that incorporates a ground plane. (Why it doesn't simply add

    Vias to reconnect a "fallen apart" ground plane is beyond me.)   Just

    auto routing the GND class/net with via cost way down produces a

    beautiful result, but as soon as the rest of the board is routed with

    ground/VCC planes, everything goes to heck.  But that's another story.

     

    I've got to get around these crashes first, it's all but completely

    un-useable now, the crashes are 100% now, somewhere between 5 and 15min

    into an autoroute (that looks like it should be a multi-hour process

    with my settings.)

     

    Hi Ben,

     

    Let's make sure you're permissions for EAGLE are setup correctly first.

    The crash time you're talking about 5 to 15 min is close to the

    automatic backup generation interval. If EAGLE isn't permitted to

    perform the backup, then it will crash.

     

    Here's the procedure to setup EAGLE's permissions

     

    1. Open Finder.

    2. Navigate to Application

    3. right click on EAGLE-7.1.0 Folder and select “Get Info”

    4. left click on the lock symbol at the bottom right and log into your

    admin account.

    5. select the plus sign on the bottom left and add your login name to

    the access list.

    6. select your access list the change it to read & write.

    7. left click on the lock symbol to close access to permission changes.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Just checked the new beta 7.5.4 - the same problem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to autodeskguest

    Hi there,

     

    I have the same problem - random crashes every 5-50 min.

     

    Eagle 7.5.0, Mac OS 10.9.5.  I really doubt it is related to the memory - I've got 18Gb and no other apps are running.

     

    If I run an old version 6.6.0 - no problems besides the commonly known screen re-draw issue.

     

    Cheers

    Kir

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to e14 Contributor

    Am 24.04.2016 um 04:01 schrieb Herb Sims:

    Jorge,

     

    I am having the same problem with V7.5 and Mac El Capitan OS.

     

    Here is what is says after more more than 30 seconds of autorouter:

     

    | Process:            | EAGLE |

    | Path:               |

    /Applications/EAGLE-7.5.0/EAGLE.app/Contents/MacOS/EAGLE |

    | Identifier:         | EAGLE |

    | Version:            | 7.5.0 (7.5.0) |

    | Code Type:          | X86-64 (Native) |

    | Parent Process:     | ??? |

    | Responsible:        | EAGLE |

    | User ID:            | 501 |

     

     

    Could be a memory problem. What are the grid settings for the

    Autorouter and the size of the board? How many routing jobs are

    running simultaniously?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to e14 Contributor

    Am 24.04.2016 um 04:01 schrieb Herb Sims:

    Jorge,

     

    I am having the same problem with V7.5 and Mac El Capitan OS.

     

    Here is what is says after more more than 30 seconds of autorouter:

     

    | Process:            | EAGLE |

    | Path:               |

    /Applications/EAGLE-7.5.0/EAGLE.app/Contents/MacOS/EAGLE |

    | Identifier:         | EAGLE |

    | Version:            | 7.5.0 (7.5.0) |

    | Code Type:          | X86-64 (Native) |

    | Parent Process:     | ??? |

    | Responsible:        | EAGLE |

    | User ID:            | 501 |

     

     

    Could be a memory problem. What are the grid settings for the

    Autorouter and the size of the board? How many routing jobs are

    running simultaniously?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to e14 Contributor

    Am 24.04.2016 um 04:01 schrieb Herb Sims:

    Jorge,

     

    I am having the same problem with V7.5 and Mac El Capitan OS.

     

    Here is what is says after more more than 30 seconds of autorouter:

     

    | Process:            | EAGLE |

    | Path:               |

    /Applications/EAGLE-7.5.0/EAGLE.app/Contents/MacOS/EAGLE |

    | Identifier:         | EAGLE |

    | Version:            | 7.5.0 (7.5.0) |

    | Code Type:          | X86-64 (Native) |

    | Parent Process:     | ??? |

    | Responsible:        | EAGLE |

    | User ID:            | 501 |

     

     

    Could be a memory problem. What are the grid settings for the

    Autorouter and the size of the board? How many routing jobs are

    running simultaniously?

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    This can be a sign that you ran out of memory. If you are running other processes, please stop them and try again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    This can be a sign that you ran out of memory. If you are running other processes, please stop them and try again.