EAGLE User Support (English) Wot, still no package land pattern vias?
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
  • Replies 31 replies
  • Subscribers 181 subscribers
  • Views 2875 views
  • Users 0 members are here
Related

Wot, still no package land pattern vias?

Former Member
Former Member over 11 years ago

The one thing I expected to be fixed in v7 was vias in land patterns. Nope, still AWOL, in spite of a glaring need for thermal transfer to ground via the center pad on some parts. What gives? When is this coming?

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 9/18/2014 10:58 PM, Ryan Pettigrew wrote: The one thing I expected to be fixed in v7 was vias in land patterns. Nope, still AWOL, in spite of a glaring need for thermal transfer to ground via the center…
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 9/18/2014 10:58 PM, Ryan Pettigrew wrote:

    The one thing I expected to be fixed in v7 was vias in land patterns.

    Nope, still AWOL, in spite of a glaring need for thermal transfer to

    ground via the center pad on some parts. What gives? When is this

    coming?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/126808

     

     

    Hi Ryan,

     

    This is already possible. Here's what you would do:

     

    In the package:

     

    1. Place the thermal transfer through-hole pads(pads and vias are

    physically the same thing, the distinction we make in EAGLE is that pads

    are always associated with components and go through the hole board,

    vias are on the board and generally associated with transitions between

    layers).

     

    2. Draw polygons enclosing these pads on the Top, Bottom, tStop, bStop,

    tCream, and bCream layers. My assumption here is that the thermal pad

    shows up on both sides of the board, this isn't always the case but for

    the sake of generality I've included them here.

     

    3. In the device editor, assign all of those pads to the same pin of

    your symbol, because they're within the boundaries of the polygon the

    polygon is considered an extension of those pads.

     

    That's pretty much all you have to do, and EAGLE will handle it without

    errors. Section 8.14 of the EAGLE manual covers this in greater

    detail.The Help pages for PAD and SMD provide more details

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    That's pretty much all you have to do, and EAGLE will handle it without

    errors. Section 8.14 of the EAGLE manual covers this in greater

    detail.The Help pages for PAD and SMD provide more details

     

    Jorge, the problem is, you can't then assign it to the via layer, with all the other vias, where it belongs, and where it is convenient for the board assembler to find it, and know what it is, and what its purpose is supposed to be.

     

    I reiterate; I am NOT interested in ways of working around this problem; I am interested in this problem being fixed, so no workaround is required. If I wanted help getting around this limitation in the software, I would have posted in the help forum, not here in the suggestion forum.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    Besides, Eagle has a lot more important issues to fix first.

    The importance of an issue to be fixed is a matter of opinion, not of fact, and is no justification for an issue to not be fixed. Until Cadsoft decides to have a vote on which feature to fix next, opinions like this are better kept to yourself.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

     

    Regarding tenting/via plugging, there are several methods to do that. It

    could be copper fill and stop mask fill in different ways. Both are

    manufacturer specific, and not something you can expect from a general pcb

    manufacturer. Only some manufacturers can do it reliable for the type of

    heat transfer we talk about. Eagle should not behave as this was an obvious

    thing to do. As with other packages, you need to define a package that suits

    your pcb manufacturer and pick and place manufacturing process.

     

    And I was not complaning about anything. I have learnt the lessons from real

    life and I see its up to the designer, not Eagle, to do this right. I can

    not see a general via placement in the package could solve all the

    manufacturing methods I know, so why bother Cadsoft with it. So far, Eagle

    allows me to manually change paste and stop masks as I need to.

     

    The diagonal fill you link to is fine, but thats not the method I use. The

    most important issue you need to think about is that solder doesnt get

    sucked into unplugged vias, and that your paste doesnt trap pockets of air

    that will pop during soldering. I used all kinds of openings myself. The

    favorite is the "+" shaped between vias, but diagonals may be good too. (I

    favor the "+" because that allows stencil detail stiffness, because the

    details doesnt get too long and thin and reduce its lifetime, wich I would

    question in the diagonal type.) Then you need to make sure there is not too

    much or too little solder stuck under it. Too much will lift it and in worst

    case end up with pads in the air, or too little gives bad heat transfer.

     

    To summarize, Eagle already offers what you need to do thermal vias. Imo,

    what you ask is not a general improvement, but a manufacturer spesific.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    To summarize, Eagle already offers what you need to do thermal vias. Imo,

    what you ask is not a general improvement, but a manufacturer spesific.

    Nonsense. All I am asking for is for actual vias to be available on the actual via layer in a Land Pattern. There's NOTHING manufacturer specific about that. It's a needless omission to the software, and should be fixed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    "Ryan Pettigrew"  skrev i nyhetsmeldingen:

    1860534984.341411648578570.JavaMail.jive@flmspu-csapp-02.premierfarnell.com

    ...

     

    CadSoft Guest wrote:

    To summarize, Eagle already offers what you need to do thermal vias.

    Imo,

    what you ask is not a general improvement, but a manufacturer

    spesific.

    Nonsense. All I am asking for is for actual vias to be available on the

    actual via layer in a Land Pattern. There's NOTHING manufacturer

    specific about that. It's a needless software specific omission, and

    should be fixed.

     

    OK, lets just agree to disagree then. I've never seen a manufacturer care if

    its a via or pin through hole in my life, and I still don't get why they

    should.

    I give them a drill layer and a drill tool set, and they can filter drill

    diameter if they want to. One time I accidentially left 0.6mm microvias on a

    board, and they of course wanted to change them into 0.1mm, so they do check

    for their DFM rules.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    OK, lets just agree to disagree then.

    I'll agree to that so long as you agree to do your disagreeing in some other thread. Just because a manufacturer is willing to work around the flawed output, that doesn't mean it doesn't need to be fixed; nor does having a board successfully made with the existing files justify the status quo as not needing to be changed. I shouldn't have to depend on human intervention to get my board made correctly, and failing that, only as little intervention as possible should be required. Eliminating the misidentification of vias as through holes is an important step in keeping the mistakes of humans at bay. The ideal to strive for is NOT a successfully made board! The ideal to strive for is a successfully made board manufactured WITHOUT human intervention! This requires that as much of the construction details as possible be both present and correct in the board design file, including whether something is a via, or a through hole. If my manufacturer wants a separate file for vias that indicates which are to be filled, which are to be over-plated, and which are to be left empty, the software should accommodate them! It shouldn't be up to the manufacturer to adapt to the software! That's how support for software gets dropped; manufacturers calling it quits with a design file that refuses to keep up!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 2014-09-24 14:03:42 +0000, Morten Leikvoll said:

    Sometimes I have just left out the themal pads, but put a note on doc

    layer that I need to add via's manually,

     

    you can always get around it by making a special package for it, with a

    "add thermal via" self notification on a doc layer.

     

    I think you're missing his point.

     

    A great deal of work with Eagle involves "get around it by" and "make a

    note of" and "ignore/approve the DRC here" and other workarounds and

    hacks.

     

    Eagle is a mature product and there is a very large and growing list of

    BASIC features which we, the loyal Eagle user, is having to work around

    in order to use Eagle for what is becoming standard board designs. It's

    frustrating to keep hearing responses like "just do this" or "you can

    get around it by" or my personal favourite, "write a script" -- It's

    true that Eagle's power lies in its ability to script your way around

    (some) limitations, but the scripting language itself has some HUGE

    deficiencies which make the "just script it" answer unworkable because

    it involves me typing out net/part/class names (instead of being able

    to select or tab-complete) or otherwise interrupting a normal routing

    workflow.

     

    I believe THIS is the point that Ryan is trying to make.

     

    -A.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 2014-09-25 01:33:52 +0000, Ryan Pettigrew said:

    comfortable with the idea of the manufacturer seeing a via and checking

    notes for fill and over-plating, than seeing a through-hole, and hoping

    he'll figure out that it's supposed to be a via, and then do the

    additional checks.

     

    Your board manufacturer looks at your Eagle files (instead of the

    gerbers)? I've never had a board manufacturer want anything more than

    the gerbers, and on the gerbers there is absolutely no difference

    between (through-board) via and a pad. Could you elaborate?

     

    -A.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    No, I'm afraid I can't. Suffice it to say, though, if my board manufacturer wants a Gerber of the Via layer, I don't want to make excuses for not giving it to them. And I certainly shouldn't have to make excuses on the behalf of a piece of software.

     

    And it's not like vias don't have to be redone anyway. I was talking to someone last week who was using Diptrace, and wondered if he should be using Eagle. I was mentioning the footprint via issue, and someone nearby showed him a board he just had done, and commented that the vias on it were the smallest that Eagle could do. He responded, more or less, "What? That's all? I just had a board rejected from the manufacturer because the vias I wanted were too small!". I'm pretty sure he stopped worrying about his choice of software after that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    "Ryan Pettigrew"  skrev i nyhetsmeldingen:

    831887068.431415681396399.JavaMail.jive@flmspu-csapp-02.premierfarnell.com

    ...

     

    And it's not like vias don't have to be redone anyway. I was talking to

    someone last week who was using Diptrace, and wondered if he should be

    using Eagle. I was mentioning the footprint via issue, and someone

    nearby showed him a board he just had done, and commented that the vias

    on it were the smallest that Eagle could do. He responded, more or less,

    "What? That's all? I just had a board rejected from the manufacturer

    because the vias I wanted were too small!". I'm pretty sure he stopped

    worrying about his choice of software after that.

     

    And the point is?

    Eagle doesnt have a minimum via size that I know of. I've even used

    microvias of 0.1mm (they are laserdrilled), and never had this intial

    problem of this thread. I suspect your choise of manufacturer is the issue.

    They should not care if its a via or pad as they are manufactured the same

    way. PCB manufacturers are all different. Making pcb's is not a

    straightforward job easily described in one single file.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 2014-11-11 04:49:26 +0000, Ryan Pettigrew said:

    No, I'm afraid I can't. Suffice it to say, though, if my board

    manufacturer wants a Gerber of the Via layer, I don't want to make

    excuses for not giving it to them. And I certainly shouldn't have to

    make excuses on the behalf of a piece of software.

     

    Interesting. I can't think of a scenario where a board manufacturer

    would want to distinguish vias from any other plated/drilled hole

    except in instances where they want to easily change the drill/annulus

    of ONLY vias.

     

    If my board manufacturer wanted me to supply a layer that contained the

    pads for every 0805 component only, I'd be hard-pressed to provide that

    using ANY EDA package. The fact that you can't elaborate seems to

    indicate that there isn't actually a real use-case where this would be

    necessary.

     

    Not trying to throw stones (see my own posts in e.s.e), just trying to

    understand the requirement.

     

    -A.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 2014-11-11 04:49:26 +0000, Ryan Pettigrew said:

    No, I'm afraid I can't. Suffice it to say, though, if my board

    manufacturer wants a Gerber of the Via layer, I don't want to make

    excuses for not giving it to them. And I certainly shouldn't have to

    make excuses on the behalf of a piece of software.

     

    Interesting. I can't think of a scenario where a board manufacturer

    would want to distinguish vias from any other plated/drilled hole

    except in instances where they want to easily change the drill/annulus

    of ONLY vias.

     

    If my board manufacturer wanted me to supply a layer that contained the

    pads for every 0805 component only, I'd be hard-pressed to provide that

    using ANY EDA package. The fact that you can't elaborate seems to

    indicate that there isn't actually a real use-case where this would be

    necessary.

     

    Not trying to throw stones (see my own posts in e.s.e), just trying to

    understand the requirement.

     

    -A.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    If my board manufacturer wanted me to supply a layer that contained the

    pads for every 0805 component only, I'd be hard-pressed to provide that

    using ANY EDA package.

    Well yeah, but while Eagle doesn't have a layer called "SMT Components"; it does have a layer called "Via", which, in theory, should have all the vias on it; and if it did, like it should, I could easily give the manufacturer what they want. Everyone suggests I use the through-hole tool; if I could then assign the through-hole to the Via layer, where it belongs, I'm sure the board manufacturer would take the hint, obtuse as it is; but currently, that doesn't work. I'm merely asking for the practice to match the theory, so any board manufacturers will understand the construction of my board.