EAGLE User Support (English) OSX Yosemite and slow zooming with 6.6.0
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
  • Replies 9 replies
  • Subscribers 183 subscribers
  • Views 742 views
  • Users 0 members are here
Related

OSX Yosemite and slow zooming with 6.6.0

autodeskguest
autodeskguest over 11 years ago

I've updated my OS to 10.10 and while everything went smoothly, I have

noticed that Eagle 6.6.0 now absolutely CRAWLS when it comes to zooming.

 

The best description I can give is that the zoom (particuarly zooming

out) "lags" behind the trackpad.  e.g. if I have a board file open and

zoom out to show more of the board, I may have only pinched my fingers

together on the trackpad for 1/3s, but it takes the GUI a good 2 or 3

seconds to stop zooming out.

 

Panning is still very fast, but the zoom is now very very very slow.

 

I've tried turning off transparency in the system preferences but this

had no effect. On the off chance that it was something very obscure I

also reset the NVRAM and did an SMC reset of the mac.  It's a 2012 core

i7 Macbook Air with 8GB of memory, so the machine itself is no slowpoke

and no other application appears to have this issue.

 

I do not yet have Eagle 7.1.0, although I am downloading it currently

to test. I'm not yet ready to upgrade, and in all honestly I don't

think I will upgrade. 7.1.0 does not have any new features that I would

like, so the $700 price tag is not at all appealing. It's a pity, I've

been a very happy user of Eagle for over a decade now, but that's the

subject for another post...

 

Has anyone else seen this? Does anyone have any suggestions on what to

try or how to gather more information to help the Eagle development

team figure out what's going on?

 

Regards,

Andrew

 

 

  • Sign in to reply
  • Cancel
Parents
  • SouthernAtHeart
    SouthernAtHeart over 11 years ago

    Is there any update of a fix for the sluggish zooming?  It is very frustrating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • SouthernAtHeart
    SouthernAtHeart over 11 years ago

    Is there any update of a fix for the sluggish zooming?  It is very frustrating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 11 years ago in reply to SouthernAtHeart

    Nothing yet,

     

    But developers are wearing down their fingers typing as we speak,

    towards V7.3 which should bring relief.

     

    As soon as something is available, I will reply to this thread with a

    link, to the first beta so that you guys can check to make sure this is

    improved.

     

    hth,

    Jorge Garcia