Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Controlling Main Breaker (150 amp ) using arduino
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 2783 views
  • Users 0 members are here
  • contactor
  • main_power
  • breaker
  • arduino
  • 150amp
Related

Controlling Main Breaker (150 amp ) using arduino

e14 Contributor
e14 Contributor over 11 years ago

Hello there ,

 

i've been digging around on how to control my home main breaker(150 amp )  using arduino ( i asked my local lawyer , and he said it's legal ).

and i asked electrician "how can i do my project" he  told me that i need to get 150 amp Contactor (this : lsIS_GMC_09_12_18_22_32.jpg_220x220.jpg)

But now i'm stuck, how to control this using my arduino uno ? i dig even more and somebody told me i need to use SSR as following  [Arduino>SSR>Contactor>Main Breaker] but i'm confused i need a true expert who can guide me to the right answer ( which i believe he will be from element14 community ) .

  • Sign in to reply
  • Cancel
Parents
  • aldenridge
    aldenridge 5 months ago

    Controlling a 150A main breaker with an Arduino is not done directly in real electrical practice. The Arduino should never be connected to the high-current path or anything related to the breaker terminals. The correct method is to control a properly rated contactor, and even then only its low-voltage coil side.

    Most 150A contactors use a 24V AC or DC coil. Since an Arduino UNO only outputs 5V logic signals, an intermediate switching stage is required, such as a relay module or a transistor with opto-isolation. This stage safely switches the 24V coil circuit, which then energizes the contactor. The contactor itself handles the actual load switching on the mains side.

    The idea of using an SSR between Arduino and contactor is often misunderstood. SSRs are generally used for directly switching certain AC loads, but they are not required for driving a contactor coil and can introduce unnecessary complexity.

    In proper installations, all high-current wiring and protection devices remain inside a certified electrical enclosure. Only the low-voltage control lines are exposed to automation logic. A licensed electrician should always handle integration at the distribution panel level.

    A useful reference for safe installation practices and professional wiring approaches can be found through Electrician Singapore, which is a Singapore-based electrical service resource that reflects how controlled load switching is typically implemented in real residential environments.

    Overall, Arduino should be limited to control logic only, while certified electrical hardware manages all mains switching safely.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • aldenridge
    aldenridge 5 months ago

    Controlling a 150A main breaker with an Arduino is not done directly in real electrical practice. The Arduino should never be connected to the high-current path or anything related to the breaker terminals. The correct method is to control a properly rated contactor, and even then only its low-voltage coil side.

    Most 150A contactors use a 24V AC or DC coil. Since an Arduino UNO only outputs 5V logic signals, an intermediate switching stage is required, such as a relay module or a transistor with opto-isolation. This stage safely switches the 24V coil circuit, which then energizes the contactor. The contactor itself handles the actual load switching on the mains side.

    The idea of using an SSR between Arduino and contactor is often misunderstood. SSRs are generally used for directly switching certain AC loads, but they are not required for driving a contactor coil and can introduce unnecessary complexity.

    In proper installations, all high-current wiring and protection devices remain inside a certified electrical enclosure. Only the low-voltage control lines are exposed to automation logic. A licensed electrician should always handle integration at the distribution panel level.

    A useful reference for safe installation practices and professional wiring approaches can be found through Electrician Singapore, which is a Singapore-based electrical service resource that reflects how controlled load switching is typically implemented in real residential environments.

    Overall, Arduino should be limited to control logic only, while certified electrical hardware manages all mains switching safely.