EAGLE User Support (English) How to update board layout with new components?
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 4220 views
  • Users 0 members are here
Related

How to update board layout with new components?

Former Member
Former Member over 10 years ago

Hi,

couldn't find anything how to update the board layout with new components added (replaced) in the schematic layout (Version Eagle 7.2.0 light).

 

E.g I have added a connector and deleted another one. CR check tells me the deleted part is missing in the schematic and the new component is missing on the board.

 

So - eagle knows whats wrong but how can I update the board automatically?

 

thanks for any hint

 

Cheers

Rainer

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    It looks like you broke the consistency of the schematic /Board pair by

    editing without both editors being open. With both open, now, you can

    confirm this, there will be a red (ish) dot in the lower right status bar.

    Normally it should be green when the schematic and board are  consistent.

     

    There is no automatic repair. It's probably to late to use undo. You need

    to manually get the board and schematic consistent by deleting where one

    exists in one editor and not the other.

     

    When deleting you may need to do this with only that editor open.

     

    Perform an ERC check at each step, eventually the two will be consistent.

    Once at that point, add the required (missing) parts in the schematic. The

    part footprints (elements) will then be available in the board where you

    will need to place and route them.

     

    In future you can change packages and devices if you right click on the

    symbol in schematic or element in Board.

     

    HTH

    Warren

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    Hi,

     

    thanks for your help.

     

    It seems that there is a problem (I) using the Autorouter.

    ERC check is OK, run Autorouter (medium) and still everything is OK. Click on EVALUATE and move a component in the board layout. restart Autorouter and ERC errors appears.

     

    Part X10 has inconsistent package in layout and board.

     

    How can I fix this?

     

    many thanks for any hint

     

    Rainer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to Former Member

    Somehow the link is now fixed again - schematic and board are now synced with no errors.