Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Drill file changes from 4 digit to 5 digit randomly (seemingly)?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 484 views
  • Users 0 members are here
Related

Drill file changes from 4 digit to 5 digit randomly (seemingly)?

e14 Contributor
e14 Contributor over 11 years ago

Hi All,

 

     I've had the occasional problem here with my drill file seemingly to randomly generate files that are way out of bounds.  For example, on a board that is .75 x 1.2 inches, I get drill values out in the 11" range.  As reported by both gcpreview, and 4pcb dfm...

 

Only on a few boards.   Usually the small ones.

 

Anyone know where I should start looking for the problems?

 

Thanks!


Jason

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 4/5/2015 2:03 PM, jason winters wrote:

    Hi All,

     

          I've had the occasional problem here with my drill file seemingly

    to randomly generate files that are way out of bounds.  For example, on

    a board that is .75 x 1.2 inches, I get drill values out in the 11"

    range.  As reported by both gcpreview, and 4pcb dfm...

     

    Only on a few boards.   Usually the small ones.

     

     

    Hi Jason,

     

    I hope you're doing well. The issue lies with the gerber viewers not

    EAGLE. As of Version 7.2 excellon files default to 2.5 precision instead

    of the 2.4 in previous versions of EAGLE.

     

    Gerber viewers take a guess at the format if you don't specify it. With

    small boards the tendency is for them to make a mistake.

     

    If you let the gerber viewer know what the file format is at the time of

    import, you'll see that everything comes in correctly.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    Hey Jorge,

     

       Thanks for the reply.  I'm still not sure what to make of this, as the PCB house has the same issue, so it's not just a viewer.   However, I re-installed eagle 7.2 about an hour ago, and now it works fine again...   Yes, I had switched to a 2.5 precision when 7.2 came out, as that bit me hard (but I could duplicate it by going back to 7.1, so was able to debug it by comparing output files).


    So, I'd have to say it _does_ have something to do with eagle...   something is being trashed somewhere!

     

    Thanks!


    Jason

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    Hey Jorge,

     

       Thanks for the reply.  I'm still not sure what to make of this, as the PCB house has the same issue, so it's not just a viewer.   However, I re-installed eagle 7.2 about an hour ago, and now it works fine again...   Yes, I had switched to a 2.5 precision when 7.2 came out, as that bit me hard (but I could duplicate it by going back to 7.1, so was able to debug it by comparing output files).


    So, I'd have to say it _does_ have something to do with eagle...   something is being trashed somewhere!

     

    Thanks!


    Jason

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    Well, since it appears to be an Eagle issue, they aren't interested.

     

    I did find one problem... in the library supplied with Eagle (con-lstb), it is causing the problem.  I then tried modifying text (just something to change) in the library so it re-wrote it, and it started working again.  So apparently not all of the libraries have been updated?  Ah well.  Have a work around now, so that's good.

     

    Cheers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14 Contributor

    On 4/6/2015 3:54 PM, jason winters wrote:

    Hey Jorge,

     

        Thanks for the reply.  I'm still not sure what to make of this, as

    the PCB house has the same issue, so it's not just a viewer.   However,

    I re-installed eagle 7.2 about an hour ago, and now it works fine

    again...   Yes, I had switched to a 2.5 precision when 7.2 came out, as

    that bit me hard (but I could duplicate it by going back to 7.1, so was

    able to debug it by comparing output files).

     

    Hi Jason,

     

    Who at the PCB house is having the same issue? If it a sales rep, I

    would lean on the side of user error. This a rather subtle issue and in

    many cases reps are not aware of it. If the engineering or manufacturing

    departments are raising the flag then we would have to look into their

    setup.

     

    If you specify the format explicitly then everyone should see the same

    thing.

     

    hth,

    Jorge Garcia