Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Pad with complex hole
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 691 views
  • Users 0 members are here
Related

Pad with complex hole

eugeny
eugeny over 11 years ago

Hello, connector has its through-hole chassis pin 2.4 x 1 mm size, what is the right way to create pad for it?

SMD pad with holes give errors, hole without pad leaves space with no copper around the hole (0.2 mm clearance is required by PCB manufacturer).

Please advise.

  • Sign in to reply
  • Cancel
Parents
  • e14candies
    e14candies over 11 years ago

    Your description is not clear to offer full help..

    You say the shape of the pin is 2.4 x 1 mm?   So any round hole must be

    2.4mm for the pin to fit.  This post did not mention center-to-center

    spacing of the pins, this is critical.

    Since this is not a surface mount part, you will not use surface mount

    packages

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • eugeny
    eugeny over 11 years ago in reply to e14candies

    Thanks. Let me rephrase the question.

    I need hole in the PCB of 2.4 x 1 mm size with plating around it (but better with plating in it like in pad).

     

    As you see this is not a round hole.

    It has nothing to do with spacing, pitch or whatever.

    I just need one hole of defined size and defined properties at the center of the 10 x 10 mm PCB.

    Do not ask me why image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • eugeny
    eugeny over 11 years ago in reply to e14candies

    Thanks. Let me rephrase the question.

    I need hole in the PCB of 2.4 x 1 mm size with plating around it (but better with plating in it like in pad).

     

    As you see this is not a round hole.

    It has nothing to do with spacing, pitch or whatever.

    I just need one hole of defined size and defined properties at the center of the 10 x 10 mm PCB.

    Do not ask me why image