Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Pad with complex hole
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 189 subscribers
  • Views 682 views
  • Users 0 members are here
Related

Pad with complex hole

eugeny
eugeny over 11 years ago

Hello, connector has its through-hole chassis pin 2.4 x 1 mm size, what is the right way to create pad for it?

SMD pad with holes give errors, hole without pad leaves space with no copper around the hole (0.2 mm clearance is required by PCB manufacturer).

Please advise.

  • Sign in to reply
  • Cancel
  • e14candies
    e14candies over 11 years ago

    By the way it sounds like you are trying to create this internal "hole"

    using the dimension layer.  I don't know if that it really correct, since

    this should be used to form the "outer" border/perimeter of the pcb.  I

    suspect any copper crossing over the dimension border will always generate

    an error.

     

    Perhaps you should generate your "hole" using the layer 47 "milling".  I'm

    just tossing out thoughts, since I haven't used layer 47 myself.

     

    In fact I just now searched the word "milling" & found this post, you may

    like:

     

    Eagle CAD Non-circle through hole pads?

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14candies
    e14candies over 11 years ago

    You could triple check you layout & just bluntly approve this error & move

    ahead with the work. 

     

    Or, you might need to adjust your min allowable "dimensions" in the various

    DRC configuration tabs  (PCB, TOOLS==>DRC).  Or set up a special class for

    this net.  I'm sure others will weigh in with even better proposals.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • eugeny
    eugeny over 11 years ago in reply to e14candies

    Norm, thank you very much for

    >Putting copper on the top (and bottom)SURFACES by force is simple, just place a "wire"

    I did not think about such solution - I was trying SMD pads or polygons.

    However your solution gives "dimension" error in DRC - both for circular hole (drill) and for any shape drawn in dimension layer. Is there any approved way for having same result, but without error?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14candies
    e14candies over 11 years ago

    Sadly, the picture link is not working (website is temp broken), maybe it

    will come back in a few hours.

     

    Since I can't see anything, I'm assuming you plan to "drill" the

    non-circular hole using laser cutting, since it is not a "hole" in the

    sense of Eagle, I'm not sure how you can force the interior edge of the

    hole to be plated from topside to bottom.

     

    Putting copper on the top (and bottom)SURFACES by force is simple, just

    place a "wire" (use wire selection in pcb drawing) having the width,

    dimensions, and position you desire over the "hole".  To minimize false

    errors, give the wire the same net name as the net associated with your

    "hole".

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • eugeny
    eugeny over 11 years ago in reply to e14candies

    Thanks. Let me rephrase the question.

    I need hole in the PCB of 2.4 x 1 mm size with plating around it (but better with plating in it like in pad).

     

    As you see this is not a round hole.

    It has nothing to do with spacing, pitch or whatever.

    I just need one hole of defined size and defined properties at the center of the 10 x 10 mm PCB.

    Do not ask me why image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14candies
    e14candies over 11 years ago

    Your description is not clear to offer full help..

    You say the shape of the pin is 2.4 x 1 mm?   So any round hole must be

    2.4mm for the pin to fit.  This post did not mention center-to-center

    spacing of the pins, this is critical.

    Since this is not a surface mount part, you will not use surface mount

    packages

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.