Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Export Schematic Image in High Resolution
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 190 subscribers
  • Views 6609 views
  • Users 0 members are here
  • board
  • layout
  • image
  • schematic
  • export
Related

Export Schematic Image in High Resolution

e14 Contributor
e14 Contributor over 11 years ago

Hello all.

 

I'm here to ask a question. I'm a member of a big project and to not confused about how the project works, I will do a PDF file explaining how all project works. But when I export the shematic image by using comand File>Export>Image, the image lose almost every high resolution. Whatever if I put 1200dpi, the image still looks horrible. Can anyone help me about this?

  • Sign in to reply
  • Cancel
Parents
  • Morosh
    Morosh over 11 years ago

    download "http://www.cadsoftusa.com/downloads/file/epsdraw.ulp"

    it'll convert schematic to eps format, that you can use in word: insert -->picture --> from file --> xx.eps

     

    HTH

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Morosh

    Thanks a lot. But it is happening an error as you can see on the image.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Morosh
    Morosh over 11 years ago in reply to e14 Contributor

    I made a mistake, there is a newer one epsdraw_411:

    http://www.cadsoftusa.com/downloads/file/epscdraw_411.ulp

     

    HTH

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14candies

    On 6/27/2015 11:19 AM, Hoyt wrote:

    That's one of the potential ongoing problems of requiring an external ulp

    versus having the required functionality built into Eagle itself. Many

    common tasks that could be included are not.

     

     

    Hi Hoyt,

     

    In this case, the issue is likely because the user hard coded scale

    factors, instead of using the conversion functions that ship with EAGLE.

    ULPs that make use of those functions are completely portable between V5

    and newer because the functions have already compensated for the

    improved resolution.

     

    I can't find the origin of this thread, but the high resolution images

    can be achieved without the use of a ULP. You can use the CAM processor

    or the export image option under the file menu.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14candies

    On 6/27/2015 11:19 AM, Hoyt wrote:

    That's one of the potential ongoing problems of requiring an external ulp

    versus having the required functionality built into Eagle itself. Many

    common tasks that could be included are not.

     

     

    Hi Hoyt,

     

    In this case, the issue is likely because the user hard coded scale

    factors, instead of using the conversion functions that ship with EAGLE.

    ULPs that make use of those functions are completely portable between V5

    and newer because the functions have already compensated for the

    improved resolution.

     

    I can't find the origin of this thread, but the high resolution images

    can be achieved without the use of a ULP. You can use the CAM processor

    or the export image option under the file menu.

     

    hth,

    Jorge Garcia