EAGLE User Support (English) SMD package for capacitors 1206 bigger than 1608
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
  • Replies 3 replies
  • Subscribers 179 subscribers
  • Views 667 views
  • Users 0 members are here
  • frontpage
Related

SMD package for capacitors 1206 bigger than 1608

Former Member
Former Member over 10 years ago

Hi,

 

Someone can explain me why when i check the size of SMD 1206 is more bigger than SMD 1608. I don't understand because normally it's the countrary. I use the rcl library.

 

Thank you.

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    Hi,

     

    You appear to be comparing the 'Metric' and 'Imperial' designations of two

    parts, which is leading to some confusion. See this description:

    https://en.wikipedia.org/wiki/Surface-mount_technology

     

    I hope this helps!

     

    John

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    Thank you. I search the dimensions of a SMD package to create my new one. I try to understand which tolerance they use for a SMD package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 29.06.2015 23:45, jmorley@endeavour-usa.com wrote:

    Hi,

     

    You appear to be comparing the 'Metric' and 'Imperial' designations of two

    parts, which is leading to some confusion. See this description:

    https://en.wikipedia.org/wiki/Surface-mount_technology

     

    Note that there is also rather big variations on pad sizes for wave vs

    reflow soldering. Im not sure if this is the issue here tho.