Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Use / switch-to different / new library for all objects in a schematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 178 subscribers
  • Views 215 views
  • Users 0 members are here
  • eagle
  • library
  • 6.6
  • linux
Related

Use / switch-to different / new library for all objects in a schematic

Former Member
Former Member over 10 years ago

Hi,

 

I have created a project library from a project schematic in Eagle 6.6 (Linux).  The library is in the directory with the project files.  Now I would like for the objects in the schematic to use only that library.  I can't find a way to make all of the schematic objects be taken from the new project library.

 

I have turned off all libraries except the new project library and enabled it.  When I look at object properties in the schematic they still refer to the old libraries.

 

Any way to force all objects to use the new library?

 

Thanks!

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 27.08.2015 um 01:47 schrieb Bob Smither:

    Hi,

     

    I have created a project library from a project schematic in Eagle 6.6

    (Linux).  The library is in the directory with the project files.  Now I

    would like for the objects in the schematic to use only that library.  I

    can't find a way to make all of the schematic objects be taken from the

    new project library.

     

    I have turned off all libraries except the new project library and

    enabled it.  When I look at object properties in the schematic they

    still refer to the old libraries.

     

    Any way to force all objects to use the new library?

     

    Thanks!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/158831

     

     

     

    Hi,

     

    the schematic and board file contain the whole library definition:

    In schematic DeviceSymbolPackage, in Board only the Package.

    And it is stored the name of the library where it was taken from.

    That's necessary in case you want to make a library update, for example.

    There is no library linked to schematic and board. The objects do

    not use/need a library in the background.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Thanks Richard - that helps!