Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Adding company part numbers in Eagle that I can access with ULP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1995 views
  • Users 0 members are here
  • number
  • ulp
  • part
Related

Adding company part numbers in Eagle that I can access with ULP

rx8pilot
rx8pilot over 10 years ago

Hello all,

 

I have successfully written my first ULP to format data for my pick and place machine. For the most part I got the data formatted to be a direct import into the machine except for one detail - part numbers.

 

The software in the machine needs to associate every reference designator with a part number. This association tells it what package, reel, value, etc it is. In Eagle, I am not sure how to assign our internal part number to each component so that when it comes time to program the pick and place it can be one swift ULP action to get the data I need.This is also a problem when outputting general purpose BOM's

 

I have been using the same resistor for all the resistors on the PCB of the same package type. Just change the values as needed. This of course is the same for the capacitors as well. What I would like to have is our part number for all the variations of values, tolerance, type, etc.

 

Active and unique parts are seemingly a little easier because I use a specific part in general. This is not always the case though, maybe an MCU with the same package has a number of variants of memory, speed, or whatever.

 

Does anyone have any suggestions or best practices for associating part number with a part that can be output via ULP's to Pick and Place centroid files and BOM's? Hoping there is an easy solution that is hiding in plain site.

 

Thanks in advance for anyone willing to help.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 25/10/15 06:05, Carlos Acosta wrote:

    Hello all,

     

    I have successfully written my first ULP to format data for my pick and

    place machine. For the most part I got the data formatted to be a direct

    import into the machine except for one detail - part numbers.

     

    The software in the machine needs to associate every reference

    designator with a part number. This association tells it what package,

    reel, value, etc it is. In Eagle, I am not sure how to assign our

    internal part number to each component so that when it comes time to

    program the pick and place it can be one swift ULP action to get the

    data I need.This is also a problem when outputting general purpose BOM's

     

    I have been using the same resistor for all the resistors on the PCB of

    the same package type. Just change the values as needed. This of course

    is the same for the capacitors as well. What I would like to have is our

    part number for all the variations of values, tolerance, type, etc.

     

    Active and unique parts are seemingly a little easier because I use a

    specific part in general. This is not always the case though, maybe an

    MCU with the same package has a number of variants of memory, speed, or

    whatever.

     

    Does anyone have any suggestions or best practices for associating part

    number with a part that can be output via ULP's to Pick and Place

    centroid files and BOM's? Hoping there is an easy solution that is

    hiding in plain site.

     

     

    The usual recommended method, these days, is to place the part number as

    an attribute of all components on the schematic or board. That feels

    like another manual step to me, but apparently it's the "right" way.

     

    I still use V4 for some of the work I do, which didn't have attributes.

    For that, I use a variant of the old BoM ULP, which matches both part

    and value against a TSV database of known parts. So where I use an

    R_EU_0805 and set its value to 10K, the BoM ULP produces a different

    part number than if an identical R_EU_0805 has a value of 100K.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rx8pilot
    0 rx8pilot over 10 years ago in reply to autodeskguest

    Thank you for taking the time to post. I was reading about the attributes and did a quick test outputting a ULP. It seems to work quite well for the 'fixed' parts. For the passives with variable attributes - it gets a bit tedious as you pointed out. Do you think it is practical to use the 'variants' for the different values so that I could pick from a list? I have never used variants before so I am not sure if that is even possible.

     

    I am going to take a look at the BOM ULP that uses the external data base to cross ref part numbers. That could be the best long term solution albeit a bit of a setup commitment up front.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rx8pilot
    0 rx8pilot over 10 years ago in reply to autodeskguest

    Thank you for taking the time to post. I was reading about the attributes and did a quick test outputting a ULP. It seems to work quite well for the 'fixed' parts. For the passives with variable attributes - it gets a bit tedious as you pointed out. Do you think it is practical to use the 'variants' for the different values so that I could pick from a list? I have never used variants before so I am not sure if that is even possible.

     

    I am going to take a look at the BOM ULP that uses the external data base to cross ref part numbers. That could be the best long term solution albeit a bit of a setup commitment up front.