Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Adding company part numbers in Eagle that I can access with ULP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1989 views
  • Users 0 members are here
  • number
  • ulp
  • part
Related

Adding company part numbers in Eagle that I can access with ULP

rx8pilot
rx8pilot over 10 years ago

Hello all,

 

I have successfully written my first ULP to format data for my pick and place machine. For the most part I got the data formatted to be a direct import into the machine except for one detail - part numbers.

 

The software in the machine needs to associate every reference designator with a part number. This association tells it what package, reel, value, etc it is. In Eagle, I am not sure how to assign our internal part number to each component so that when it comes time to program the pick and place it can be one swift ULP action to get the data I need.This is also a problem when outputting general purpose BOM's

 

I have been using the same resistor for all the resistors on the PCB of the same package type. Just change the values as needed. This of course is the same for the capacitors as well. What I would like to have is our part number for all the variations of values, tolerance, type, etc.

 

Active and unique parts are seemingly a little easier because I use a specific part in general. This is not always the case though, maybe an MCU with the same package has a number of variants of memory, speed, or whatever.

 

Does anyone have any suggestions or best practices for associating part number with a part that can be output via ULP's to Pick and Place centroid files and BOM's? Hoping there is an easy solution that is hiding in plain site.

 

Thanks in advance for anyone willing to help.

  • Sign in to reply
  • Cancel
  • sande1
    0 sande1 over 8 years ago

    Carlos ,

     

    Right now I am trying to get match the exitsing part numbers for bunch of resistors and capacitors by just changing values on schematic .

    Did you find any solution for this ? I am struck at the same question .

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Carlos Acosta wrote on Sun, 25 October 2015 02:05

    Does anyone have any suggestions or best practices for associating

    part

    number with a part ...

     

     

    I recently added a house part number system to my Eagle BOM generation

    tools.  I allow for two ways to associate private part numbers to parts:

     

    1: The INHOUSE attribute.  This would normally be set in the library, but

    of course can be set in the schematic for one-off uses too.  The private

    part numbers for a number of organizations can be set this way.  For

    example, the string "Acme:12345;MegaCorp:789" specifies that the private

    part number within the Acme organization is 12345, and within MegaCorp is

    789.

     

    2: The BOM generation program tries to find matching parts to the ones in a

    design in a special set of CSV files.  These CSV files have close to the

    same format as the resulting BOM spreadsheets, and are easily generated

    from such BOM spreadsheets after the private part numbers for the

    organization are filled in.  You dig out the private part numbers for the

    parts used in a design, export the data to a CSV file, and from then on the

    BOM utility automatically knows the private part numbers of those parts

    without them having to be in the INHOUSE attribute.  The data in these CSV

    files includes the organization name, so results from multiple

    organizations with different private part numbers can be thrown together.

     

    The CSV_BOM program, which does most of the heavy lifting of BOM creation

    in my system, is run in the Eagle directory for the particular board.  It

    searches up the tree of directories looking for a "housename" file.  It

    reads the first one it finds to get the name of the organization to find

    in-house part numbers for.  Since the boards for each customer are in a

    separate tree, all you have to do is create the housename file once per

    customer, then the BOM tools automatically know which organization any new

    boards belong to.

     

    This all seems to be working correctly, but I haven't updated the Eagle

    Tools release with this new facility yet.  I'm having trouble getting the

    new version of Visual Studio to make 32 bit EXEs when running on a 64 bit

    system, but that's a different issue.  I can try to make this a higher

    priority if there is interest in this.

     

    I have uploaded the eagle_attr.txt file, which documents how my BOM system

    uses various attributes.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    eagle_attr.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rx8pilot
    0 rx8pilot over 10 years ago in reply to autodeskguest

    I have been reading up on this, but not getting too far. It is not yet clear to me how the the "Technologies" and "Attributes" are structured and managed. Do you have any links or other resources that might be more helpful than the user manual?

     

    I also started another thread that is somewhat related - asking about how to get this data out to a file with a ULP. Back to step one, which is how and where to organize the part number data in the first place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Carlos Acosta wrote:

    I have successfully written my first ULP to format data for my pick and

    place machine. For the most part I got the data formatted to be a direct

    import into the machine except for one detail - part numbers.

     

    The software in the machine needs to associate every reference

    designator with a part number. This association tells it what package,

    reel, value, etc it is. In Eagle, I am not sure how to assign our

    internal part number to each component so that when it comes time to

    program the pick and place it can be one swift ULP action to get the

    data I need.This is also a problem when outputting general purpose BOM's

     

    I have been using the same resistor for all the resistors on the PCB of

    the same package type. Just change the values as needed. This of course

    is the same for the capacitors as well. What I would like to have is our

    part number for all the variations of values, tolerance, type, etc.

     

    have a look at "technologies".

     

    Going that way will require to manage the part value using

    "technologies" in the library.

    But you then are able to use an attribute to carry a part number

    depending on the technology/value (or even multiple attributes to

    handle second source)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rx8pilot
    0 rx8pilot over 10 years ago in reply to autodeskguest

    Thank you for taking the time to post. I was reading about the attributes and did a quick test outputting a ULP. It seems to work quite well for the 'fixed' parts. For the passives with variable attributes - it gets a bit tedious as you pointed out. Do you think it is practical to use the 'variants' for the different values so that I could pick from a list? I have never used variants before so I am not sure if that is even possible.

     

    I am going to take a look at the BOM ULP that uses the external data base to cross ref part numbers. That could be the best long term solution albeit a bit of a setup commitment up front.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 25/10/15 06:05, Carlos Acosta wrote:

    Hello all,

     

    I have successfully written my first ULP to format data for my pick and

    place machine. For the most part I got the data formatted to be a direct

    import into the machine except for one detail - part numbers.

     

    The software in the machine needs to associate every reference

    designator with a part number. This association tells it what package,

    reel, value, etc it is. In Eagle, I am not sure how to assign our

    internal part number to each component so that when it comes time to

    program the pick and place it can be one swift ULP action to get the

    data I need.This is also a problem when outputting general purpose BOM's

     

    I have been using the same resistor for all the resistors on the PCB of

    the same package type. Just change the values as needed. This of course

    is the same for the capacitors as well. What I would like to have is our

    part number for all the variations of values, tolerance, type, etc.

     

    Active and unique parts are seemingly a little easier because I use a

    specific part in general. This is not always the case though, maybe an

    MCU with the same package has a number of variants of memory, speed, or

    whatever.

     

    Does anyone have any suggestions or best practices for associating part

    number with a part that can be output via ULP's to Pick and Place

    centroid files and BOM's? Hoping there is an easy solution that is

    hiding in plain site.

     

     

    The usual recommended method, these days, is to place the part number as

    an attribute of all components on the schematic or board. That feels

    like another manual step to me, but apparently it's the "right" way.

     

    I still use V4 for some of the work I do, which didn't have attributes.

    For that, I use a variant of the old BoM ULP, which matches both part

    and value against a TSV database of known parts. So where I use an

    R_EU_0805 and set its value to 10K, the BoM ULP produces a different

    part number than if an identical R_EU_0805 has a value of 100K.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer