Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Adding company part numbers in Eagle that I can access with ULP
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1995 views
  • Users 0 members are here
  • number
  • ulp
  • part
Related

Adding company part numbers in Eagle that I can access with ULP

rx8pilot
rx8pilot over 10 years ago

Hello all,

 

I have successfully written my first ULP to format data for my pick and place machine. For the most part I got the data formatted to be a direct import into the machine except for one detail - part numbers.

 

The software in the machine needs to associate every reference designator with a part number. This association tells it what package, reel, value, etc it is. In Eagle, I am not sure how to assign our internal part number to each component so that when it comes time to program the pick and place it can be one swift ULP action to get the data I need.This is also a problem when outputting general purpose BOM's

 

I have been using the same resistor for all the resistors on the PCB of the same package type. Just change the values as needed. This of course is the same for the capacitors as well. What I would like to have is our part number for all the variations of values, tolerance, type, etc.

 

Active and unique parts are seemingly a little easier because I use a specific part in general. This is not always the case though, maybe an MCU with the same package has a number of variants of memory, speed, or whatever.

 

Does anyone have any suggestions or best practices for associating part number with a part that can be output via ULP's to Pick and Place centroid files and BOM's? Hoping there is an easy solution that is hiding in plain site.

 

Thanks in advance for anyone willing to help.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    Carlos Acosta wrote:

    I have successfully written my first ULP to format data for my pick and

    place machine. For the most part I got the data formatted to be a direct

    import into the machine except for one detail - part numbers.

     

    The software in the machine needs to associate every reference

    designator with a part number. This association tells it what package,

    reel, value, etc it is. In Eagle, I am not sure how to assign our

    internal part number to each component so that when it comes time to

    program the pick and place it can be one swift ULP action to get the

    data I need.This is also a problem when outputting general purpose BOM's

     

    I have been using the same resistor for all the resistors on the PCB of

    the same package type. Just change the values as needed. This of course

    is the same for the capacitors as well. What I would like to have is our

    part number for all the variations of values, tolerance, type, etc.

     

    have a look at "technologies".

     

    Going that way will require to manage the part value using

    "technologies" in the library.

    But you then are able to use an attribute to carry a part number

    depending on the technology/value (or even multiple attributes to

    handle second source)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    Carlos Acosta wrote:

    I have successfully written my first ULP to format data for my pick and

    place machine. For the most part I got the data formatted to be a direct

    import into the machine except for one detail - part numbers.

     

    The software in the machine needs to associate every reference

    designator with a part number. This association tells it what package,

    reel, value, etc it is. In Eagle, I am not sure how to assign our

    internal part number to each component so that when it comes time to

    program the pick and place it can be one swift ULP action to get the

    data I need.This is also a problem when outputting general purpose BOM's

     

    I have been using the same resistor for all the resistors on the PCB of

    the same package type. Just change the values as needed. This of course

    is the same for the capacitors as well. What I would like to have is our

    part number for all the variations of values, tolerance, type, etc.

     

    have a look at "technologies".

     

    Going that way will require to manage the part value using

    "technologies" in the library.

    But you then are able to use an attribute to carry a part number

    depending on the technology/value (or even multiple attributes to

    handle second source)

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rx8pilot
    0 rx8pilot over 10 years ago in reply to autodeskguest

    I have been reading up on this, but not getting too far. It is not yet clear to me how the the "Technologies" and "Attributes" are structured and managed. Do you have any links or other resources that might be more helpful than the user manual?

     

    I also started another thread that is somewhat related - asking about how to get this data out to a file with a ULP. Back to step one, which is how and where to organize the part number data in the first place.