EAGLE User Support (English) Search/Find an element, how???
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
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 180 subscribers
  • Views 2064 views
  • Users 0 members are here
  • find
  • run
Related

Search/Find an element, how???

Joop14
Joop14 over 10 years ago

In the schematic editor, when I press Ctl-F, I get the dialog from the ULP "find".

My question is, how do I search for an element that has a value that contains the string "J113"?

Wildcards like * or ? don't seem to work. When I type the exact value PMBFJ113, it finds the element.

When I type J113 or *J113*, it doesn't find anything. What am I doing wrong?

 

Kind Regards,

 

Joop

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    You should try xfind.ulp. Bind it to Ctrl-F and life just became a little easier.

     

    http://www.cadsoftusa.com/downloads/file/xfind.ulp

     

    Eric

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Joop14
    0 Joop14 over 10 years ago in reply to autodeskguest

    Thanks!

     

    What I don't understand however, is why Cadsoft is not able to update / maintain their ulp's. Many of them need improvement, or they stopped working since version 7.

     

    Instead of adding connections with online parties, Cadsoft should work on the core of Eagle and their ulp's.

    For example:

     

    - board mirror view

    - exceptions for thermals in polygons

    - check used libraries / report missing libraries and inconsistencies during "update from libray" something like: Eagle library check

    - restrict layers for inner layers

    - LTSpice export on Linux

    - locale for printf() in ULP

    - after smash, properties of names and values are not updated from library anymore

    - save last modification date-time stamp in brd and sch file

    - X-ref for busses

     

    Wake-up Cadsoft team!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Joop14

    On 10/29/2015 9:55 AM, Joop14 wrote:

    Thanks!

     

    What I don't understand however, is why Cadsoft is not able to update /

    maintain their ulp's. Many of them need improvement, or they stopped

    working since version 7.

     

    Instead of adding connections with online parties, Cadsoft should work

    on the core of Eagle and their ulp's.

    For example:

     

    - board mirror view

    This is possible with the mirror-board.ulp that ships with EAGLE

    - exceptions for thermals in polygons

    There's a couple of ways to handle this already. For example within the

    library you can specify if certain pads should always use solid

    connections by unchecking the thermals box for the pad. The downside of

    that is that the pad always needs to be treated the same way.

     

    Another way to do that would be a polygon within a polygon, with the

    internal polygon having thermals off. Neither way is super nice but they

    work.

    - check used libraries / report missing libraries and inconsistencies

    during "update from libray" something like: Eagle library check

    (http://www.teuniz.net/eagle/eaglelibcheck/)

    +1, This one has gotten some movement lately but I wasn't involved in

    the final determination of EAGLE's roadmap so I don't know if that's in

    there.

    - restrict layers for inner layers

    +1, I personally think it would be cleaner if polygons could assume some

    sort of restrict property that way you wouldn't need a separate layer.

    - LTSpice export on Linux

    +1

    - locale for printf() in ULP

    Not sure I understand this one, could you elaborate?

    - after smash, properties of names and values are not updated from

    library anymore

    I don't think this would be a good idea. Generally if you are assigning

    values in the schematic or board, you would not want a library update to

    change them. Could create confusion, unless I'm misunderstanding what

    you're asking for.

    - save last modification date-time stamp in brd and sch file

    This is already possible with the >LAST_DATE_TIME text variable. It

    updates every time you save the file, or are you asking for something else.

    - X-ref for busses

    This one is odd to me as well. In the case of a single net the XREF

    makes sense since you want to easily find other instances of that net. A

    bus however is a collection of nets, so I find an X-ref for a bus less

    useful since it's doesn't aid in finding a particular signal.

    Additionally, Bus labels can get pretty long so I'm sure there are cases

    where this would be inconvenient.

     

    The idea behind these comments is to show that if some form of

    workaround exists even if it's not the most convenient that usually

    makes a given feature medium to low prio. In the case of others I

    totally agree that we need them but determining priorities is very

    difficult because everyone has a different opinion and some of the

    heaviest opinions aren't coming from technical staff.

     

    I'm happy to see that first time ever we are really adding features

    progressively throughout a major version, instead of having the lions

    share up front and then sticking to bugfixes and minor tweaks as a

    version aged. Maybe some of the new stuff isn't all up your alley, but

    other users do find it useful.

     

    Thank you for your input we really appreciate.

     

    Best Regards,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Joop14
    0 Joop14 over 10 years ago in reply to autodeskguest

    Hello Jorge, I hope you are doing well.

     

    First of all, thank you for responding, I appreciate it.

     

    CadSoft Guest wrote:

     

    On 10/29/2015 9:55 AM, Joop14 wrote:

    Thanks!

     

    What I don't understand however, is why Cadsoft is not able to update /

    maintain their ulp's. Many of them need improvement, or they stopped

    working since version 7.

     

    Instead of adding connections with online parties, Cadsoft should work

    on the core of Eagle and their ulp's.

    For example:

     

    - board mirror view

    This is possible with the mirror-board.ulp that ships with EAGLE

    I don't like the fact that mirror-board act on the actual content of the board.

    Also, all coordinates are wrong when using this ulp to mirror the board.

     

    - exceptions for thermals in polygons

    There's a couple of ways to handle this already. For example within the

    library you can specify if certain pads should always use solid

    connections by unchecking the thermals box for the pad. The downside of

    that is that the pad always needs to be treated the same way.

     

    Another way to do that would be a polygon within a polygon, with the

    internal polygon having thermals off. Neither way is super nice but they

    work.

    I'll try that.

     

    - locale for printf() in ULP

    Not sure I understand this one, could you elaborate?

    When you print the value of a float or double in a formatted string with printf(), the decimal separator will

    be a dot or a comma, depending on the locale settings of the pc i.e. in the US it will print 1.23 and in most

    countries in Europe it will print 1,23. This causes big problems, for example when printing values to a file

    in csv format.

     

    - after smash, properties of names and values are not updated from

    library anymore

    I don't think this would be a good idea. Generally if you are assigning

    values in the schematic or board, you would not want a library update to

    change them. Could create confusion, unless I'm misunderstanding what

    you're asking for.

    When I change a library (for example, I change the text size of the name and value) and then I do an

    update from library in a schematic, size of text of name and value of all instances will be updated, apart

    from the ones that are smashed. Why?

    Smash should only detach the name and value labels from the element for their position.

    Appearantly, it looses the ability to get updated from library.

     

    - save last modification date-time stamp in brd and sch file

    This is already possible with the >LAST_DATE_TIME text variable. It

    updates every time you save the file, or are you asking for something else.

    Eagle uses the date/time when it was last saved, not necessarily modified.

    The difference is subtle but important.

    For example, when I copy the file to another destination, the save date/time in Eagle changes

    but there are no modifications compared with the original.

    Another example, I send a copy of a schematic to somebody via email.

    He receives the schematic and saves it on his pc. The save date/time will be different despite the file

    has not been modified.

    What I would like to see is that Eagle stores the last modification date/time stamp in the schematic/board

    files. This will make it more clear if a file has been altered or not.

     

    - X-ref for busses

    This one is odd to me as well. In the case of a single net the XREF

    makes sense since you want to easily find other instances of that net. A

    bus however is a collection of nets, so I find an X-ref for a bus less

    useful since it's doesn't aid in finding a particular signal.

    Additionally, Bus labels can get pretty long so I'm sure there are cases

    where this would be inconvenient.

    As an example, I have an MCU with an 8-bit parallel databus in sheet 4. The datalines are attached to a bus

    with the name "databus". The bus suddenly stops at the border without any indication.

    In sheet 12 I draw the same bus with name "databus" where the datalines are connected to another chip.

    After printing the schematic, when reading sheet 4, how does one know where to find the other end of the bus?

     

     

    What about the broken IDF export?

     

    http://www.element14.com/community/thread/43949/l/idf-export-broken?displayFullThread=true

     

     

    Kind Regards,

     

    Joop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kikoun
    0 kikoun over 10 years ago in reply to Joop14

    Hi,

    CadSoft Guest wrote:

    On 10/29/2015 9:55 AM, Joop14 wrote:

    Thanks!

    What I don't understand however, is why Cadsoft is not able to update /

    maintain their ulp's. Many of them need improvement, or they stopped

    working since version 7.

    Instead of adding connections with online parties, Cadsoft should work

    on the core of Eagle and their ulp's.

    For example:

    - board mirror view

    This is possible with the mirror-board.ulp that ships with EAGLE

    I don't like the fact that mirror-board act on the actual content of the board.

    Also, all coordinates are wrong when using this ulp to mirror the board.

    Me too, when I need a mirrored view of a board, it's only because I have a board on my desk, and need to find a part or a net to put an oscilloscope on it. I don't want to change my board , certainly not !!

    I just need a mirrored view of it, simply because in real life, after designing a board virtually on a computer, I get a real one in my hand, I need to test it and sometime looking on the top is not enough !

     

    - X-ref for busses

    This one is odd to me as well. In the case of a single net the XREF

    makes sense since you want to easily find other instances of that net. A

    bus however is a collection of nets, so I find an X-ref for a bus less

    useful since it's doesn't aid in finding a particular signal.

    Additionally, Bus labels can get pretty long so I'm sure there are cases

    where this would be inconvenient.

    No, I think the Xref for bus is to locate the bus.

    It should work like net, and locate the position of the other XREF of the same bus (same bus = same bus name).

     

     

     

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to kikoun

    On 30/10/15 11:51, Guillaume barrey wrote:

    Me too, when I need a mirrored view of a board, it's only because I have

    a board on my desk, and need to find a part or a net to put an

    oscilloscope on it. I don't want to change my board , certainly not !!

    I just need a mirrored view of it, simply because in real life, after

    designing a board virtually on a computer, I get a real one in my hand,

    I need to test it and sometime looking on the top is not enough !

     

    I which case what I do is print the bottom side, mirrored, to a PDF.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to kikoun

    On 30/10/15 11:51, Guillaume barrey wrote:

    Me too, when I need a mirrored view of a board, it's only because I have

    a board on my desk, and need to find a part or a net to put an

    oscilloscope on it. I don't want to change my board , certainly not !!

    I just need a mirrored view of it, simply because in real life, after

    designing a board virtually on a computer, I get a real one in my hand,

    I need to test it and sometime looking on the top is not enough !

     

    I which case what I do is print the bottom side, mirrored, to a PDF.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • kikoun
    0 kikoun over 10 years ago in reply to autodeskguest

    On 30/10/15 11:51, Guillaume barrey wrote:

    Me too, when I need a mirrored view of a board, it's only because I have

    a board on my desk, and need to find a part or a net to put an

    oscilloscope on it. I don't want to change my board , certainly not !!

    I just need a mirrored view of it, simply because in real life, after

    designing a board virtually on a computer, I get a real one in my hand,

    I need to test it and sometime looking on the top is not enough !

     

    I which case what I do is print the bottom side, mirrored, to a PDF.

    It's what I do now but tell me how to you use the 'show @' command on printed pdf, how you follow net, how do you manage to highlight a net... I tried to click with my pen on the paper but nothing happen !!!!!

    More seriously... if some people ask this feature it's is not just for been annoying...(i know I'm no the only one to ask this...) maybe it because it would be easier to do some task....

     

    Guillaume.